Multicomp Pro
  • Products & Partners
  • Manufacturers
  • Multicomp Pro
  • More
  • Cancel
Multicomp Pro
Forum What are you using to reduce and prevent static when working on kit and projects?
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Multicomp Pro to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 27 subscribers
  • Views 2459 views
  • Users 0 members are here
  • static eliminator ac ion fan
  • multicomp pro
  • ion fan
Related

What are you using to reduce and prevent static when working on kit and projects?

cstanton
cstanton over 2 years ago

Multicomp Pro now has a series of products  available for you to use on your bench top to reduce static while you're working with its ion fans.

MP741063MP741064

These are available on our EU and APAC stores, they do not have US plugs supplied with them.

Bill of Materials

Product Name Manufacturer Quantity View Products
MULTICOMP PRO MP741063 Static Eliminator AC Ion Fan, Benchtop, 240V, 15W MULTICOMP PRO 1 Buy Now
MULTICOMP PRO MP741064 Static Eliminator AC Ion Fan, Benchtop, Remote Control, 240V, 20W MULTICOMP PRO 1 Buy Now
MULTICOMP PRO MP741063 STATIC ELIMINATOR AC ION FAN, 240V, 15W ROHS COMPLIANT: YES MULTICOMP PRO 1 Buy Now
MULTICOMP PRO MP741068 ION LAUNCHER, STATIC ELIMINATOR DC FAN ROHS COMPLIANT: NA MULTICOMP PRO 1 Buy Now
MULTICOMP PRO MP741069 ION EMITTING NEEDLE, STATIC DC FAN ROHS COMPLIANT: NA MULTICOMP PRO 1 Buy Now
MULTICOMP PRO MP741070 ION LAUNCHER, STATIC ELIMINATOR AC FAN ROHS COMPLIANT: NA MULTICOMP PRO 1 Buy Now
 

Do you use this kind of hardware when you're working on electronics? What do you think of them? Let us know in the comments below.

  • Sign in to reply
  • Cancel

Top Replies

  • misaz
    misaz over 2 years ago +2
    I just touch something grounded before opening package. Otherwise I mostly ignore precautions.
  • Gough Lui
    Gough Lui over 2 years ago +2
    I used to take no precautions at all, and don't ever recall being bitten by it. Touching grounded metal was advice freely given back in the days, but I feel like this isn't sufficient (perhaps bordering…
  • michaelkellett
    michaelkellett over 2 years ago +2
    I use an antistatic mat. Good for protecting the bench as well and easy to clean. I wonder how the ioniser fan gets on competing with a fume extractor - the fume extractor isn't that good at moving the…
Parents
  • shabaz
    shabaz over 2 years ago

    Hehe anything with a fan in it to cool a place down would be extremely welcome right now.

    Interesting devices! I've never used one of these, but it sounds like something worth trying. Should be easy to see the effects of it, various science-experiments can indicate presence or absence of static charges. 

    I always use a wrist-strap (except the times I forget to plug it in if I temporarily detatch!), plus have a grounded mat, so not a whole lot of effort currently. My soldering iron has a grounded ring that is easy to touch as well.

    Same as Doug, I try not to touch parts when not in-circuit. ESD tweezers help with that! They have possibly saved hundreds of components from damage. Especially MOSFETs; it's standard practice for me to solder them in plus a resistor to help protect them a little bit at least, without touching any of the connections.

    Also, I try to solder resistors first, and then semiconductors, so that the board is as ready as possible to try to reduce damage.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 2 years ago

    Hehe anything with a fan in it to cool a place down would be extremely welcome right now.

    Interesting devices! I've never used one of these, but it sounds like something worth trying. Should be easy to see the effects of it, various science-experiments can indicate presence or absence of static charges. 

    I always use a wrist-strap (except the times I forget to plug it in if I temporarily detatch!), plus have a grounded mat, so not a whole lot of effort currently. My soldering iron has a grounded ring that is easy to touch as well.

    Same as Doug, I try not to touch parts when not in-circuit. ESD tweezers help with that! They have possibly saved hundreds of components from damage. Especially MOSFETs; it's standard practice for me to solder them in plus a resistor to help protect them a little bit at least, without touching any of the connections.

    Also, I try to solder resistors first, and then semiconductors, so that the board is as ready as possible to try to reduce damage.