NXP Semiconductors
  • Products & Partners
  • Manufacturers
  • NXP Semiconductors
  • More
  • Cancel
NXP Semiconductors
Forum how to let the program run from function _Startup
  • Blog
  • Forum
  • Documents
  • Events
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NXP Semiconductors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 41 subscribers
  • Views 361 views
  • Users 0 members are here
Related

how to let the program run from function _Startup

bluesea
bluesea over 17 years ago

I'm trying to debug my application based on MC9S08DZ60 and encountered a problem need your help.

 

I used the following link file in my project and hope the program will run from the function _Starup in the file Star08.c . but in fact, the program runs from the function main in full chip simulation mode.  could any one tell me why the problem occurs and how to resolve the problem?

 

below is the link file I uesd. Thanks

 

###################################################################
*/

NAMES

END

SECTIONS
    Z_RAM                    =  READ_WRITE   0x0080 TO 0x009F;
    RAM                      =  READ_WRITE   0x00A0 TO 0x107F;
    ROM                       =  READ_ONLY    0x1900 TO 0xFFAD;
    EEPROM                   =  READ_ONLY    0x1400 TO 0x17FF;
END

PLACEMENT
    DEFAULT_RAM                         /* non-zero page variables */
                                        INTO  RAM;

    DEFAULT_ROM, ROM_VAR, STRINGS       INTO  ROM;
    _DATA_ZEROPAGE,                     /* zero page variables */
    MY_ZEROPAGE                         INTO  Z_RAM;
END

 

the CPU module. */

STACKSIZE 0x0080                       /* Size of the system stack. Value can be changed on the "Build options" tab */

VECTOR 0 _Startup /* Reset vector: this is the default entry point for an application. */

  • Sign in to reply
  • Cancel
  • AlexLuFarnell
    AlexLuFarnell over 17 years ago

    The application does start at _Startup, just for "ease of use" the debugger let is run to main

    before you first see the state. There is a setting for this, check the menus in hiwave (sorry forget where it is exactly). Find it, change it and click the save menu once, then it should be used in future debug sessions.

    Another way to start debugging from _Startup is to simply press the reset button. Then you end up starting the debug process again at _Startup.

     

    This can be done in HI-WAVE in the following way:

      - Start the debugger the usual way (click on Debug button).

      - Select "File" -> "Configuration"

      - Change to "Load" Tab

      - Uncheck "Run after Successful load"

      - Click OK to close the dialog.

     

    Next time you start eh debugger application will stop at its entry point (_Startup).

     

    Note that this settings is project specific, So you need to do that once for each project you want to debug.

     

    I hope this helps.image