NXP Semiconductors
  • Products
  • Manufacturers
  • NXP Semiconductors
  • More
  • Cancel
NXP Semiconductors
Forum Freescale and Bluetechnix competition
  • Blog
  • Forum
  • Documents
  • Events
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NXP Semiconductors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 26 replies
  • Subscribers 47 subscribers
  • Views 3110 views
  • Users 0 members are here
  • i.mx51
  • sbc-i.mx51
  • freescale
  • computer
  • bluetechnix
  • mobile
  • gpu
  • platform
  • single-board
Related

Freescale and Bluetechnix competition

awinning
awinning over 14 years ago

Freescale and Bluetechnix have asked me to run a competition with three Bluetechnix SBC-iMX51 boards as prizes. I've posted the main specs of the board below, and if you need more information I've also linked the datasheet. All you have to do is tell us what you'd use the board for if you won. After the event I'll include the answers in one or more polls and you can vote for the best ideas. Winners of the poll(s) get the boards


You have until May 3rd to get your entry in

 



SBC-I.MX51SBC-I.MX51

The Single-Board Computer SBC-I.MX51SBC-I.MX51 is based on Freescale’s high-performance i.MX51 mobile platform, incorporating

an ARM Cortex-A8 CPU, an Image Processing Unit (IPUv3EX), a Video Processing Unit (VPU) and a Graphical Processing Unit

(GPU). The IPUv3EX provides comprehensive support for connectivity to displays and cameras. The VPU supports hardware

encoding and decoding of MPEG-4, H.263, H.264 and many more standards. The GPU serves 3D and 2Dacceleration in

hardware. The board‘s memory capabilities (NAND Flash, DDR2) and numerous interfaces like Ethernet, HDMI,4xUSB

and USB-OTG turn the SBC-I.MX51SBC-I.MX51 into the ultimate development board for future high-end embedded devices.

http://datasheets.bluetechnix.at/goto/SBC-i.MX51/SBC-i.MX51_OV_20110324.pdf  SBC-I.MX51SBC-I.MX51


Terms and Conditions http://www.element14.com/community/docs/DOC-29410

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 14 years ago

    Since it has low power consumption, lots of I/O and is fairly powerful, I would see if I could make an interesting environmental monitor. Since it should be well suited to being remotely situated, connected to various sensors and whilst capable of locally processing data and/or serving content.

     

    Rather than things such as temperature and wind speed etc, I'd be more concerned with measurements such as the earth's magnetic field and radiation levels. The latter is particularly topical for obvious reasons, and the former since it's been predicted that we are entering a period of increased geomagnetic activity. So, ideally I'd like to try and construct a proton precession magnetometer, although this may turn out to be quite a challenge. However, measuring background radiation would be simpler and there are perhaps simpler instruments for measuring the earth's magnetic field to a lower resolution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 14 years ago

    Since it has low power consumption, lots of I/O and is fairly powerful, I would see if I could make an interesting environmental monitor. Since it should be well suited to being remotely situated, connected to various sensors and whilst capable of locally processing data and/or serving content.

     

    Rather than things such as temperature and wind speed etc, I'd be more concerned with measurements such as the earth's magnetic field and radiation levels. The latter is particularly topical for obvious reasons, and the former since it's been predicted that we are entering a period of increased geomagnetic activity. So, ideally I'd like to try and construct a proton precession magnetometer, although this may turn out to be quite a challenge. However, measuring background radiation would be simpler and there are perhaps simpler instruments for measuring the earth's magnetic field to a lower resolution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • awinning
    awinning over 14 years ago in reply to Former Member

    Some more great entries. Thanks guys. Michael, this wouldn't be you would it?