NXP Semiconductors
  • Products & Partners
  • Manufacturers
  • NXP Semiconductors
  • More
  • Cancel
NXP Semiconductors
Forum RS08 keyboard interrupt
  • Blog
  • Forum
  • Documents
  • Events
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NXP Semiconductors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 41 subscribers
  • Views 493 views
  • Users 0 members are here
Related

RS08 keyboard interrupt

bluesea
bluesea over 17 years ago

I checked the MC9RS08KA2.pdf but am still not sure about two things:

 

1. When I configure multiple pins as a keyboard interrupt source, how am I supposed to find out which pin did actually cause the interrupt?

From how I got it, I need to poll SIP1_KBI (same for all pins) to find out about an interrupt at all.

What is the recommended best practice after that, just read the value of the port bits, like this:

 

if(PTAD_PTAD0) // Key 0 pressed

...

if(PTAD_PTAD1) // Key 1 pressed

 

or is there  a different method?

 

2. How do I reset the interrupt flag to allow for successive interrupts?

 

Chapter 5.8.6 says (about the SIP1_KBI bit):

"Clearing the KBF flag of the KBISC register clears this bit."

 

Chapter 7.3.1 however states:

"Writes have no effect on KBF." So I assume "KBISC_KBF = 0;" won't work.

 

Then I find:

"Writing a 1 to KBACK is part of the flag-clearing mechanism."

 

This sounds like it would take several steps to really clear the flag, however I can't seem to find a more detailed description of the mentioned "flag-clearing mechanism."

 

So is "KBISC_KBACK = 1;" all there is to do? According to the block diagram this seems fine, but the above quote is somewhat confusing to me.image

  • Sign in to reply
  • Cancel
Parents
  • AlexLuFarnell
    0 AlexLuFarnell over 17 years ago

    imageFirstly, I have no experience with the RS08. These comments are based on S08.

     

    You have to work out which of the enabled KBI pins caused the interrupt yourself.

    Normally you would read the whole port into a variable first and analyse it from there. This avoids the time skew of polling each one individually.

     

    You can poll the flag to find out if a KBI enabled pin has been activated, or you can enable interrupts to interrupt when the flag becomes set.

     

    Writing a 1 to KBACK is all that is required to clear the flag and acknowledge the interrupt.

     

    Hope that helps.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • AlexLuFarnell
    0 AlexLuFarnell over 17 years ago

    imageFirstly, I have no experience with the RS08. These comments are based on S08.

     

    You have to work out which of the enabled KBI pins caused the interrupt yourself.

    Normally you would read the whole port into a variable first and analyse it from there. This avoids the time skew of polling each one individually.

     

    You can poll the flag to find out if a KBI enabled pin has been activated, or you can enable interrupts to interrupt when the flag becomes set.

     

    Writing a 1 to KBACK is all that is required to clear the flag and acknowledge the interrupt.

     

    Hope that helps.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer