NXP Semiconductors
  • Products & Partners
  • Manufacturers
  • NXP Semiconductors
  • More
  • Cancel
NXP Semiconductors
Forum Hi-WAVE Communicationto the target has failed (target MCU has no clock or wrong BDM clock speed is used or derivative is secured!)
  • Blog
  • Forum
  • Documents
  • Events
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NXP Semiconductors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 40 subscribers
  • Views 822 views
  • Users 0 members are here
Related

Hi-WAVE Communicationto the target has failed (target MCU has no clock or wrong BDM clock speed is used or derivative is secured!)

e14 Contributor
e14 Contributor over 12 years ago

Hello,

 

I am using MCU MC9S12G series. The controller is already mounted on a PCB.

 

I am using a jig to flash the MCU using PEs USB BDM Multilink (6 pin).

 

The controller is part of a pre-aged component.

The actual working voltage of the whole pcb is 24v.

 

The regulator supplies the MCU with 5V.

 

The voltages at the jig and BDM Multilink interfaces are Vdd = 5V

  Reset = 5V

  BGND = 5V

 

I am using code warrior for loading the code. The error obtained is

 

Hi-WAVE Communication to the target has failed 

(target MCU has no clock or wrong BDM clock speed is used or derivative is secured!)

 

I have set the clock.

CLKDIV: [entered value here |default 73]

 

When i try to unsecure the MCU using the unsecure command in code warrior i get the following message :

 

"Derivative could NOT be unsecured"

 

I am unable to flash the code.

 

Another team has used the same jig to flash the code on to a 12v version of the pcb having same MCU, successfully.

 

Can the input voltage of the jig have any effect on flashing if i am getting 5v to the mcu?

 

Please help.