NXP Semiconductors
  • Products & Partners
  • Manufacturers
  • NXP Semiconductors
  • More
  • Cancel
NXP Semiconductors
Documents Freescale introduces the first magnetometer in its Xtrinsic sensor portfolio
  • Blog
  • Forum
  • Documents
  • Events
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NXP Semiconductors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: MAb
  • Date Created: 13 Jan 2011 3:41 PM Date Created
  • Last Updated Last Updated: 9 Nov 2021 4:55 PM
  • Views 620 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Freescale introduces the first magnetometer in its Xtrinsic sensor portfolio

New three-axis magnetometer provides directional heading accuracy for use in localization applications for smart mobile devices

 

http://cache.freescale.com/files/graphic/product_freescale/MAG3110cs.jpgFreescale Semiconductor is expanding its Xtrinsic line of intelligent  sensing solutions with the introduction of the MAG3110, the company's  first magnetometer. The Xtrinsic MAG3110 is a small-profile, low-power,  three-axis digital magnetometer that delivers enhanced digital  electronic compass (eCompass) functionality for location-based services  (LBS) such as navigation, dead-reckoning and location-tracking in smart  mobile devices and other electronics.

 

When coupled with an accelerometer and GPS, the Xtrinsic MAG3110  helps give end-users precise orientation and location information for a  more comprehensive navigational system. The Xtrinsic MAG3110 also acts  as a backup system when both cellular and GPS signals are unavailable by  sensing the earth's magnetic field to provide directional context.

 

The Xtrinsic MAG3110 is designed to address rapidly growing consumer  demand for devices featuring LBS capabilities. LBS has fueled consumer  adoption of a number of popular smart mobile device applications  including Foursquare, Facebook Places and Google Goggles. A forecast by  Juniper Research predicts global LBS revenues could soar to $12.7  billion by 2014, up from $3 billion in 2009. As this type of  functionality gains popularity, end-users are expected to demand  always-on navigational connections and more accurate location  identification, which can be enabled through the use and design of  magnetometer sensor technology such as the Xtrinsic MAG3110.

 

To read the full announcement on Freescale website, go here

 

To get access to the description of MAG3110, go here

 

To access the fact sheet of the MAG3110, go here

 

To access the data sheet of the MAG3110, go here

  • Freescale Tagged Content
  • freescale
  • ap:sensor
  • ap:accelerometer
  • magnetometer