NXP Semiconductors
  • Products & Partners
  • Manufacturers
  • NXP Semiconductors
  • More
  • Cancel
NXP Semiconductors
Documents Freescale’s latest Qorivva microcontrollers help automotive industry advance toward zero-fatality goal
  • Blog
  • Forum
  • Documents
  • Events
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NXP Semiconductors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: MAb
  • Date Created: 7 Apr 2011 3:51 PM Date Created
  • Last Updated Last Updated: 9 Nov 2021 5:01 PM
  • Views 610 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Freescale’s latest Qorivva microcontrollers help automotive industry advance toward zero-fatality goal

New 32-bit MCU family designed to make advanced driver assistance systems more affordable for a broad range of vehicles


The U.S. Insurance Institute for  Highway Safety reports that one in three fatal passenger vehicle crashes  and one in five serious or moderate injury crashes could have been  avoided if more vehicles had been equipped with crash-avoidance  technologies. Freescale Semiconductor’s cost-effective new family of  Qorivva 32-bit microcontrollers (MCUs) is designed to help make advanced  driver assistance systems more affordable and accessible for a broad  range of vehicle models.

 

The Qorivva MPC567xK family of 32-bit MCUs, built on Power  ArchitectureRegistered technology, provides designers of automotive safety  systems the ability to engineer advanced, yet economical, safety  features, such as blind-spot detection, lane-departure warning systems,  side view assistance and adaptive headlights. These and similar advanced  automotive safety systems are part of the rapidly growing market known  as advanced driver assistance systems (ADAS).

 

The Qorivva MPC567xK family helps reduce and, in many cases,  eliminate the need for additional external signal processing components.  With its high-throughput, dual-core architecture, high-density on-chip  memory and optimized signal processing engines (SPE), the MPC567xK  family delivers an affordable, compelling solution for the latest ADAS  applications. The MPC567xK family uses a dual core implementation of the  new Z7 Power Architecture CPU. This same core is used on the MPC5674F  which recently achieved an unprecedented benchmark score of 305  AutomarksTm in the Embedded Microprocessor Benchmark Consortium’s  (EEMBCRegistered) AutoBenchTm suite of tests. Even in that single core  configuration the Z7 demonstrated more than three times the performance  of the previous highest score set by a competitor.

 

“Freescale’s Qorivva MPC567xK MCUs are a cost-effective way for  automakers to help satisfy consumers seeking safer vehicles and meet  global government regulations requiring better passenger protections,”  said Ray Cornyn, director of Freescale’s Automotive MCU business. “This  economical, scalable new MCU family, which is built on Power  Architecture technology we’ve tailored specifically for the automotive  market, allows us to deliver a competitive advantage for the global ADAS  market and can help make vehicles safer around the world.”

Even with rapidly increasing global demand, the expense of ADAS  components has sometimes made it difficult for automakers to incorporate  the systems into the full range of their vehicle lineups. As a leading  global supplier of automotive semiconductors, Freescale has developed a  cost- and power-efficient solution to help lower the barriers to  providing ADAS for all vehicles.

The 32-bit, dual-core MPC567xK MCUs include a lock-step mode to  detect and mitigate common hardware and software faults while meeting  automotive software integrity level D standards ahead of anticipated  global legislative mandates for more active safety. Ideal for radar- and  camera-based ADAS, the MPC567xK family operates at up to 180 MHz, with  up to 2 MB flash memory and 512K SRAM.

 

Freescale announced the Qorivva line of 32-bit automotive MCUs in November 2010. In addition, the company announced the expansion of the Xtrinsic intelligent sensing portfolio with a 77 GHz silicon Germanium (siGe) chipset for intelligent radar  technology. Freescale’s Qorivva MPC567xK family, in combination with its   siGE products, allows it to address the core chipset for radar based  ADAS solutions. With these innovations and more than 200 million 32-bit  Power Architecture MCUs shipped to date, Freescale has proven itself as a  trusted supplier of solutions for the automotive electronics market.

 

Comprehensive ecosystem for Qorivva MCUs
The  strength and value of Qorivva microcontrollers extend beyond the  silicon. Each Qorivva MCU comes with a full run-time software solution,  including AUTOSAR MCAL driver suites and AUTOSAR real-time operating  system for single-core and multicore MCUs. Qorivva MCUs also are  supported by development tools, including high-performance compilers and  multicore debuggers from Freescale development partners and Freescale’s  CodeWarrior development studio.

Freescale’s deep roots in the automotive electronics industry are  apparent in its involvement with industry consortia. Freescale is a  founding member of the DSI, Power.org, FlexRayTm and LIN consortia, a  premium member of AUTOSAR and an active member of the PSI5, JASPAR and  GENIVI consortia. Freescale’s Power Architecture products are also  supported by its global systems labs and software customization  services.

 

Availability
Freescale plans to offer sample  quantities of the first member of the MPC567xK family in March. General  availability is planned for Q3 2011. For more information, visit www.freescale.com/automotive.

  • Freescale Tagged Content
  • freescale
  • qorivva
  • sp:freescale
  • microcontroller