NXP Semiconductors
  • Products & Partners
  • Manufacturers
  • NXP Semiconductors
  • More
  • Cancel
NXP Semiconductors
Documents Tutorial: Accelerating the Freescale FRDM-KL25Z Freedom Board
  • Blog
  • Forum
  • Documents
  • Events
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NXP Semiconductors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: MAb
  • Date Created: 15 Oct 2012 3:44 PM Date Created
  • Last Updated Last Updated: 9 Nov 2021 5:05 PM
  • Views 1313 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Tutorial: Accelerating the Freescale FRDM-KL25Z Freedom Board

This tutorial was extracted from Erich Styger blog http://mcuoneclipse.wordpress.com with his agreement.

 

 

In “Tutorial: Enlightning the Freedom KL25Z Board” I used the RGB LED on the FRDM-KL25Z board. This tutorial extends it to use the Freescale MMA8451Q    MMA8451Q inertial sensor on the board which is connected through I2C to the Freescale MKL25Z128VLK4    MKL25Z128VLK4 microcontroller:

 

Freedom Board Block Diagram

Freedom Board Block Diagram with MMA8451Q (lower right corner)

 

 

The goal is show the accelerometer x, y and z-axis on the RGB LED.

 

I’m using CodeWarrior for MCU V10.3 which has the ARM gcc build tools integrated for the Kinetis family. It is possible to extend the “Tutorial: Enlightning the Freedom KL25Z Board” project and to add the I2C and accelerometer, or starting with a new project. In the steps below I create a new project, but I’m not going into the details how to add the LED as this is explained in the previous tutorial.

 

 

Creating the Project

 

I use the menu File > New > Bareboard Project:

 

File New Menu to create a new Bareboard project

File New Menu to create a new Bareboard project

 

 

Next, I need to specify a name for my project:

 

Naming the project

Naming the project

 

 

Next, I select the MKL25Z128 as my device:

 

Hint: I can use the filter field to at the top of the dialog to filter the devices.

 

 

Selecting KL25Z128 with filter text

Selecting KL25Z128 with filter text

 

 

Next, to select the debug connection. As the Freedom Board has the new OpenSDA on it, this is my choice:

 

OpenSDA Debug Connection

OpenSDA Debug Connection

 

 

In the next dialog, I can go with the default settings. the ARM GNU GCC is the only (and default) tool-chain for Kinetis L (Cortex M0+) family:

 

gcc ARM Toolchain

gcc ARM Toolchain

 

 

Next, I select Processor Expert for my project:

 

Processor Expert

Processor Expert

 

 

Pressing ‘Finish’ creates the project for me:

 

Freedom Project

Freedom Project

 

 

RGB LED

 

How to add the RGB LED support is shown in “Tutorial: Enlightning the Freedom KL25Z Board” so I’m not explaining the details here.

 

Hint: I can copy-paste components from one project to another project in MCU10.3, even between workspaces. Simply select the component(s), use the ‘copy’ context menu, switch to the other project and past it into the Components group of that project. Really cool!

 

With the LEDs added, the component list should look something like this:

 

LED components

LED components

 

 

I2C

 

Processor Expert provides an I2C component (I2C_LDD) which implements a driver for it. I make sure that I have my project selected, then I choose in the Components Library view the I2C_LDD and add it to my project:

 

Adding I2C_LDD

Adding I2C_LDD

 

 

According to the schematics, the accelerometer is on the I2C0 channel (with PTE25 and PTE25), so this is already the default, so no change here:

 

I2C Channel with pins

I2C Channel with pins

 

 

I’m only using the accelerometer on the bus, and the MMA8451QR1 is using the (hex) 1D slave address, so I specify this in the properties. To enter hex values, I need to switch the format to the ‘H’ mode:

 

Target Slave Address

Target Slave Address

 

 

What I need to know the maximum bus clock frequency. The MMA8451QR1 Reference guide gives this information:

 

I2C MMA8451 clock speed

I2C MMA8451QR1 clock speed

 

 

And the schematic of the Freedom board has this:

 

I2C Inertial Sensor Schematics

I2C Inertial Sensor Schematics

 

 

So we have I2C Pullups with 4.7K Ohm, but Cb is not specified. With 100 KHz I would be on the safe side, but I tried 1 MHz and that worked fine for me:

 

I2C Clock Settings

I2C Clock Settings

 

 

With this, I have my basic settings in place and can generate the driver code:

 

Generate Driver Code

Generate Driver Code

 

 

Accelerometer Interface

 

Time to write the software :-) . Using the I2C_LDD, I need to use a device data structure with flags for data received and sent. So I declare this in my header file MMA8451.h:

 

 

01/*
02* MMA8451.h
03* Author: Erich Styger
04*/
05
06#ifndef MMA8451_H_
07#define MMA8451_H_
08
09#include "PE_Types.h"
10#include "PE_LDD.h"
11
12typedef struct {
13volatile bool dataReceivedFlg; /* set to TRUE by the interrupt if we have received data */
14volatile bool dataTransmittedFlg; /* set to TRUE by the interrupt if we have set data */
15LDD_TDeviceData *handle; /* pointer to the device handle */
16} MMA8451_TDataState;
17
18/* \brief Run the demo application */
19void MMA8451_Run(void);
20
21#endif /* MMA8451_H_ */

 

 

I2C_LDD Events

 

 

The I2C_LDD is using events callback. For this I need to set the proper flags in the event:

 

 

01/*
02** ===================================================================
03** Event : I2C2_OnMasterBlockSent (module Events)
04**
05** Component : I2C2 [I2C_LDD]
06** Description :
07** This event is called when I2C in master mode finishes the
08** transmission of the data successfully. This event is not
09** available for the SLAVE mode and if MasterSendBlock is
10** disabled.
11** Parameters :
12** NAME - DESCRIPTION
13** * UserDataPtr - Pointer to the user or
14** RTOS specific data. This pointer is passed
15** as the parameter of Init method.
16** Returns : Nothing
17** ===================================================================
18*/
19void I2C2_OnMasterBlockSent(LDD_TUserData *UserDataPtr)
20{
21MMA8451_TDataState *ptr = (MMA8451_TDataState*)UserDataPtr;
22
23ptr->dataTransmittedFlg = TRUE;
24}
25
26/*
27** ===================================================================
28** Event : I2C2_OnMasterBlockReceived (module Events)
29**
30** Component : I2C2 [I2C_LDD]
31** Description :
32** This event is called when I2C is in master mode and finishes
33** the reception of the data successfully. This event is not
34** available for the SLAVE mode and if MasterReceiveBlock is
35** disabled.
36** Parameters :
37** NAME - DESCRIPTION
38** * UserDataPtr - Pointer to the user or
39** RTOS specific data. This pointer is passed
40** as the parameter of Init method.
41** Returns : Nothing
42** ===================================================================
43*/
44void I2C2_OnMasterBlockReceived(LDD_TUserData *UserDataPtr)
45{
46MMA8451_TDataState *ptr = (MMA8451_TDataState*)UserDataPtr;
47
48ptr->dataReceivedFlg = TRUE;
49}

 

 

Aditionally, I need to include my header file into Events.c:

 

 

01/** ###################################################################
02** Filename : Events.c
03** Project : ProcessorExpert
04** Processor : MKL25Z128VLK4
05** Component : Events
06** Version : Driver 01.00
07** Compiler : GNU C Compiler
08** Date/Time : 2012-08-23, 07:09, # CodeGen: 0
09** Abstract :
10** This is user's event module.
11** Put your event handler code here.
12** Settings :
13** Contents :
14** Cpu_OnNMIINT - void Cpu_OnNMIINT(void);
15**
16** ###################################################################*/
17/* MODULE Events */
18
19#include "Cpu.h"
20#include "Events.h"
21
22/* User includes (#include below this line is not maintained by Processor Expert) */
23#include "MMA8451.h"

 

 

Accelerometer Implementation

 

 

For this I create a file MMA8451.c with routines to read and write accelerometer registers:

 

 

01/*
02* MMA8451.c
03* Author: Erich Styger
04*/
05#include "MMA8451.h"
06#include "I2C2.h"
07#include "LED1.h"
08#include "LED2.h"
09#include "LED3.h"
10
11/* External 3-axis accelerometer control register addresses */
12#define MMA8451_CTRL_REG_1 0x2A
13/* MMA8451QR1 3-axis accelerometer control register bit masks */
14#define MMA8451_ACTIVE_BIT_MASK 0x01
15#define MMA8451_F_READ_BIT_MASK 0x02
16
17/* External 3-axis accelerometer data register addresses */
18#define MMA8451_OUT_X_MSB 0x01
19#define MMA8451_OUT_X_LSB 0x02
20#define MMA8451_OUT_Y_MSB 0x03
21#define MMA8451_OUT_Y_LSB 0x04
22#define MMA8451_OUT_Z_MSB 0x05
23#define MMA8451_OUT_Z_LSB 0x06
24
25static MMA8451_TDataState deviceData;
26
27uint8_t MMA8451_ReadReg(uint8_t addr, uint8_t *data, short dataSize) {
28uint8_t res;
29
30/* Send I2C address plus register address to the I2C bus *without* a stop condition */
31res = I2C2_MasterSendBlock(deviceData.handle, &addr, 1U, LDD_I2C_NO_SEND_STOP);
32if (res!=ERR_OK) {
33return ERR_FAILED;
34}
35while (!deviceData.dataTransmittedFlg) {} /* Wait until data is sent */
36deviceData.dataTransmittedFlg = FALSE;
37
38/* Receive InpData (1 byte) from the I2C bus and generates a stop condition to end transmission */
39res = I2C2_MasterReceiveBlock(deviceData.handle, data, dataSize, LDD_I2C_SEND_STOP);
40if (res!=ERR_OK) {
41return ERR_FAILED;
42}
43while (!deviceData.dataReceivedFlg) {} /* Wait until data is received received */
44deviceData.dataReceivedFlg = FALSE;
45return ERR_OK;
46}
47
48uint8_t MMA8451_WriteReg(uint8_t addr, uint8_t val) {
49uint8_t buf[2], res;
50
51buf[0] = addr;
52buf[1] = val;
53res = I2C2_MasterSendBlock(deviceData.handle, &buf, 2U, LDD_I2C_SEND_STOP); /* Send OutData (3 bytes with address) on the I2C bus and generates not a stop condition to end transmission */
54if (res!=ERR_OK) {
55return ERR_FAILED;
56}
57while (!deviceData.dataTransmittedFlg) {} /* Wait until date is sent */
58deviceData.dataTransmittedFlg = FALSE;
59return ERR_OK;
60}

 

 

RGB Demo

 

 

What is missing is the demo code itself. I keep things simple here, and turn on one of the LEDs if the acceleration on an axis is exceeding a threshold:

 

01static int8_t xyz[3];
02
03void MMA8451_Run(void) {
04uint8_t res;
05
06LED1_On();
07LED2_On();
08LED3_On();
09deviceData.handle = I2C2_Init(&deviceData);
10/* F_READ: Fast read mode, data format limited to single byte (auto increment counter will skip LSB)
11* ACTIVE: Full scale selection
12*/
13res = MMA8451_WriteReg(MMA8451_CTRL_REG_1, MMA8451_F_READ_BIT_MASK|MMA8451_ACTIVE_BIT_MASK);
14if (res==ERR_OK) {
15for(;;) {
16res = MMA8451_ReadReg(MMA8451_OUT_X_MSB, (uint8_t*)&xyz, 3);
17LED1_Put(xyz[0]>50);
18LED2_Put(xyz[1]>50);
19LED3_Put(xyz[2]>50);
20}
21}
22I2C2_Deinit(deviceData.handle);
23LED1_Off();
24LED2_Off();
25LED3_Off();
26}

 

 

Calling from main()

 

 

And the last piece is to call my demo routine from main():

 

01/** ###################################################################
02** Filename : ProcessorExpert.c
03** Project : ProcessorExpert
04** Processor : MKL25Z128VLK4
05** Version : Driver 01.01
06** Compiler : GNU C Compiler
07** Date/Time : 2012-08-23, 07:09, # CodeGen: 0
08** Abstract :
09** Main module.
10** This module contains user's application code.
11** Settings :
12** Contents :
13** No public methods
14**
15** ###################################################################*/
16/* MODULE ProcessorExpert */
17
18/* Including needed modules to compile this module/procedure */
19#include "Cpu.h"
20#include "Events.h"
21#include "LED1.h"
22#include "LED2.h"
23#include "LED3.h"
24#include "GPIO1.h"
25#include "GPIO2.h"
26#include "I2C2.h"
27/* Including shared modules, which are used for whole project */
28#include "PE_Types.h"
29#include "PE_Error.h"
30#include "PE_Const.h"
31#include "IO_Map.h"
32
33/* User includes (#include below this line is not maintained by Processor Expert) */
34#include "MMA8451.h"
35
36int main(void)
37{
38/* Write your local variable definition here */
39
40/*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/
41PE_low_level_init();
42/*** End of Processor Expert internal initialization. ***/
43
44/* Write your code here */
45MMA8451_Run();
46
47/*** Don't write any code pass this line, or it will be deleted during code generation. ***/
48/*** RTOS startup code. Macro PEX_RTOS_START is defined by the RTOS component. DON'T MODIFY THIS CODE!!! ***/
49#ifdef PEX_RTOS_START
50PEX_RTOS_START(); /* Startup of the selected RTOS. Macro is defined by the RTOS component. */
51#endif
52/*** End of RTOS startup code. ***/
53/*** Processor Expert end of main routine. DON'T MODIFY THIS CODE!!! ***/
54for(;;){}
55/*** Processor Expert end of main routine. DON'T WRITE CODE BELOW!!! ***/
56return 0;
57} /*** End of main routine. DO NOT MODIFY THIS TEXT!!! ***/
58
59/* END ProcessorExpert */
60/*
61** ###################################################################
62**
63** This file was created by Processor Expert 10.0 [05.02]
64** for the Freescale Kinetis series of microcontrollers.
65**
66** ###################################################################
67*/

 

 

Accelerometer In Action

 

 

If I place the board flat on the table, the blue LED is on:

 

Blue LED

Blue LED

 

 

With the board on the side, the green LED is on:

 

Green LED

Green LED

 

 

And with the board standing up, the red LED is on:

 

Red LED

Red LED

 

 

Happy accelerating :-)

  • 32bit
  • freescaledocs
  • Freescale Tagged Content
  • low_power
  • processor_expert
  • freescale
  • Cortex-M
  • accelerometer
  • codewarrior
  • frdm-kl25z
  • kinetis-l
  • 10.3beta
  • microcontroller
  • mcu
  • arm
  • freedom
  • sensor
  • software