NXP Semiconductors
  • Products & Partners
  • Manufacturers
  • NXP Semiconductors
  • More
  • Cancel
NXP Semiconductors
Documents Imagine Never Having to Change a SIM Again
  • Blog
  • Forum
  • Documents
  • Events
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NXP Semiconductors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: peggy-nxp
  • Date Created: 20 Aug 2020 2:00 PM Date Created
  • Last Updated Last Updated: 6 Oct 2021 10:26 PM
  • Views 632 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Imagine Never Having to Change a SIM Again

image

We are probably all aware of what a SIM is. Those fiddley thin pieces of plastic we or the phone salesperson inserts into our new cellular phone when we make a change. Over the years, SIMs have become smaller and smaller, yet they still contain the same crucial information that identifies our cellular device to the service provider and the network operator. Without a valid SIM, we’re not able to connect to any network. While we’ve all had challenges inserting a new SIM or waiting for the updated configuration details to propagate through the cellular network, spare a thought for the installers of the rapidly increasing numbers of IoT devices that use mobile connectivity. For them, the idea of having to insert hundreds or even thousands of SIMs for an IoT sensor deployment and the added complications of dealing with cross border, regional or world-wide implementations creates not only a significant operational challenge but also a major on-going management overhead.

Thankfully, the cellular industry has been working towards a practical solution; the eSIM. An eSIM is just like any other surface-mounted component. It is soldered on to the device’s PCB and is capable of being remotely programmed with the access profiles of multiple cellular networks.

Suddenly, the logistical and management challenges associated with using traditional SIMs have disappeared. An eSIM provides the opportunity for any device to be quickly and easily reconfigured to operate on another operator’s cellular network. Although the eSIM has solved the inconveniences associated with a physically changeable SIM, it requires the mobile industry to agree on how eSIMs are accessed and managed across the network. Naturally, any device connected to a network poses a security risk, something that network operators wanted reassurance on before widely provisioning eSIM support.

This reassurance came from the GSMA. The eSIM Consumer specification was developed by the GSMA and gained certification in 2015. It documents not only the essential features of an eSIM but more importantly, the recommended approach to security and software implementation when built into a device’s embedded universal integrated circuit card (eUICC). The specification stipulates that all security-based functions shall be certified against the GSMA Embedded UICC for Consumer Devices Protection Profile – PP0100. Despite initial caution from the operator community, the existence of the GSMA eUICC Consumer Protection Profile, viewed as a ‘gold standard’ of security protection and the Common Criteria certification approach, have now facilitated broad operator implementation of eSIM and eUICC capabilities.

The Common Criteria evaluation involves independent design analysis conducted by approved evaluation laboratories overseen by a government scheme. For example, it provides the same level of assurance required for ePassports against Common Criteria EAL5+. The evaluation includes the ability to resist state of the art attack methods such as side-channel analysis, laser fault injections and differential fault analysis.

An example of an eUICC is NXP’s SN110U. This single-die PP0100 CC certified IC features an embedded secure element, a near field communications function and an eSIM.