NXP Semiconductors
  • Products & Partners
  • Manufacturers
  • NXP Semiconductors
  • More
  • Cancel
NXP Semiconductors
Documents Innovative Design Drives Electric Vehicle Growth
  • Blog
  • Forum
  • Documents
  • Events
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NXP Semiconductors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: peggy-nxp
  • Date Created: 8 Jan 2021 12:48 PM Date Created
  • Last Updated Last Updated: 6 Oct 2021 10:30 PM
  • Views 581 views
  • Likes 1 like
  • Comments 0 comments
Related
Recommended

Innovative Design Drives Electric Vehicle Growth

placeholder

 

 

2020 may turn out to be a key milestone in the world’s journey away from fossil fuel dependence. The economic slowdown caused by the Covid-19 pandemic has given a powerful insight into an environment with cleaner air, changing peoples’ working and traveling habits and highlighting the damage caused to our planet by climate change. As countries around the world strive to re-start their economies, the recognition that reliance on fossil fuels has to end for the sake of climate change is driving demands to “build back better”.

The transport sector, responsible for around 24% of CO2 emissions globally, is fully in the environmental spotlight, and governments are pushing ahead with ever stricter regulations on vehicle emissions. Norway is at the more aggressive end of the scale, planning to phase out all new sales of internal combustion engine, (ICE), passenger cars by 2025. In the rest of Europe, targets vary between 2030 and 2040, and China is aiming for a minimum 50% market share of New energy vehicles (NEVs) by 2035.

The global automotive sector is responding to these looming emissions deadlines, with all major manufacturers, including Volvo, Daimler, Volkswagen and Ford announcing massive investments in EV development programs. Led by Tesla, the market leader with almost 30% of global sales in the first half of 2020, global automakers collectively launched 143 new EVs in 2019 and plan to introduce another 450 models by 2022.

image

Perhaps one of the biggest barriers to EV adoption thus far has been consumer perception over EV price and performance limitations, especially range; the distance a vehicle can travel before the battery needs to be recharged. These perceptions are progressively eroded as charging infrastructure increases and the industry invests heavily in improving EV development, with a strong focus on battery technology and efficiency improvement.

The modern automobile contains a number of advanced electronic subsystems, each responsible for controlling specific functionality, such as ADAS, infotainment, functional safety and drivetrain, including battery management. The architecture of these onboard systems has evolved away from multiple electronic control units (ECUs) to a collection of domains, each managed by domain controllers which share data and collaborate with each other. These domain controllers are based on powerful, embedded microcontrollers which enable complex processing, using advanced techniques such as virtualization, formerly the preserve of datacentre-based servers.

The impact of this onboard processing capability increases exponentially thanks to developments in vehicle connectivity. C-V2X technology leverages the improved performance and coverage of cellular networks to share the massive amounts of data generated by the car and its sensors, (up to 4 Terabytes per hour), to the cloud. This shared data enables a number of value-adding use cases, including insurance, fleet management, preventative diagnostics and intrusion detection. The connected car also brings the power of cloud-edge processing and artificial intelligence to enhance the power of the onboard domain controllers.

image

The ongoing quest to improve vehicle efficiency and range is driving significant research and development in the propulsion control domain, where energy optimization is a key challenge. A hybrid-electric vehicle (HEV) can optionally be powered by its ICE or its electric motor, and the vehicle’s range is directly dependent on the optimal use of these energy sources. Powerful control algorithms within the propulsion controller decide which source to use, where to use the ICE, where to use the electric motor and where regenerative braking can be used to increase the battery charge state. The quality of these decisions, which directly affect the vehicles range, is enhanced when the controller has access to cloud-based contextual information such as precise location, traffic conditions, average speed of route, expected duration of journey, charging stations locations, gradients on the planned route and driver style.

Vehicle connectivity also enables energy optimization to be enhanced by cloud-edge processing techniques, where deep learning frameworks train machine learning (ML) models in the cloud. These ML models are deployed to the domain controller in the vehicle (the edge) where they use a process known as inferencing to make predictions based on real-time data generated from the vehicle’s sensors.

To integrate the power of this technology, vehicle manufacturers require access to specialist knowledge backed by in-depth resources and NXP Semiconductors are one of a select number of organizations in the ecosystem with this capability. A global leader in auto microprocessors, ADAS, radar, secure car access, infotainment and in-vehicle networking, the NXP comprehensive solution portfolio enables our customers to accelerate the design of their next generation automotive designs, enabling rapid time to market and scalability.

We have a strong track record working with some of the world’s largest vehicle manufacturers to deliver high performance, safe and reliable mobile solutions. To learn more about our specific capabilities, look out for our forthcoming whitepaper, “ Using Vehicle to Cloud Connectivity to Extend Electric Vehicle Range” on our website.