NXP Semiconductors
  • Products & Partners
  • Manufacturers
  • NXP Semiconductors
  • More
  • Cancel
NXP Semiconductors
Documents Press Release - NXP - NXP Semiconductors Announces High Speed Converter Interoperability / Interworking with Altera FPGAs
  • Blog
  • Forum
  • Documents
  • Events
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NXP Semiconductors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rwang
  • Date Created: 23 Feb 2010 6:42 AM Date Created
  • Last Updated Last Updated: 7 Oct 2021 3:09 AM
  • Views 436 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Press Release - NXP - NXP Semiconductors Announces High Speed Converter Interoperability / Interworking with Altera FPGAs

Eindhoven, The Netherlands, February 11, 2010 - NXP Semiconductors has announced that its CGVTm series of JESD204A-compliant data converters are now interoperable with Altera Corporation’s Stratix IV GX and Arria II GX FPGA families, and will also be interoperable in the future with the Cyclone IV GX FPGA family. Assured interoperability and interworking between programmable logic devices and high-speed converters is a critical acceptance criterion for equipment designers, because it eliminates risk and cost associated with project schedules.

 

The new JESD204A-compliant converters from NXP are suitable for cellular base stations and other wireless communication infrastructure equipment, as well as medical, instrumentation and military/aerospace applications. NXP offers ADC and DAC evaluation boards that include the Altera HSMC interface for easy connection to Altera FPGA evaluation boards allowing rapid demonstration of device interoperability. The NXP and Altera evaluation boards are available to qualified OEMs worldwide. NXP’s JESD204A ADC evaluation board based on the ADC1413D will be previewed during the Mobile World Congress 2010 show in Barcelona, Spain, February 15-18.

 

“NXP Semiconductors is pleased to extend this assured interoperability to our CGV customers, many of whom are interested in using the latest Altera FPGAs in their system designs”, said Maury Wood, senior director and product line manager, high speed converters, NXP Semiconductors. “With the proven interoperability of companion JESD204A IP blocks available from Altera, manufacturers can get to market quickly and cost effectively with the supply chain benefits of industry-standard architectures”.

 

“Altera is looking forward to participating in equipment design developments with NXP‘s CGV data converters, where the design engineer will be assured of seamless interoperability with our industry-leading FPGA families including Stratix IV GX, Arria II GX and Cyclone IV GX with integrated transceivers”, said Arun Iyengar, senior director of Altera‘s communications and broadcast business units. “This combination of NXP‘s JESD204A-compliant data converters and Altera's FPGAs will provide designers of wireless base stations and remote radio heads a high degree of flexibility and scalability, while enabling ease-of-use and cost reduction”.

 

CGVTm(Convertisseur Grande Vitesse) designates NXP‘s compliant, superset implementation of the JEDEC JESD204A interface standard, with enhanced rate (4.0 Gbps typical), enhanced reach (100 cm typical), enhanced features (multiple DAC synchronization) and assured FPGA interoperability.

 

Specifically, NXP offers enhancements in terms of transceiver rate (up to 4.0 Gbps versus the standard rate of 3.125 Gbps, a 28% increase), and transmitter reach (up to 100 cm versus the standard reach of 20 cm, a 400% increase). The enhanced CGV features include Multi Device Synchronization (MDS) for the DAC1408D series of D/A Converters, which is not specified, but informatively discussed in the JEDEC specification. NXP has implemented this optional feature to enable LTE MIMO base station and other advanced multi-channel applications. NXP‘s implementation of MDS enables up to sixteen DACs data streams to be sample synchronized and phase coherent.

 

Altera FPGAs

 

  • The 40-nm Stratix IV GX FPGA family offers the industry‘s most advanced FPGAs with unprecedented densities, performance, and system bandwidth, all at the lowest power for high-end FPGAs. Targeting customers in a variety of markets, including communications, broadcast, test, medical and military, Stratix IV GX FPGAs enables designers to achieve new levels of integration and innovation.
  • The 40-nm Arria II GX FPGA family with integrated transceivers, are the ideal devices for 3-Gbps transceiver applications requiring low-cost FPGAs with high-end capabilities. They offer 25% higher performance, up to 50% lower price and up to 50% lower power, compared to competitive high-end FPGAs. Arria II GX FPGAs are targeted for applications using mainstream protocols such as CPRI, PCIe and GbE.
  • The Cyclone IV GX FPGA family with integrated transceivers provides the market‘s lowest cost, lowest power FPGAs. Ideal for high-volume, cost-sensitive applications, Cyclone IV GX FPGAs enable system designers to respond to increased low-cost bandwidth needs driven by the demand for mobile video, voice, and data access, and the hunger for high-quality 3D images.

 

Availability


NXP CGV evaluation boards are available to qualified OEMs worldwide. For more information about NXP‘s data converters, please visit: http://www.nxp.com/products/data_converters/index.html#preview

 

About NXP Semiconductors

NXP Semiconductors provides High Performance Mixed Signal and Standard Product solutions that leverage its leading RF, Analog, Power, Digital Processing and manufacturing expertise. These innovations are used in a wide range of automotive, industrial, consumer, lighting, medical, computing and identification applications. Headquartered in Europe, the company has about 29,000 employees working in more than 30 countries and posted sales of USD 5.4 billion in 2008. News from NXP is located at www.nxp.com.

 

Forward-looking Statements


This release may contain certain forward-looking statements with respect to the financial condition, results of operations and business of NXP and certain plans and objectives of NXP with respect to these items. By their nature, forward-looking statements involve risk and uncertainty because they relate to events and depend on circumstances that will occur in the future and there are many factors that could cause actual results and developments to differ materially from those expressed or implied by these forward-looking statements.

  • tc:embedded
  • sp:nxp
  • pt:fpga
  • at:press_release