NXP Semiconductors
  • Products & Partners
  • Manufacturers
  • NXP Semiconductors
  • More
  • Cancel
NXP Semiconductors
Documents New i.MX product family delivers performance, integration and energy efficiency required for next generation smart mobile devices
  • Blog
  • Forum
  • Documents
  • Events
  • Quiz
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NXP Semiconductors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: PBrunner
  • Date Created: 9 Jun 2010 12:46 PM Date Created
  • Last Updated Last Updated: 7 Oct 2021 5:03 AM
  • Views 428 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

New i.MX product family delivers performance, integration and energy efficiency required for next generation smart mobile devices

Freescale’s  flagship applications processor product line enjoys marketplace  momentum, spawns new offering


TAIPEI (Computex 2010) – June 1, 2010 – Eighteen months since its  introduction, Freescale’s i.MX51 product family has sparked compelling  new product categories, cemented the company’s leadership position in  fast-growing markets and secured more than 50 design wins across a broad  range of consumer applications.

Today, Freescale introduces the i.MX535 processor, the first member  of the new i.MX53 product family, offering HD playback and integrating  key technologies that boost performance and help lower the costs of next  generation consumer products.

Exploding demand for touch-screen consumer devices that deliver  all-day battery life and engaging end-user experiences has fueled  tremendous market acceptance for Freescale’s i.MX51 processor. More than  50 OEM and ODM customers have selected the i.MX51 to power a wide array  of consumer products including tablets, smartbooks, eReaders,  smartphones and video-enabled IP phones.

Building on the market momentum and technical innovation of the  i.MX51, Freescale’s new i.MX535 processor debuts at Computex 2010 to  deliver new levels of performance, integration and software optimization  for smart mobile devices. The processor features 1080p video decode,  720p video encode, improved graphics performance, and a 400MHz-capable  external memory bus that enables larger LCD screens. The device also  integrates a vast array of key peripherals including DDR3, Serial ATA,  LVDS, Ethernet and four USB ports, thereby boosting scalability and  lowering bill of material costs.

The i.MX535 is based on an enhanced version of the ARM CortexTm-A8  core running at up to 1 GHz, and a derivative part designed to deliver  up to 1.2 GHz of performance is planned for later this year.

“Freescale’s long track record of optimizing the advantages of  advanced ARM technology continues with the newest addition to  Freescale’s pacesetting i.MX product line,” said Bernd Lienhard, vice  president and general manager of Freescale’s Multimedia Applications  Division. “The i.MX535 delivers a compelling blend of features,  functionality, performance and energy efficiency that consumer device  manufacturers need to take smart mobile device design to new levels.”

The i.MX535 processor’s rich feature set supports a number of highly  compelling use cases:

  • HD capability with 1080p video decode provides access to HD content  available on popular online video platforms, while duplex video in HD  delivers outstanding video conferencing experiences and supports the  growing media/V2IP market.
  • AdobeRegistered FlashRegistered Player 10.1 is optimized to run on the i.MX535’s  OpenGLRegistered ES graphics engine and H.264 video cores to deliver outstanding  video experiences and long battery life.
  • Integrated LVDS and support for analog TV outputs up to 1080p60 are  ideal for tablets and enable the creation of “next-gen ready” consumer  products that don’t require additional or costly external components.
  • External memory support up to 2GB prepares end devices for cloud  computing applications, as well as future operating systems and  browsers. And improved graphics performance means faster windowing,  accelerated gaming, and more responsive user interfaces.

Optimal code reuse and broad software support
Because the  i.MX535 shares operating system support and multiple peripherals with  the i.MX51, manufacturers can preserve the value of their i.MX51  software investments and simplify code migration to the newer device.  The i.MX535 also enjoys support from a deep pool of software partners.  Many popular operating systems integrate tightly with the processor’s  ARM Cortex-A8 core, including AndroidTm OS, Microsoft WindowsRegistered Embedded  Compact 7, LinuxRegistered OS and ChromiumTm OS.

“Opportunities for OEMs to deliver rich, immersive user experiences  and streamlined connectivity on a range of specialized consumer devices,  such as slates, feature phones and other CIDs, continue to grow,” said  David Wurster, senior product manager for Windows Embedded at Microsoft  Corp. “We are excited to work with Freescale and our entire ecosystem of  global partners to drive differentiated devices that are easy to use  and provide seamless connections to the world of Windows 7-based PCs,  servers and online services through Windows Embedded Compact 7.”

Multicore roadmap
As smart mobile devices evolve to meet  consumer demand for ever-greater performance and energy efficiency,  Freescale is laying the groundwork for next generation multicore i.MX  product families. The company is investing in a new family of single,  dual and many core processors leveraging the very latest core technology  from ARM, Ltd. Optimized specifically for tablets, eReaders and other  select smart mobile device markets, this family of scalable processors  is planned for initial sampling during the first half of 2011.

Exceptional energy efficiency
The i.MX535 has qualified for  the Freescale Energy Efficient Solutions mark, which means it is  designed to offer customers assurance that Freescale has employed the  right combination of technologies and techniques to achieve optimal  energy savings as relevant to a particular application space. The mark  stands for Freescale’s technology expertise in delivering products  optimized for high performance within the constrained energy and power  budgets of embedded environments.

i.MX535 availability and pricing
The i.MX535 processor is  expected to ship in volume quantities in Q1 2011. Pricing and additional  information are available from regional Freescale sales offices. For  more information, visit www.freescale.com/imx535

About Freescale Semiconductor
Freescale Semiconductor is a  global leader in the design and manufacture of embedded semiconductors  for the automotive, consumer, industrial and networking markets. The  privately held company is based in Austin, Texas, and has design,  research and development, manufacturing or sales operations around the  world. www.freescale.com.

  • microprocessor
  • sp:freescale