onsemi
  • Products & Partners
  • Manufacturers
  • onsemi
  • More
  • Cancel
onsemi
Forum Transistor Amp
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join onsemi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Subscribers 11 subscribers
  • Views 4392 views
  • Users 0 members are here
  • transistor
  • guitar
  • amplifier
Related

Transistor Amp

nick123
nick123 over 12 years ago

How can I make a transistor amp that can amplify a electric guitar?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 12 years ago in reply to nick123 +1
    Hi Nick, Yes you could use an LM386 which can give you approximately 1 watt power output. You will also have to build a preamp to drive the LM386 as the voltage from your guitar pickups is fairly low.…
  • D_Hersey
    D_Hersey over 12 years ago +1
    The Zout of an electric guitar is on the order of 30K ohms. Therefore, I would work on a preamp to get me out of this regime, where I could use Plain-Off-The-Shelf tech for the right-hand side of the gain…
Parents
  • jw0752
    0 jw0752 over 12 years ago

    Hi Nick, I found this simple 386 Guitar Amp Project in the Instructables Site. It looks simple and it would give you a start on your project with minimal parts. Here is the link.

     

    http://www.instructables.com/id/Portable-Guitar-or-iPod-Amplifier-Amp-9v-LM3/

     

    Good Luck John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to jw0752

    That's a good link John. I like the second (bridge) circuit best where he uses the FET follower as a high impedance buffer - certainly easier to solder than my TL071 suggestion. The only worry I would have is that the 100uF cap across the supply may not be big enough if a not very good battery/adapter is used as the power source. (Because the high currents through the speaker will modulate the 9V supply and this may upset the input buffer amp. At high frequencies the 100uF will be OK but at bass guitar frequencies (30Hz open B string) the 100uF cap has an impedance of 53R so it's not very low compared with the suggested speaker load of 4 R. 4700uF would feel better to me.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 12 years ago in reply to michaelkellett

    Thanks Michael, You are right as usual. I too have had problems in the past where the draw on my battery would modulate the power to the other sections of my circuit and cause problems. In addition to having a decent size cap on my power supply I have also gotten in the habit of putting a .1 cap Vcc to Vss on any IC I am working with for stability. Nick should be able to put something together from what we have given him.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 12 years ago in reply to michaelkellett

    Thanks Michael, You are right as usual. I too have had problems in the past where the draw on my battery would modulate the power to the other sections of my circuit and cause problems. In addition to having a decent size cap on my power supply I have also gotten in the habit of putting a .1 cap Vcc to Vss on any IC I am working with for stability. Nick should be able to put something together from what we have given him.

    John