onsemi
  • Products & Partners
  • Manufacturers
  • onsemi
  • More
  • Cancel
onsemi
Documents CAT24M01 & CAT24C512 CMOS Serial EEPROM
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join onsemi to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: doctorcdf
  • Date Created: 13 Dec 2011 10:45 AM Date Created
  • Last Updated Last Updated: 13 Dec 2011 10:53 AM
  • Views 2644 views
  • Likes 0 likes
  • Comments 3 comments
Related
Recommended

CAT24M01 & CAT24C512 CMOS Serial EEPROM

CAT24M01: 1 Mb I2C Serial EEPROM

The CAT24M01 is a 1024 kb Serial CMOS EEPROM, internally organized as 131,072 words of 8 bits each. It features a 256−byte page write buffer and supports the Standard (100 kHz), Fast (400 kHz) and Fast−Plus (1 MHz) I2C protocol.
Write operations can be inhibited by taking the WP pin High (this protects the entire memory). External address pins make it possible to address up to four CAT24M01 devices on the same bus.

The CAT24M01 is a 1024 kb Serial CMOS EEPROM, internally organized as 131,072 words of 8 bits each. It features a 256−byte page write buffer and supports the Standard (100 kHz), Fast (400 kHz) and Fast−Plus (1 MHz) I2C protocol. Write operations can be inhibited by taking the WP pin High (this protects the entire memory). External address pins make it possible to address up to four CAT24M01 devices on the same bus.

 

CAT24M01XI-T2CAT24M01XI-T2

 

CAT24C512: 512 kb I2C Serial EEPROM

The CAT24C512 is a 512 kb Serial CMOS EEPROM, internally organized as 65,536 words of 8 bits each. It features a 128−byte page write buffer and supports the Standard (100 kHz), Fast (400 kHz) and Fast−Plus (1 MHz) I2C protocol. Write operations can be inhibited by taking the WP pin High (this protects the entire memory). External address pins make it possible to address up to eight CAT24C512 devices on the same bus.

 

CAT24C512LI-GCAT24C512LI-G

CAT24C512WI-GT3CAT24C512WI-GT3

CAT24C512XI-T2CAT24C512XI-T2

CAT24C512YI-GT3CAT24C512YI-GT3

  • cmos_serial_eeprom
  • EEPROM
  • memory
  • cmos
  • on_semiconductor
  • serial_eeprom
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
  • perigalacticon
    perigalacticon over 10 years ago

    For anyone using ATTINYs with these, specifically the ATTINY85, I modified an EEPROM library that uses TinyWireM to access these EEPROMs from the ATTINY85 that includes a "readNextByte" function that maximizes read data transfer speed with the small I2C buffer available to TinyWireM.  It works perfectly for audio applications for sound bytes sampled at 8kHz.  Just let me know I may have it published on GitHub in a few weeks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • perigalacticon
    perigalacticon over 10 years ago

    Do you know of any good Arduino example code for how to use these?  Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Farnell (Element 14) are supporting good Inventory of ON Semi EEPROM's.... from 1K to 1M in I2C and SPI Bus.