Panasonic
  • Products
  • Manufacturers
  • Panasonic
  • More
  • Cancel
Panasonic
Blog Metal composite inductors - do they make ferrite inductors an anachronism for good?
  • Blog
  • Forum
  • Documents
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Panasonic to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: moritzcehak
  • Date Created: 11 Feb 2021 8:22 PM Date Created
  • Views 2736 views
  • Likes 5 likes
  • Comments 4 comments
  • panasonic industry
  • ferrite
  • inductor
  • metal composite
Related
Recommended

Metal composite inductors - do they make ferrite inductors an anachronism for good?

moritzcehak
moritzcehak
11 Feb 2021

The have been the coil of choice for generations of engineers - despite a number of immanent weak spots: Ferrite inductors. With the rise of metal composite inductors, however, there has finally been a leap in overcoming the disadvantages of this 20th-century technology.

But what exactly are the key differences between these two types of inductors? In the following, we try to answer this question by explaining the different characteristics that emerge from different material and structure, looking at the range of metal composite inductors from Panasonic Industry – one of this technology’s pioneering companies.

The choice for downsizing

Metal composite inductors come with a remarkably higher energy density compared to their ferrite predecessors. This leads to 30% - 50% smaller case sizes which, for example, serves the trend for downsizing high current ECU power circuits. Furthermore, smaller case sizes also have the pleasant side-effect of being less prone to get damaged in harsh or vibrating environments. A true plus in terms of long term reliability.

 

volume to weight ratio

Evolution of DC Bias characteristics

Excellent magnetic saturation characteristics of metal composite inductors (i.e. Ferrite core = 0.4T vs. Metal Composite Type = above 1.5T) render it difficult to magnetically saturate, which in turn is resulting in good inductance vs. current performance, without a substantial drop off. In comparison, ferrite inductors do not only suffer from a fairly quicker inductance drop off. Their inductance also suffers the undesirable effect that it varies with temperature, whereas the performance of their metal composite counterparts is stable over the entire specified temperature range. Naturally, the qualification of applications using ferrite inductors needs increased effort compared to metal composite inductors due to consideration of different temperature ranges.

DC bias characteristics

Robust, qua Natura

Ferrite inductors consist of several sintered parts being constructively composed with an air gap inside the body, whereas metal composite inductors are based on a monolithic design without air gap. Due to that assembled structure, the ferrite types’ resistance to vibrations is limited to <4G to maximum 10G. Opposed to that, the monolithic structure of the Panasonic Industry metal composite inductors leads to a significantly higher vibration resistance - up to 50G, depending on the inductor type.

vibration proof body

Low EMI noise

Also in terms of a lower leakage flux outside the power inductors, the point goes to the metal composite types: Their monolithic structure causes by far less leakage as the magnetic flux simply is concentrated inside the inductor housing.

magnetic flux comparison

To briefly summarize: Modern metal composite inductors clearly outperform the rather archaic ferrite technology in many regards. Hence, they are more and more finding their way into contemporary application design, in particular in the automotive industry.

Small package sizes, a stable inductance over DC current and temperature, high reliability as well as mechanical robustness and not at least a low EMI noise are nowadays essential prerequisites for next-gen product design. In all these aspects, metal composite inductors make their ferrite ancestors look as old as they are indeed: Basically a post-WWII technology that hasn’t been questioned for many years – until Panasonic Industry succeeded in becoming a pioneer for establishing metal composite types as a 21st-century coil of choice, suitable for a vast field of modern designs.

  • Sign in to reply

Top Comments

  • baldengineer
    baldengineer over 5 years ago +3
    Interesting comparison. As always in engineering, there are trade-offs. Certainly, there is some trade-off to use a metal composite inductor. Mechanically, they look denser/smaller than their ferrite cousin…
  • baldengineer
    baldengineer over 5 years ago in reply to Gough Lui +2
    With the right frequency, they can be both! j/k
  • Gough Lui
    Gough Lui over 5 years ago +1
    I suspect you meant "do they make ferrite INDUCTORS an anachronism for good", as I've never heard of a ferrite capacitor before ... - Gough
  • moritzcehak
    moritzcehak over 5 years ago

    Dear James,

     

    You raised an interesting question and indeed as always in engineering there are trade-offs.

    One trade-off is the high frequency behavior. Metal-composite inductors generate higher losses around frequencies above 5 MHz. However, Panasonic for example just recently launched a new series which also is overcoming this weakness, called ETQP***HF* series (see for example Automotive power inductors | Panasonic Industry Europe GmbH). But if it comes above 10MHz, ferrite can keep their performance better due to magnetic characteristic. Currently, this is still a niche-application and we are optimistic to keep track with our development.

     

    Another trade-off is as you mention the pricing: Ferrites are a commodity material with a wide range of suppliers, high availability and an easy manufacturing process. So when you compare the same case size between metal composite and ferrite, you might always find a cheaper version.

     

    However, if you compare the details of the datasheet or specification, you may recognize in many application that using a metal-composite inductor is the better choice because of downsizing, lower leakage and higher efficiency. And in the end the price of an inductor itself has to be seen in the total picture of the PCB layout and  board performance (quality, robustness, performance, space saving, etc.), which a designer must consider in her/his process.

     

    Your sincerely.

    Panasonic team.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 5 years ago in reply to Gough Lui

    With the right frequency, they can be both! j/k

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 5 years ago

    I suspect you meant "do they make ferrite INDUCTORS an anachronism for good", as I've never heard of a ferrite capacitor before ...

     

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 5 years ago

    Interesting comparison. As always in engineering, there are trade-offs. Certainly, there is some trade-off to use a metal composite inductor. Mechanically, they look denser/smaller than their ferrite cousin. Are there any electrical performance trade-offs? (Any cases where ferrite would perform better?)

     

    Or it is a case of cost? (and if that is the case, is it just a matter of time until their volumes are higher so there is even less of a price difference?)

     

    Also, I always wondered about metal composites, how are they manufactured? Is the composite material sintered?

    • Cancel
    • Vote Up +3 Vote Down