Panasonic
  • Products
  • Manufacturers
  • Panasonic
  • More
  • Cancel
Panasonic
Blog Metallized PP Film Capacitors - a closer look on Panasonic Industry's Fuse Function technology
  • Blog
  • Forum
  • Documents
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Panasonic to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: moritzcehak
  • Date Created: 19 Feb 2021 12:47 PM Date Created
  • Views 2577 views
  • Likes 3 likes
  • Comments 0 comments
Related
Recommended

Metallized PP Film Capacitors - a closer look on Panasonic Industry's Fuse Function technology

moritzcehak
moritzcehak
19 Feb 2021

When the talk is about a device’s overall reliability, we know that is first and foremost a question of the components it is consisting of. Next to the ability to withstand rough operational conditions such as vibrations and shocks, it is high voltage stress that can pose a severe risk of damage to components such as capacitors in high power designs – as found in automotive applications, industrial power supplies, DC/DC, AC/DC converters, solar inverters and many more.

In those contexts, high voltage stress cannot be abolished – but there are to avoid overall and fatal product failure: The fuse function is an integral part of the Panasonic Industry Film Capacitor technology which is worth a closer look for everyone designing next-gen high voltage applications.

Film Caps – a brief clarification on the basic principle

Film capacitors, commonly also known as plastic film capacitors, or polymer film capacitors, are electrical capacitors utilizing an insulating plastic film as the dielectric. The dielectric film materials vary depending on required dielectric strength, primarily Polypropylene (PP), Polyester (PET), Polyphenylene sulfide (PPS) etc. The electrodes could be metallized aluminium, zinc or Al-Zn alloy applied directly to the surface of the plastic film. So far concerning the constructive essence.

 

basic principles of metallised polypropylene file capacitor

Film Caps – and the benefits of self-healing

To a certain but remarkable extent, metallized film capacitors have the ability to “repair” themselves. This so-called "self-healing" ability applies when a capacitor with metallized films has the foils exposed to each other due to dielectric breakdown under voltage stress. The combination of the foils’ thinness and the high energy density at the damaged area causes the foils to vaporize - and the capacitor stays in operation. However, when too many of such damaged areas fail in a very short period of time, metallized film capacitors short circuit upon failure. In pursuit of higher safety and higher reliability for most of the industries’ innovations, the market correspondingly shows an increased demand for film capacitors to also open upon failure.

Better safe - with patterned metallization

Responding to this growing demand, Panasonic Industry has developed film capacitors with a specific patterned metallization technology – better known as “fuse function” that emerges from a segmented thin layer of vapour-deposited aluminium.

Those segments isolate the failure caused by overvoltage, therefore the damage is only encapsulated in a few areas of the capacitor. In case too many of those areas fail in a very short period of time, the capacitor will then open in a safe manner.

general and patterned metallisation

A comparison

The difference is apparent: When “treating” dielectric material with high- or overvoltage, the un-patterned version reveals far more severe damage than the patterned fuse function film cap concept from Panasonic Industry.

high voltage stress with fuse

high voltage stress without fuse

To have a closer look, watch our comparison in motion:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

This patterned fuse function should be a core criterion for everyone involved in high voltage application design and looking for the ideal type of capacitor. Or – shortly said: Better patterned than sorry!