Panasonic
  • Products & Partners
  • Manufacturers
  • Panasonic
  • More
  • Cancel
Panasonic
Blog Unlocking the Power of EV Inverters: Panasonic Solutions for Next-Gen Mobility
  • Blog
  • Forum
  • Documents
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Panasonic to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: riyo@panasonic
  • Date Created: 31 Oct 2025 12:51 AM Date Created
  • Views 1154 views
  • Likes 3 likes
  • Comments 2 comments
  • EV inverter components
  • chip resistors for EV
  • automotive capacitors
  • Film Capacitors
  • noise suppression in automotive electronics
  • DC to AC inverter
  • Panasonic electronic components
  • automotive inductors
  • panasonic industry
  • compact inverter design
  • Panasonic automotive electronics
  • automotive communication interface protection
  • Chip Varistors
  • electric vehicle power conversion
  • thermal management in EVs
  • element14 Panasonic
  • Panasonic EV solutions
  • high voltage inverter design
  • Panasonic inverter components
  • DC/DC converter components
  • hybrid aluminum electrolytic capacitors
  • EV motor control
Related
Recommended

Unlocking the Power of EV Inverters: Panasonic Solutions for Next-Gen Mobility

riyo@panasonic
riyo@panasonic
31 Oct 2025
Unlocking the Power of EV Inverters: Panasonic Solutions for Next-Gen Mobility
As electric vehicles (EVs) continue to reshape the automotive landscape, one component plays a pivotal role in driving performance and efficiency: the inverter. This essential device converts direct current (DC) from the battery into alternating current (AC) to power the motor. In this article, we’ll explore the role of inverters in EVs, key design requirements, and how Panasonic’s advanced electronic components are enabling the future of e-mobility.

What Is an EV Inverter?

An inverter is a DC/AC converter that transforms the battery’s direct current into alternating current, which is required by most EV traction motors. Without an inverter, the motor cannot operate. Depending on the vehicle type, one or more inverters may be installed—especially in models with in-wheel motors, where each wheel is powered independently.
Brief description of the inverter

Motor Types and the Need for Inverters

EV motors fall into two main categories:
  • Brush Motors: Simple and cost-effective, these run on DC and are typically used in small devices.
  • Brushless Motors: Preferred for EVs due to their high efficiency and precise speed control. These require AC power, making inverters indispensable.

Features of brush motors and brushless motors


Market Trends: Why High-Performance Inverters Matter

With the rapid adoption of EVs, the demand for high-output inverters is surging. Key trends include:

1. High Power Output

Modern EVs require inverters that can handle voltages up to 800V and large currents. This demands robust semiconductor components capable of managing high power without compromising reliability.

2. Heat Resistance

As components shrink, heat density increases. High thermal resistance is essential to prevent degradation and ensure long-term performance.

3. Compact & Lightweight Design

While power output increases, size and weight must decrease to maintain vehicle efficiency. Panasonic addresses this challenge with miniaturized, high-performance components.

Inside the Inverter: Key Circuit Blocks

An EV inverter is a complex system composed of several critical circuits:
  • Noise Filter: Suppresses internal and external electromagnetic interference.
  • Voltage Measuring Circuit: Monitors input voltage for precise control.
  • Voltage Conversion Circuit: Uses switching elements (e.g., FETs) to convert voltage, with film capacitors and resistors to manage noise and energy discharge.
  • Current Measuring Circuit: Ensures accurate current control.
  • Control Circuit: Coordinates the entire conversion process.
  • DC/DC Converter: Powers the control circuit using hybrid aluminum electrolytic capacitors and automotive-grade inductors.
  • Communication Interface (CAN, Ethernet): Protected by chip varistors to guard against static and noise.

Overall configuration of the inverter


Panasonic’s Component Solutions for EV Inverters

Panasonic Industry offers a comprehensive lineup of components tailored for inverter applications, including:
  • Film Capacitors: Essential for suppressing electromagnetic noise and stabilizing voltage fluctuations.
  • NTC Thermistors: Used for precise temperature monitoring and thermal protection of switching elements.
  • Hybrid Aluminum Electrolytic Capacitors: Deliver stable power in DC/DC converter circuits, ensuring reliable operation under high-load conditions.
  • Power Inductors: Automotive-grade inductors optimized for efficient voltage conversion and noise filtering.
  • Chip Varistors: Provide electrostatic discharge (ESD) protection for communication interfaces such as CAN and Ethernet.
  • Chip Resistors: Crucial for gate control in switching circuits, noise suppression, and energy discharge management. These resistors help stabilize inverter operation and contribute to overall system reliability.
These components are engineered to meet the demands of high power, thermal resilience, and compact design, making them ideal for next-generation EV platforms.

Conclusion: Driving the Future with Panasonic

As EV technology evolves, so too must the components that power it. Panasonic’s advanced solutions for inverters help engineers meet the challenges of high performance, miniaturization, and reliability. Whether you're designing for a compact city EV or a high-performance electric SUV, Panasonic has the components to bring your vision to life.
Point right Explore Panasonic’s inverter-ready components on https://www.element14.com/ and accelerate your EV innovation today.
Component Feature High Voltage Large Current  Low Loss Miniaturization High Heat Resistance High Precision
Film Capacitors High reliability advantage advantage
Conductive Polymer Hybrid Aluminum Electrolytic Capacitor Low ESR
High reliability
advantage advantage advantage advantage advantage
Power Inductor for Automotive Application Large current, low loss
High reliability
advantage advantage advantage advantage
Chip Resistor High precision, high resistance to heat advantage advantage advantage advantage advantage
Chip Varistor Small and light advantage
NTC thermistor Small, high resistance to heat advantage advantage advantage
  • Sign in to reply
  • Sohaib@@
    Sohaib@@ over 1 year ago

    Nice post. Btw I'm also thinking to make an inverter as a project 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Sohaib@@
    Sohaib@@ over 1 year ago

    Nice post. Btw I'm also thinking to make an inverter as a project