Panasonic
  • Products & Partners
  • Manufacturers
  • Panasonic
  • More
  • Cancel
Panasonic
Forum Ask me a question about Solid State Relays?
  • Blog
  • Forum
  • Documents
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Panasonic to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 27 subscribers
  • Views 1200 views
  • Users 0 members are here
  • mosfet
  • cxr
  • testing
  • life
  • optocoupler
  • long
  • low
  • photomos
  • solid
  • optical
  • state
  • ssr
  • relay
  • ate
Related

Ask me a question about Solid State Relays?

e14 Contributor
e14 Contributor over 14 years ago

When to use Solid State Relays vs. Electromechnical Relays?

If faster switching response, no bounce, silent operation and long life are required.

  • Sign in to reply
  • Cancel
Parents
  • Injunear
    0 Injunear over 13 years ago

    Hello,

     

    I don't know if this is the kind of question you are looking for but we are using the International Rectifier

    AUIPS7091 to turn on and off hydraulic valves. The valves draw about half an amp each but sometimes two or three may be temporarily connected to the same output.

     

    I am planning on using the Si8660 to convert a microcontroller 3.3 V 1 mA output to a 5 V signal that will (hopefully) control the 7091.

     

    Do you have any suggestions on any other ways I might use a 3.3 V signal at 1mA or less to control a 24 VDC 2-3 Amp output?

     

    Thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Injunear
    0 Injunear over 13 years ago

    Hello,

     

    I don't know if this is the kind of question you are looking for but we are using the International Rectifier

    AUIPS7091 to turn on and off hydraulic valves. The valves draw about half an amp each but sometimes two or three may be temporarily connected to the same output.

     

    I am planning on using the Si8660 to convert a microcontroller 3.3 V 1 mA output to a 5 V signal that will (hopefully) control the 7091.

     

    Do you have any suggestions on any other ways I might use a 3.3 V signal at 1mA or less to control a 24 VDC 2-3 Amp output?

     

    Thank you.