Rohm Semiconductor
  • Products & Partners
  • Manufacturers
  • Rohm Semiconductor
  • More
  • Cancel
Rohm Semiconductor
Forum UART COMMUNICATION
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Rohm Semiconductor to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 16 subscribers
  • Views 1068 views
  • Users 0 members are here
  • BP35C5-T01
  • rohm
  • Wi-SUN module
  • BP35C5
Related

UART COMMUNICATION

R.Manu
R.Manu over 2 years ago

Hi,

When trying to communicate with BP359C & BP35C5-T01 via UART from STM32F103RCT6 with Echo mode off. When query is sent a response is received, but when "Ip 2001:db8::26" is sent to change the IP address a response is not received. 


Thanks 
Revanth M

  • Sign in to reply
  • Cancel

Top Replies

  • neilp
    neilp over 2 years ago +1 suggested
    Dear Revanth, Thank you for the question, and we trust this provides a suitable response based on details supplied. Commands must begin with a lowercase letter, therefore, sending the following should…
  • neilp
    neilp over 2 years ago in reply to R.Manu +1 verified
    Hi Revanth, Thank you for the question. The module you are operating is working properly. You need to use “ip” command to confirm the configured address. By the way, which buffer are you referring…
Parents
  • neilp
    0 neilp over 2 years ago

    Dear Revanth,

    Thank you for the question, and we trust this provides a suitable response based on details supplied.

    Commands must begin with a lowercase letter, therefore, sending the following should work.

    "ip.2001:db8::26"

    Best regards,

    ROHM Semiconductor

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • R.Manu
    0 R.Manu over 2 years ago in reply to neilp

    Dear Neil,

    The command "ip 2001:db8::26" is sent with echo mode off but still the is not response. But the IP address has changed to "ip 2001:db8::26" this can only be confirmed by sending 2nd command "ip".
    Also is the any buffer available in BP35C5 module?

    Regards 
    Revanth
    +91 7483581847

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • R.Manu
    0 R.Manu over 2 years ago in reply to neilp

    Dear Neil,

    The command "ip 2001:db8::26" is sent with echo mode off but still the is not response. But the IP address has changed to "ip 2001:db8::26" this can only be confirmed by sending 2nd command "ip".
    Also is the any buffer available in BP35C5 module?

    Regards 
    Revanth
    +91 7483581847

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • neilp
    +1 neilp over 2 years ago in reply to R.Manu

    Hi Revanth,

    Thank you for the question.

    The module you are operating is working properly.
    You need to use “ip” command to confirm the configured address.
    By the way, which buffer are you referring to?
    It's not clear what your concern is.

    Kindest regards,

    Neil

    ROHM Semiconductor

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer