STMicroelectronics
  • Products & Partners
  • Manufacturers
  • STMicroelectronics
  • More
  • Cancel
STMicroelectronics
Forum Toolchain options for the STM32VLDISCOVERY - also for Linux
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STMicroelectronics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 26 subscribers
  • Views 628 views
  • Users 0 members are here
Related

Toolchain options for the STM32VLDISCOVERY - also for Linux

e14 Contributor
e14 Contributor over 15 years ago

Hi there,

 

I made a list of the toolchains I'm aware of - also including Linux-compatible options. See it here:

http://embeddednewbie.blogspot.com/2011/01/free-toolchains-for-stm32vldiscovery.html

 

Hope it's of any help!

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Another opensource compiler is FreePascal

     

    Granted, it's not as mature as the other options, since the CortexM3 support still is very young, and the rtl isn't completely finished yet(the interrupt vectors basically aren't defined). But it's a fun and logical platform to use. Logical in the sense that it isn't extremely complicated like most tools for STM32 - or other new 32bit MPUs for that matter - tend to be. I still haven't figured out how the magical directory structure of C files work for STM-FW projects work

     

    Now if only there was an easy way of downloading the generated program using the ST-Link... image

     

    If anyone are interested they can see some instructions on my site(Yes I know it's 103, but it should be almost the sameimage) http://j-software.dk/stm32f103.aspx

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Thanks, I added it to the list!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Nice, thanks