STMicroelectronics
  • Products & Partners
  • Manufacturers
  • STMicroelectronics
  • More
  • Cancel
STMicroelectronics
Forum STM32 development, what to use? Noob
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STMicroelectronics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 27 subscribers
  • Views 1790 views
  • Users 0 members are here
  • frontpage
  • stm32_f0
Related

STM32 development, what to use? Noob

camuyano
camuyano over 10 years ago

I want to start using some STM32 chips, but I do not know where to start.

Specifically I want to work with STM32F0 chips I will be using a cheap development board  STM32F030F4P6STM32F030F4P6 Arm Cortex-M0

I would like to code in Windows, Linux and Mac.

I want to use this chip because it is less than $2 and seems to work with very little support components and have USB support.

 

To simplify please comment on these question.

 

What FREE tools are available to code for STM32F0 boards (any platform)?

What is the most common use tool for this devices?

 

I am totally new to this MCU, normally I use Arduino but I want to get my hands in other non Atmel chips. Just to get more experience and learn.

Any comment is welcome.

  • Sign in to reply
  • Cancel
  • michaelkellett
    0 michaelkellett over 10 years ago

    This is a nice cheap board for STM32F0xx work:

     

    http://www.st.com/web/en/catalog/tools/PF259997

     

    and it comes with a range of free to use development environments:

     

    Supported by wide choice of Integrated Development Environments (IDEs) including IARTm, KeilRegistered, GCC-based IDEs

     

    I recommend the Keil tools as the best for Windows based development - if you insist on working on directly Windows, Mac and Linux then GCC is your only hope and you'll gain yourself a lot of grief trying to get exactly the same environment running directly on all three platforms. Don't bother - use Keil on Windows and run in a VM on Linux or Mac if you must.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • camuyano
    0 camuyano over 10 years ago in reply to michaelkellett

    Thanks. I am planning on building a conference Badge using an STM32F0 chip. If this design get selected a board will be handle to each participant and I wanted to know if there were multiplatform development tools for the badge. I use the Keil and will try to make my design play well with it. Also will test the rest to provide first hand comments about the different development environments to the community. Most participant use at least two operating system but there might be a small group that is Mac only and I like to enable everyone to play with the boards.
    This is the first time I am working with an STM32 (actually boards are in the mail so soon will start) but from my reading seems to be simple enough to have a simple design working very quickly. So any other pointer to reference places about STM32 stuff is welcome.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • camuyano
    0 camuyano over 10 years ago

    As a comment. I now have been playing with STM32F0 MCUs. After trying and trying to make them work on linux I decided to do all my development for now on Windows official tools. Windows compiler just works. On linux I have managed to compile and download code to the MCU, however the simple blink example has not make my led blink. No blinking on linux, easy blink on Windows.

    However for STM8 I did managed to make it compile and work correctly on linux. On the STM32 in linux, I am trying to use the UART bootloader, on STM8 I used the STLink programmer. That may be part of the problem, but I am not that sure. Didn't wanted to risk overriding factory UART boot loader, now that I have a second chip I might give it a shot.

    There seems to be a lot of information for STM32 but is hard to understand for a beginner.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to camuyano

    If you are on Windows the ST CubeMX software package will get you up and running with about the least possible pain although it is not the most efficient (in terms of code size) way of working. The clock support is quite good but you will need to read the reference manual for the chip quite carefully since the MX tool provides you with a very complicated interactive clock tree diagram - great when you know and understand the chip quite well but a bit daunting at the first look.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • camuyano
    0 camuyano over 10 years ago in reply to michaelkellett

    I used the CubeMX to create the project for Keil to make a simple blink. It was useful in terms that I only clicked on the mode for the pin mode and just pasted some extra code on the main for the blink to take place. And yes, it took a lot of time to build a simple blink project. Yes it produces a lot of code, a lot. Until I learn to use another thing this will be my tool.

    Thanks!