STMicroelectronics
  • Products & Partners
  • Manufacturers
  • STMicroelectronics
  • More
  • Cancel
STMicroelectronics
Forum Anyone has STM32F0 SPI eeprom example?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STMicroelectronics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 25 subscribers
  • Views 2000 views
  • Users 0 members are here
  • stm32
  • at93c66a
Related

Anyone has STM32F0 SPI eeprom example?

camuyano
camuyano over 10 years ago

Does anyone has any example using an STM32F0 reading/writing to an external SPI eeprom?

Or code from other MCU using an eeprom AT93C66A?

I am using HAL libraries for SPI communication. My development environment is uVision Keil

 

I want to talk to an external eeprom via SPI and haven't been able to. I do not have experience with SPI that's why this is a general question.

Maybe with some example code I can go into the right direction.

If I cannot resolve my situation I will post a new question with diagrams and code that can be a more detailed question.

  • Sign in to reply
  • Cancel
Parents
  • camuyano
    camuyano over 10 years ago

    I manage to use the eeprom. It was straight forward however difficult to begin with since I had no experience. Also I am not sure if I did test all possible instructions. My code is not well organized but is at
    https://github.com/soynerdito/BSidesBadge2016_firmware/blob/master/Src/main.c in case anyone need a head start. There are a set of libraries that I wrote to ease the pain of writing and reading.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • camuyano
    camuyano over 10 years ago

    I manage to use the eeprom. It was straight forward however difficult to begin with since I had no experience. Also I am not sure if I did test all possible instructions. My code is not well organized but is at
    https://github.com/soynerdito/BSidesBadge2016_firmware/blob/master/Src/main.c in case anyone need a head start. There are a set of libraries that I wrote to ease the pain of writing and reading.