STMicroelectronics
  • Products & Partners
  • Manufacturers
  • STMicroelectronics
  • More
  • Cancel
STMicroelectronics
Documents STMicroelectronics: iNEMO-M1, First 9-axis “brained” System on Board with ST MEMS sensors
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join STMicroelectronics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: WilliamSouplet
  • Date Created: 19 Nov 2013 3:58 PM Date Created
  • Last Updated Last Updated: 19 Nov 2013 4:01 PM
  • Views 1638 views
  • Likes 0 likes
  • Comments 2 comments
Related
Recommended

STMicroelectronics: iNEMO-M1, First 9-axis “brained” System on Board with ST MEMS sensors

iNEMO-M1 is a 9-axis inertial system including ST MEMS sensors with a dedicated software that enhance its integration in embedded applications. It is the first member of System-On-Board family designed for cost-effectiveness and low consumption. Thanks to its wide set of communication peripherals and its extremely reduced dimensions, the iNEMO-M1 is ready to be used and can be directly integrated in a huge variety of advanced motion-based platforms in several application segments.

image

 

image

Features

·         9-axis + 32-bit MCU Module

·         3-axis digital gyroscope

·         6-axis geomagnetic module

·         STM32F103 MCU: WLCSP, ARM 32-bit cortex M3 CPU, 72 MHz,

512 Kbyte Flash, 64 Kbytes RAM

·         Ultra low drop-low noise voltage regulator

·         Flexible interfaces: CAN, USART, SPI and I2C serial interfaces, Full-speed USB 2.0

·         Compact Design: 13x13x2mm, 28 pins

·         Free ADC channels for external inputs

·         iNEMO SW Fusion library

 

Applications

·         9-axis IMU

·         Advanced gesture recognition

·         Robotics and inertial body tracking

·         Augmented / Virtual reality

·         Human Machine Interface

·         Gaming industry

·         Sports & Wellness

·         Physical Therapy & recovery

 

 

iNEMO M1 Development board available

          Discovery-M1: STEVAL-MKI121V1

image

Features

•      A compact “10DoF in one board 35x35 mm2

•      INEMO-M1

•      Integrated pressure sensor LPS331AP

•      USB connector

•      SWD connector for debugging and programming

•      Several power supply options (5V via USB or 2.4V to 3.6V DC via external supply)

•      The extension connector will all INEMO-M1 pins enable building more complex applications by using an extension board

•      User LED and User button

  • inemo-m1
  • 9-axis
  • sensors
  • fusion
  • mems
  • stm32
  • i-nemo
  • stmicroelectronics
  • st
  • inemo
  • module
  • software
  • MEMS and Sensors
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
  • vsluiter
    vsluiter over 12 years ago

    Last time I checked a good and decent SDK was missing. How is that now? It would be nice to see the raw sensor specs aswell. A lot of ST parts have slightly differing part numbers, most have the same Gyro component, but especially the performance of the accelerometer can differ a lot among sensors.

    The LSM3330DLC had the cunning trick of stating that it had a '12-bit Accelerometer values', but if you read between the linesthe output is from an oversampled 8-bit ADC. Still worth its price though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago

    Any initial price number?

     

    DAB