Superior Sensor Technology
  • Products
  • Manufacturers
  • Superior Sensor Technology
  • More
  • Cancel
Superior Sensor Technology
Blog Benefits of Pressure Sensors for Measuring Airflow
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Superior Sensor Technology to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: AnthonyG
  • Date Created: 24 Sep 2025 5:57 PM Date Created
  • Views 468 views
  • Likes 4 likes
  • Comments 1 comment
  • Air Fliter
  • Advanced digital filtering
  • Multi-Range Technology
  • differential pressure sensors
  • HVAC applications
Related
Recommended

Benefits of Pressure Sensors for Measuring Airflow

AnthonyG
AnthonyG
24 Sep 2025
Sketch of a flow measuring device

Applications Requiring Airflow Measurements

Measuring airflow is important for many HVAC, industrial and medical applications. Whether it is ensuring an air conditioning system is running smoothly or a hospital ventilator is providing the right amount of air to the patient, airflow measurements provide critical system feedback. The number of systems that require feedback on airflow measurement is extensive. Here are a few examples of the feedback provided:

  • Air conditioning: notifying of partial airflow blockages, such as through dirty air filters or clogged air ducts
  • Ventilators and Respirators: if the system is pushing too much (or too little) air to the patient
  • Clean and isolation rooms: if non-pure air is entering and contaminating the room
  • Anesthesia, oxygen concentrators, nebulizers: if the right mix of gases is being administered
  • Gas chromatography: if there is a decrease in flow rate signaling potential blockages in the line
  • Automobile engine: measure the air entering the intake system to determine how much fuel to supply to the engine.

image 

Figure 1 – Some Typical Airflow Applications

The most common device for measuring airflow is an airflow sensor. However, in certain scenarios a differential pressure sensor is a better solution. Let’s take a look at the two devices and their unique advantages.

 

Airflow Sensors

An airflow sensor is a device with two pressure ports where air/gas flows from the first port to the second. Inside, there’s a sensing element with a heated surface. As air or gas flows across the sense element, heat is transferred. This creates a thermal imbalance proportional to the flowing mass. Note that the sensor is measuring the mass flow under standard conditions, not the actual volume of gas flowing through it. While most sensors are compensated for the effects of temperature, changes in atmospheric pressure that affect the density of the gas may affect the output. Airflow sensors must also be calibrated for a specific gas mix, as different gases have different thermal characteristics.

Benefits of airflow sensors:

  • As a thermal device, an airflow sensor is more stable at zero flow versus a differential pressure sensor.
  • Airflow sensors have a higher output at low flows, resulting in better resolution at very low flows versus high flows.

Challenges with airflow sensors:

  • Airflow sensor performance can be impacted by contaminants, such as dirt. If dirt enters the sensor, it can impact the resistance and resulting output. Contaminants may also affect the heat transfer to the sensing element, which again would impact the output.
  • Airflow sensors consume anywhere from 5x to 10x more power than differential pressure sensors. This can be critical for lower power and battery-operated devices.
  • Due to the heating element, airflow sensors take much longer time to stabilize on both power-up and during operation. Whereas a differential pressure sensor can stabilize within 1 msec, an airflow sensor can take up to 35 msec. In addition, the frequency response of an airflow sensor can be 10x longer than a differential pressure sensor. These deltas can be result in significant disadvantages in many time critical applications, including medical and high-speed transportation.

image 

Figure 2 – Image of typical airflow sensor

Differential Pressure Sensors

Like a flow sensor, a differential pressure sensor also has two pressure ports. But unlike the flow sensor, there is no gas flow between the two ports of a differential pressure sensor.  Instead, there is a diaphragm between the ports that measures the pressure difference between them. The two pressures to be measured are applied to opposite sides of the diaphragm. The deflection of this diaphragm, either positive or negative to the zero state, determines the difference in pressure.

Differential pressure sensors have many uses and can be used to replace airflow sensors. As with any solution, there are positives and a negative in doing so:

Benefits of differential pressure sensors over airflow sensors:

  • Unlike an airflow sensor, a differential pressure sensor is ‘dead ended’ so the only air/gas flowing into it is a small amount caused by air/gas compression or expansion under pressure. This structure reduces the possibility of contaminants impacting the output to only those cases where the flow through the tubing is completely blocked.
  • A differential pressure sensor’s output is linear over its working range, so its resolution remains consistent at both low and high flows.
  • Differential pressure sensors consume anywhere from 5x to 10x less power than airflow sensors. This can be critical for lower power and battery-operated devices.
  • As discussed above, differential pressure sensors can stabilize as quickly as within 1 msec during power-up and have a frequency response rate that can be up to 10x faster than airflow sensors. These are significant advantages for life critical and time critical applications.

Challenges of differential pressure sensors compared to airflow sensors:

  • Since a differential pressure sensor is not thermal, it is not as stable at zero flow. However, some differential pressure sensors utilize an auto-zero calibration technique that samples the output and corrects it based on thermal effects and drift. 

image 

Figure 3 – Superior’s Differential Pressure Sensor

 

Superior Sensor’s Unique Differential Pressure Sensors

Having an extremely low noise floor, Superior’s differential pressure sensors are ideal for precise air flow measurements. However, the advantages extend beyond the low noise floor. Some of Superior’s NimbleSenseTM architecture application-specific building blocks provide additional value add compared to airflow sensors.

Multi-Range TechnologyTM

Multi-Range technology allows one pressure sensor to operate at maximum performance over several different pressure ranges. Unlike airflow sensors and other differential pressure sensors, Superior’s Multi-Range allows pressure ranges to be changed ‘on the fly’ so that one device in the field can be used to serve multiple purposes. Multi-Range also enables manufacturers to bring product variants to market quickly and reduces inventory costs and product obsolescence since only one SKU needs to be stocked.

Advanced Digital Filtering

One of the biggest impediments to differential pressure sensors is errors caused by noise generated by fans, blowers and other elements. Utilizing an integrated advanced digital filtering technology, Superior’s pressure sensors eliminate the noise created by these factors prior to their reaching the sensor sub-system. Thus, the noise is eliminated before it becomes an error signal that can lead to inaccurate airflow reading.

Position Insensitivity

Superior’s unique dual-die implementation in our 210 models of sensors maintain consistent and highly accurate handheld readings regardless of physical orientation of the end device. Rated with a positional sensitivity to within 0.25 Pa, they are by far the industry leader with respect to position insensitivity.

Fastest Response Times

For time critical applications, the interval it takes the pressure sensor to update its measurement data is vital. The faster you receive updated pressure measurements, the more accurate your output. While user configurable, Superior’s sensors support update rates can be as fast as 1 msec.

Excellent Long-Term Stability

Long-term stability is defined by the maximum change in zero signal and output span signal of a pressure sensor under reference conditions within one year. This value is of greater importance in low pressure ranges as the effect on the signal is stronger. Factors such as temperature and mechanical stress can have negative effects on the long-term stability. Superior has market leading long-term stability measured typically within 0.15% of FSS within the first year.

Low Power Consumption

For handheld and other battery-operated devices, power consumption is another important factor in overall performance. With power consumption as low as 5 mA, Superior’s products will not adversely impact the battery life of even the most sophisticated equipment.

 

Conclusion

While airflow sensors are often used to measure airflow, differential pressure sensors provide several key advantages over them: less susceptibility to contaminants, consistent resolution, lower power consumption, faster stabilization on power-up and more rapid response times. Airflow sensors have a more stable zero, but many differential pressure sensors have auto-zero calibration features that minimize this advantage. 

When looking at differential pressure sensors, Superior Sensor Technology’s products have several unique features and performance benefits for airflow measurement applications:

  1. Industry’s lowest noise floor resulting in highest accuracy
  2. Multi-Range technology enabling one sensor to replace several
  3. Advanced digital filtering to block out external noise before reaching the sensing element
  4. Position insensitivity to eliminate any negative impact of device orientation
  5. Response times and update rates as fast as 1 msec
  6. Excellent long-term stability for consistent output
  7. Very low power consumption for handheld and other battery-operated devices

Major worldwide manufacturers of medical, industrial and HVAC products have entrusted Superior Sensor Technology for their differential pressure sensors needs.  For more detailed information about our various solutions or to learn how we can help improve the performance and reliability of your next product, please contact us.

  • Sign in to reply
  • DAB
    DAB 11 months ago

    I agree, pressure sensors can greatly improve HVAC implementations.

    I have been in buildings where you can physically tell when the system comes on due to pressure changes.