Superior Sensor Technology
  • Products & Partners
  • Manufacturers
  • Superior Sensor Technology
  • More
  • Cancel
Superior Sensor Technology
Blog Calibrating Lab Equipment with Pressure Sensors
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Superior Sensor Technology to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: AnthonyG
  • Date Created: 17 Sep 2026 6:15 PM Date Created
  • Views 85 views
  • Likes 2 likes
  • Comments 0 comments
  • industrial applications
  • differential pressure sensors
  • lab equipment
  • pressure sensors
  • calibration
Related
Recommended

Calibrating Lab Equipment with Pressure Sensors

AnthonyG
AnthonyG
17 Sep 2026
Sketch of lab equiment

The importance of calibrating laboratory equipment

Calibration is the process of adjusting and verifying the accuracy and precision of a measurement instrument or testing equipment. It is a critical component of quality control in scientific research, testing, and manufacturing.

Uncalibrated laboratory equipment can produce inaccurate results, potentially leading to serious consequences. For example, if a medical lab’s equipment is not calibrated correctly, it can lead to incorrect diagnoses or treatment decisions. Similarly, in a manufacturing facility, improperly calibrated equipment can result in faulty products, lower production yields, and material waste.

Calibration ensures laboratory equipment produces reliable, accurate results and helps minimize measurement errors and other uncertainties. By regularly calibrating laboratory equipment, scientists and technicians can be confident that their measurements are precise, which helps ensure the quality of their processes and research results.

To summarize, the importance of calibrating laboratory equipment cannot be overstated. It is essential for producing accurate, reliable data and maintaining the credibility and reputation of scientific research and testing.

The role pressure sensors play in calibrating laboratory equipment

Pressure sensors are important tools in calibrating laboratory equipment. They provide precise, accurate pressure measurements, a key parameter in many laboratory instruments.

The role of pressure sensors in calibrating lab equipment can be summarized as follows:

  1. Verification of Calibration: Pressure sensors can verify the calibration of other laboratory instruments that rely on pressure measurements, such as balances, pipettes, autoclaves, and pressure gauges. By comparing pressure-sensor readings with expected values, users can determine the equipment's accuracy and precision and adjust it as needed.
  2. Monitoring Performance: Pressure sensors can monitor laboratory equipment performance in real time. By measuring pressure changes during experiments, researchers can ensure the equipment is functioning correctly and adjust settings as needed.
  3. Standardization: Pressure sensors can also standardize laboratory equipment and procedures across different laboratories. By using pressure sensors to calibrate instruments and validate results, researchers can ensure that their data is comparable with data obtained from other laboratories.

Balances and Scales: Differential pressure sensors can calibrate laboratory balances and scales that use pressure transducers to measure an object's weight. By placing a known weight on the balance or scale and comparing the pressure reading with the expected value, you can verify accuracy and adjust it if needed.

Pipettes: Pressure sensors can calibrate pipettes, which measure and transfer small volumes of liquid accurately. Pressure sensors measure the force required to expel a certain volume of liquid from the pipette, ensuring the pipette’s precision.

Autoclaves: Pressure sensors can calibrate autoclaves, which sterilize laboratory equipment and materials. By monitoring pressure inside the autoclave during sterilization, pressure sensors verify that the autoclave reaches and maintains the required pressure and temperature for effective sterilization.

In summary, pressure sensors play a critical role in calibrating laboratory equipment. They ensure accurate experimental results and promote standardization (and reproducibility) in scientific research. By using pressure sensors to calibrate laboratory equipment, researchers improve data quality and the validity of experimental results.

Superior Sensor Technology’s Pressure Sensors for Equipment Calibration

Superior Sensors' proprietary NimbleSenseTM architecture is the first system-in-a-sensor integrated platform in the industry. This architecture combines the highest precision and dependability with application-specific features, using a highly differentiated advanced pressure-sensing system and the ability to integrate optional building blocks. Superior’s solutions offer many benefits for calibrating laboratory equipment thanks to the unique technology used in the ND Series.

From 62.5 pascals to 150 psi, the ND Series can measure differential, gage, and absolute pressures, and is perfect for the most demanding lab environments since it has an extended operating temperature range, the lowest noise floor in the industry, and the capacity to accommodate up to seven factory-calibrated pressures in one device.

The ND Series has a stable zero point and extremely high accuracy. Industry-leading non-linearity is typically at 0.05% FSS. The ND Series has 16-bit resolution and a configurable bandwidth filter from 1 Hz to 200 Hz. It also includes an integrated 50/60 Hz notch filter to reduce the effects of power-noise spikes. The ND Series is a superb option for applications demanding the highest level of reliability.

By combining a sophisticated piezoresistive sensing element with amplification, an ADC, a DSP, and a digital interface, the ND Series offers a new level of integration that significantly simplifies design. Advanced digital processing enables new functionality, streamlining system development and manufacturing while increasing product reliability.

The ND Series is more than a pressure sensor; it is a pressure-sensing subsystem that includes optional integrated closed-loop control, advanced digital filtering, and a 3-mode pressure switch.

Three product families make up the ND Series:

  1. The ND Series Low Pressure products are a family of differential/gage pressure sensors that measure pressures from as low as ±62.5 Pa to as high as ±7.5 kPa.
  2. The ND Series Mid Pressure products are a family of differential/gage pressure sensors that measure pressures from as low as ±0.5 psi to as high as ±150 psi.
  3. The ND Series Absolute products are a family of absolute pressure sensors that measure pressures from 15 psia to 150 psia.