Superior Sensor Technology
  • Products & Partners
  • Manufacturers
  • Superior Sensor Technology
  • More
  • Cancel
Superior Sensor Technology
Blog Multi-Range Pressure Sensor Design Choices
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Superior Sensor Technology to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: AnthonyG
  • Date Created: 20 Oct 2026 9:02 PM Date Created
  • Views 38 views
  • Likes 2 likes
  • Comments 0 comments
  • industrial applications
  • medical applications
  • Multi-Range Technology
  • differential pressure sensors
  • HVAC applications
  • pressure sensors
Related
Recommended

Multi-Range Pressure Sensor Design Choices

AnthonyG
AnthonyG
20 Oct 2026
Multi-Range Pressure Sensing Technology

A multi-range pressure sensor can eliminate a familiar design compromise: selecting a narrow span for resolution, then discovering that startup transients, changing operating modes, or future product variants require more headroom. For airflow, filtration, respiratory, and low-pressure industrial measurements, that compromise is costly. It can force separate SKUs, additional calibration effort, host-side scaling logic, or acceptance of noise that hides the signal the system needs to detect.

The better question is not simply whether one sensor can report multiple pressure spans. It is whether every available range delivers calibrated accuracy, useful effective resolution, stable zero performance, and predictable behavior in the actual measurement band. Those capabilities determine whether range flexibility reduces system complexity or merely moves it into firmware.

What a Multi-Range Pressure Sensor Actually Provides

A multi-range pressure sensor supports more than one calibrated full-scale pressure range within a single device. The selected range changes the relationship between physical pressure and the digital output, letting a system optimize the measurement span for its operating conditions without changing hardware.

This is not the same as placing a wide-range sensor in a narrow-range application and applying a different software scale factor. A sensor may survive or measure a broad pressure range, but that doesn't mean its noise floor, accuracy, and offset behavior suit every smaller span within that range. A true multi-range implementation calibrates the available ranges so the system receives specified performance at each selection.

For example, an air-handling controller may need fine differential-pressure resolution across a clean filter, while retaining a larger span for commissioning, fault analysis, or a higher-restriction filter option. A respiratory device may need to measure subtle patient flow conditions in one operating mode and accommodate broader pressure conditions in another. In both cases, a calibrated range selection can preserve sensitivity where it matters without creating a separate sensor design.

Up to eight calibrated ranges in one device can materially simplify an OEM platform strategy. The value is not only fewer components on the approved vendor list. It also enables common electronics, common mechanical interfaces, and a more consistent firmware framework across multiple end-system configurations.

Resolution Depends on Noise, Not Output Bits

A 24-bit digital output does not automatically produce 24 bits of usable pressure information. Electrical noise, MEMS noise, analog signal-chain limitations, external interference, and sampling artifacts all reduce effective resolution. That distinction matters most at low differential pressures, where a few Pascals can represent a meaningful airflow, filter-loading, or leak-detection event.

A multi-range pressure sensor should therefore be evaluated by effective resolution and noise performance at the range that will be used, not by nominal converter resolution alone. If the sensor noise consumes a substantial portion of the application’s smallest required pressure change, switching to a narrower range may not solve the problem. The system will still be unable to distinguish real change from measurement variation.

Superior Sensor Technology addresses this limitation through its NimbleSense System-in-a-Sensor architecture. Rather than leaving critical signal-conditioning functions to a conventional discrete sensor design and the host controller, the architecture integrates MEMS sensing, analog conditioning, anti-aliasing, filtering, and programmable software. This approach is designed to achieve the industry’s lowest noise floor while delivering 24-bit output resolution and approximately 18-bit effective resolution.

That difference becomes operationally visible. Lower noise can identify gradual filter loading earlier, resolve low-flow transitions more reliably, and reduce control-loop hunting caused by unstable feedback. In a medical device, the same measurement integrity supports the pressure and flow signals that influence therapy delivery and clinical monitoring.

Why Internal Sampling and Anti-Aliasing Matter

Range flexibility is only as credible as the sensor’s signal path. Many pressure systems measure slowly changing phenomena, which can lead to the false assumption that sampling behavior doesn't matter. In practice, fans, valves, pumps, motors, switching supplies, and mechanical vibration introduce higher-frequency energy into the measurement system. If that energy is not controlled before digital conversion, it can alias into the pressure band of interest.

Aliased noise is difficult to remove after the fact because it appears as legitimate low-frequency content in the sampled data. Host firmware may add averaging or filtering, but that can increase response time and obscure rapid real events. Simply adding more post-processing won't fix a filter-clog alarm that responds too slowly or a ventilator control signal distorted by noise.

An integrated approach performs anti-aliasing and filtering within the sensor signal chain. With internal sampling from 3 to 12 kHz, depending on configuration, the device can control the measurement bandwidth before presenting pressure data to the host. The result is a cleaner signal and less firmware burden for the system designer.

There is still a trade-off. Stronger filtering can reduce noise but may add latency, while a wider bandwidth may capture faster events but pass more noise. The right configuration depends on the controlled process dynamics, the control-loop rate, and the smallest pressure event that must be resolved. A sensor that makes these parameters configurable gives engineering teams a practical way to tune the measurement system without redesigning the board.

Selecting the Right Ranges for the Application

Start the range-selection process with measured pressure data rather than a nominal system specification. Consider normal operating pressure, startup and shutdown behavior, expected fault conditions, environmental variation, and the pressure drop of new and end-of-life consumables. The required calibrated span often differs from the maximum pressure the sensor must withstand.

For a low-pressure HVAC application, the primary range should place the normal differential-pressure signal high enough in the available measurement span to preserve resolution. A secondary range may provide coverage for commissioning or a high-restriction condition. In industrial automation, the right choice depends on whether the sensor measures steady pneumatic pressure, a transient process event, or a leak trend over hours.

Medical respiratory applications require an additional level of discipline. Pressure range, bidirectional measurement requirements, response time, zero stability, and interface behavior all affect the system-level design and verification plan. A range selection that appears adequate on a bench may not be adequate once tubing compliance, flow restrictions, temperature changes, and control dynamics are included.

When comparing devices, engineers should examine these questions:

  • Are the individual ranges calibrated and specified, or are they merely scaled output modes?
  • What are the noise and effective-resolution figures at each intended range?
  • How does accuracy change across pressure, temperature, and the expected common-mode condition?
  • Is zero drift actively managed during continuous operation?
  • What bandwidth, output data rate, and digital interface options fit the host architecture?

These are not documentation details. They determine whether a flexible sensor produces reliable measurements after deployment, not just favorable lab data.

Zero Stability Is Part of Range Performance

At very low pressures, offset error can dominate the measurement. A small zero shift that is insignificant over a wide pressure span may cause major error in a narrow differential-pressure application. Temperature cycling, package stress, mounting effects, and elapsed operating time can all move the apparent zero point.

For this reason, multi-range capability should be considered alongside continuous zero-drift control. If a system must periodically interrupt operation or depend on a known zero-pressure condition to correct offset, the range flexibility may be less useful in the field. This is particularly relevant in continuously operating air-quality systems, process equipment, and respiratory devices where a convenient recalibration condition may not exist.

An architecture that monitors and corrects zero behavior within the sensor reduces dependence on host-side compensation. It also helps engineers preserve the practical resolution of the narrowest selected range over the product’s operating life. The benefit is not simply a better specification table. It is fewer unexplained offsets, fewer nuisance alarms, and greater confidence that a small reported pressure change reflects a real system change.

One Device Does Not Fit Every Pressure Problem

A multi-range pressure sensor is highly useful when a product has multiple operating modes, configurable airflow paths, regional variants, service states, or a platform strategy that benefits from common hardware. It is less compelling when a single fixed pressure span dominates volume production, and the application doesn't need expanded operating coverage.

Likewise, the lowest available range is not automatically the best selection. If normal pressure excursions regularly approach full scale, the resulting clipping or reduced margin can be more harmful than the resolution gain. The selected range should support the required smallest detectable change while retaining enough headroom for credible operation under real conditions.

The engineering objective is straightforward: choose a sensor architecture that makes the measurement trustworthy at the lowest pressures your system cannot afford to miss. When you design in calibrated range flexibility, low noise, controlled sampling, and zero stability, the pressure measurement becomes a stronger foundation for the entire product.