Superior Sensor Technology
  • Products & Partners
  • Manufacturers
  • Superior Sensor Technology
  • More
  • Cancel
Superior Sensor Technology
Blog Differential Pressure Sensors Gain Intelligence with NimbleSense
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Superior Sensor Technology to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: AnthonyG
  • Date Created: 30 May 2024 5:16 PM Date Created
  • Views 442 views
  • Likes 4 likes
  • Comments 0 comments
  • differential pressure sensors
  • pressure sensors
Related
Recommended

Differential Pressure Sensors Gain Intelligence with NimbleSense

AnthonyG
AnthonyG
30 May 2024
NimbleSense Building Blocks

Background on Differential Pressure Sensors

Measuring the comparative difference between two inputs, differential pressure sensors are a critical part of most mechanical and electromechanical devices that require precise measurement of air, gases, or liquids. For example, if there is a valve in a pipe, a differential pressure sensor will measure the pressure on both sides of the valve. If pressures do not match, then it signals that either the valve is not fully open or there is a potentially serious issue (such as blockage). Differential pressure sensors are a key element in many devices, such as medical ventilators, spirometers, anesthesia devices, industrial flow meters, and HVAC systems.

While some variation of differential pressure sensing has existed for hundreds of years, today’s modern pressure sensors can trace their roots back to the late 1960s when Honeywell applied for the first patents in piezoresistive silicon sensor technology. Over the past decades, the technology has been improved by further integrating electrical and mechanical components manufactured using silicon processes similar to integrated circuits. This process is known as Microelectromechanical Systems or MEMS.

Today’s devices, whether consumer electronics such as smartphones, medical equipment such as respirators, or industrial ventilation systems, have become much more intelligent. But not all components have advanced. Critical to many applications, differential pressure sensors have changed little over the past several decades. This has resulted in product designers having to put together piecemeal solutions that are often not performance-optimized and usually extend product development timelines.

The NimbleSenseTM Architecture

Seeing this deficiency, Superior Sensor Technology created an innovative architecture enabling product designers to move beyond this piecemeal approach to a fully integrated module that combines the MEMS sensor with additional circuitry and software. This modular approach is driven by intelligent programmable software for each end application. We call this architecture NimbleSense, the industry’s first System in a Sensor. This approach is the same as IC designers have used in designing many complex SOCs (System on a Chip) that power today’s smartphones, automobiles, data centers, etc.

Figure 1:  System in a Sensor Block Diagram

image

Using the NimbleSense architecture enables product designers to create highly differentiated advanced pressure sensing systems from a technology toolbox consisting of many building blocks. This methodology greatly improves system performance in the end application while providing enhanced features and cost-optimized manufacturing solutions.

The NimbleSense architecture combines processing intelligence with signal path integration and proprietary algorithms to enable a much simpler system design and a higher level of sensor performance. Choosing from a wide array of proven and tested building blocks, product designers integrate the appropriate modules to create a differential pressure system optimized for the specific application requirements.

These different modules provide significant design flexibility and greatly speed up the time to market. With this system-in-a-sensor approach, a product designer can quickly and easily develop the pressure-sensing solution required in their end product. Introduced in the next section, these NimbleSense architecture building blocks enable a 5- to 10-fold performance improvement as well as a variety of application-specific features.

Technology Building Blocks

Flexibility is at the core of the NimbleSense architecture. This unique technology allows you to quickly prototype and design the sensor into your product, support multiple product lines with one particular sensor, add new capabilities and features via software updates and reduce system cost through lower component count and greater product reliability.

Based heavily on customer feedback, the Superior Sensor Technology engineering team is constantly innovating and introducing new building blocks in the NimbleSense architecture. Here is a listing of the currently available blocks, along with a short explanation of each. 

Multi-RangeTM: Multi-range capability allows a single sensor unit to be factory-calibrated and performance-optimized to support up to 8 different pressure ranges. This feature benefits all our market segments.

Z-TrackTM: Z-Track employs a proprietary algorithm to virtually eliminate zero drift. Zero error reduction is critical in medical devices such as Spirometers, where an inaccurate reading can have life-changing effects.

Closed Loop Control (CLC): CLC adds capabilities within the module to set and maintain flow rates via pressure management by directly controlling motors, valves, and actuators. CLC is of extreme value in medical respiratory devices such as ventilators and CPAP.

Advanced Digital Filtering: Our advanced digital filtering is optimized for each application to ensure mixed sampling noise is kept below the noise floor. By removing the mechanical noise, we maximize overall system performance.

50/60Hz Notch Filter: Superior Sensors’s notch filter allows designers to easily remove noise at either 50Hz or 60Hz that can impact overall system performance. Commonly used in HVAC applications, our integrated notch filter simplifies system design.

Pressure Switch: The integrated pressure switch activates when a certain pressure threshold is reached. It is implemented as a fast failsafe feature for overpressure conditions or other simplified on/off system feedback. The switch includes three modes for setting threshold pressure: one fixed and two variable.