TE Connectivity
  • Products
  • Manufacturers
  • TE Connectivity
  • More
  • Cancel
TE Connectivity
Blog ESD Protection for HDMI
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join TE Connectivity to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: AbhishekRao
  • Date Created: 3 Jun 2011 8:08 AM Date Created
  • Views 845 views
  • Likes 0 likes
  • Comments 0 comments
  • hdmi
  • for
  • protection
  • esd
Related
Recommended

ESD Protection for HDMI

AbhishekRao
AbhishekRao
3 Jun 2011

With an ever increasing demand for high-definition video and audio,  and an explosion in high-def signals, High-Definition Multimedia  Interface (HDMI) has become the de-facto standard in HDTV. HDMI is an  interface that provides a high-speed link between audio/ video source  devices such as notebooks, Blu-ray players and sink devices such as  HDTVs for transmitting uncompressed digital audio/video signals.

The demand for low-cost highly integrated HDMI solutions is  increasing, leading to the increase in number of HDMI chipsets  fabricated in CMOS processes. As the chip geometries have been reduced,  so has the geometric span, making them susceptible to smaller ESD  events, which may lead to system failures.

ESD threats can come from any charged entity such as user’s direct  touch or from hot plugging a charged cable. The internal on-chip ESD  protection mostly provides an immunity of up to +/- 2KV which is not  sufficient to keep the sensitive HDMI chip from becoming damaged.  Effective measures must be taken to diminish the impact of such  transients in order to protect the HDMI chip and prevent any data  corruption between field input and device output.

Signal integrity and electrical performance are critical for  maintaining the quality of HDMI’s GHz signals. Placing ESD protection on  HDMI signals affects the edge rates of high-speed signals and trace  impedances localized to the area of the ESD protection for single-ended  and differential signals. Placing ESD components on high-speed signals  is analogous to placing small capacitors on the signal lines and  introducing parasitic capacitance. In order to minimize their impact on  high-speed signals, it is advisable to have ESD components, for HDMI,  with parasitic capacitance below 1 pF.

In addition to the electrical characteristics requirement, to ensure  maximum reliability for the HDMI IC, the protection device should  provide repeatable ESD immunity to and beyond level 4, IEC 61000-4-2 ESD  to each of the exposed signal pins. In other words, when testing the  I/O or power pin of the HDMI connector, each pin should have a minimum  of ±8kV contact ESD and ±15kV air ESD handling capability.

In conjunction with ESD voltage protection level, another important  parameter to consider is ESD clamping voltage. With the increasing  sensitivity to overvoltage stress in today’s ICs, lowering the ESD  clamping voltage will reduce the risk of being damaged further. Thus, it  is important that the chosen protection device offers the lowest ESD  clamping voltage possible.