TE Connectivity
  • Products & Partners
  • Manufacturers
  • TE Connectivity
  • More
  • Cancel
TE Connectivity
Forum Can any one guide me that how to get internet connection over usb 3g dongle(any) for Raspberry pi?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join TE Connectivity to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 2 answers
  • Subscribers 23 subscribers
  • Views 10924 views
  • Users 0 members are here
Related

Can any one guide me that how to get internet connection over usb 3g dongle(any) for Raspberry pi?

e14 Contributor
e14 Contributor over 10 years ago

I am trying to get internet connection form usb 3g dongle for Raspberry pi 2 B. I have tried with wvdial.conf and usb_modeswitch.conf. I have got ip address from ppp0 but i am not getting internet connection. and even i tried with sakis3g, here also same result and no internet connection. Below i have pasted my configurations. If any one worked on this pleas let me know where i am wrong?

1)

pi@raspberrypi:~ $ lsusb

Bus 001 Device 005: ID 12d1:1436 Huawei Technologies Co., Ltd. E173 3G Modem (modem-mode)

Bus 001 Device 003: ID 0424:ec00 Standard Microsystems Corp. SMSC9512/9514 Fast Ethernet Adapter

Bus 001 Device 002: ID 0424:9514 Standard Microsystems Corp.

Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

 

2)

file : /etc/wvdial.conf

 

[Dialer Defaults]

Modem = /dev/ttyUSB0

Init1 = ATZ

Init2 = ATQ0 V1 E1 S0=0 &C1 &D2 +FCLASS=0

Init3 = AT+CGDCONT=1,"IP","TATA.DOCOMO.INTERNET"

Stupid Mode = 1

Modem Type = Analog Modem

Phone = *99#

ISDN = 0

Username = { }

Password = { }

Baud = 460800

 

3)

pi@raspberrypi:~ $ ifconfig

eth0      Link encap:Ethernet  HWaddr b8:27:eb:46:f5:a0

          inet addr:192.168.2.174  Bcast:192.168.2.255  Mask:255.255.255.0

          inet6 addr: fe80::ba27:ebff:fe46:f5a0/64 Scope:Link

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

          RX packets:21866 errors:0 dropped:0 overruns:0 frame:0

          TX packets:425 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

          RX bytes:1933201 (1.8 MiB)  TX bytes:71065 (69.3 KiB)

 

 

lo        Link encap:Local Loopback

          inet addr:127.0.0.1  Mask:255.0.0.0

          inet6 addr: ::1/128 Scope:Host

          UP LOOPBACK RUNNING  MTU:65536  Metric:1

          RX packets:528 errors:0 dropped:0 overruns:0 frame:0

          TX packets:528 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

          RX bytes:42672 (41.6 KiB)  TX bytes:42672 (41.6 KiB)

 

 

ppp0      Link encap:Point-to-Point Protocol

          inet addr:100.84.67.20  P-t-P:10.64.64.64  Mask:255.255.255.255

          UP POINTOPOINT RUNNING NOARP MULTICAST  MTU:1500  Metric:1

          RX packets:8 errors:0 dropped:0 overruns:0 frame:0

          TX packets:9 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:3

          RX bytes:158 (158.0 B)  TX bytes:221 (221.0 B)

 

 

wwan0     Link encap:Ethernet  HWaddr 02:50:f3:00:00:00

          inet addr:169.254.12.135  Bcast:169.254.255.255  Mask:255.255.0.0

          inet6 addr: fe80::edd:24ae:b709:88d8/64 Scope:Link

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:77 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

          RX bytes:0 (0.0 B)  TX bytes:22395 (21.8 KiB)

 

Any help is appreciated......

 

and what is difference between connecting GSM modem and usb 3g dongle to raspberry pi for internet connection?

  • Sign in to reply
  • Cancel

Top Replies

  • Nate1616
    Nate1616 over 10 years ago +1 suggested
    Mahantesh- Typically a powered usb hub is required for those devices. I know its trivial but have you tried a powered Hub? I had a similar issue in the past with a 3g dongle and it was just not getting…
Parents
  • clem57
    0 clem57 over 10 years ago

    Nate1616is right. I noticed you have eth0 active:

    When I was testing this I realized that you should not be connected to the internet (i.e. via eth0) when modem connection is initiated. For some reason RPi would not get proper DNS even if you disconnect eth0 after you connect with the modem, so: first disconnect your lan cable and then connect.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago

    Nate1616is right. I noticed you have eth0 active:

    When I was testing this I realized that you should not be connected to the internet (i.e. via eth0) when modem connection is initiated. For some reason RPi would not get proper DNS even if you disconnect eth0 after you connect with the modem, so: first disconnect your lan cable and then connect.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer