TE Connectivity
  • Products & Partners
  • Manufacturers
  • TE Connectivity
  • More
  • Cancel
TE Connectivity
Forum Can any one guide me that how to get internet connection over usb 3g dongle(any) for Raspberry pi?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join TE Connectivity to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 2 answers
  • Subscribers 23 subscribers
  • Views 10920 views
  • Users 0 members are here
Related

Can any one guide me that how to get internet connection over usb 3g dongle(any) for Raspberry pi?

e14 Contributor
e14 Contributor over 10 years ago

I am trying to get internet connection form usb 3g dongle for Raspberry pi 2 B. I have tried with wvdial.conf and usb_modeswitch.conf. I have got ip address from ppp0 but i am not getting internet connection. and even i tried with sakis3g, here also same result and no internet connection. Below i have pasted my configurations. If any one worked on this pleas let me know where i am wrong?

1)

pi@raspberrypi:~ $ lsusb

Bus 001 Device 005: ID 12d1:1436 Huawei Technologies Co., Ltd. E173 3G Modem (modem-mode)

Bus 001 Device 003: ID 0424:ec00 Standard Microsystems Corp. SMSC9512/9514 Fast Ethernet Adapter

Bus 001 Device 002: ID 0424:9514 Standard Microsystems Corp.

Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

 

2)

file : /etc/wvdial.conf

 

[Dialer Defaults]

Modem = /dev/ttyUSB0

Init1 = ATZ

Init2 = ATQ0 V1 E1 S0=0 &C1 &D2 +FCLASS=0

Init3 = AT+CGDCONT=1,"IP","TATA.DOCOMO.INTERNET"

Stupid Mode = 1

Modem Type = Analog Modem

Phone = *99#

ISDN = 0

Username = { }

Password = { }

Baud = 460800

 

3)

pi@raspberrypi:~ $ ifconfig

eth0      Link encap:Ethernet  HWaddr b8:27:eb:46:f5:a0

          inet addr:192.168.2.174  Bcast:192.168.2.255  Mask:255.255.255.0

          inet6 addr: fe80::ba27:ebff:fe46:f5a0/64 Scope:Link

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

          RX packets:21866 errors:0 dropped:0 overruns:0 frame:0

          TX packets:425 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

          RX bytes:1933201 (1.8 MiB)  TX bytes:71065 (69.3 KiB)

 

 

lo        Link encap:Local Loopback

          inet addr:127.0.0.1  Mask:255.0.0.0

          inet6 addr: ::1/128 Scope:Host

          UP LOOPBACK RUNNING  MTU:65536  Metric:1

          RX packets:528 errors:0 dropped:0 overruns:0 frame:0

          TX packets:528 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

          RX bytes:42672 (41.6 KiB)  TX bytes:42672 (41.6 KiB)

 

 

ppp0      Link encap:Point-to-Point Protocol

          inet addr:100.84.67.20  P-t-P:10.64.64.64  Mask:255.255.255.255

          UP POINTOPOINT RUNNING NOARP MULTICAST  MTU:1500  Metric:1

          RX packets:8 errors:0 dropped:0 overruns:0 frame:0

          TX packets:9 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:3

          RX bytes:158 (158.0 B)  TX bytes:221 (221.0 B)

 

 

wwan0     Link encap:Ethernet  HWaddr 02:50:f3:00:00:00

          inet addr:169.254.12.135  Bcast:169.254.255.255  Mask:255.255.0.0

          inet6 addr: fe80::edd:24ae:b709:88d8/64 Scope:Link

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:77 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

          RX bytes:0 (0.0 B)  TX bytes:22395 (21.8 KiB)

 

Any help is appreciated......

 

and what is difference between connecting GSM modem and usb 3g dongle to raspberry pi for internet connection?

  • Sign in to reply
  • Cancel

Top Replies

  • Nate1616
    Nate1616 over 10 years ago +1 suggested
    Mahantesh- Typically a powered usb hub is required for those devices. I know its trivial but have you tried a powered Hub? I had a similar issue in the past with a 3g dongle and it was just not getting…
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Sorry i am late to reply.... Fist, thanks for your reply.. As Nate and Clem told i tried with both steps ie, with powered USB hub and without ethernet cable. But still i got same result. and i executed the command "route -n" to check default gateway. There i was getting only ip address for destination  and not for GateWay for ppp0. Will it be a cause for my problem? ??? Do i need to add default gateway for ppp0???

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Sorry i am late to reply.... Fist, thanks for your reply.. As Nate and Clem told i tried with both steps ie, with powered USB hub and without ethernet cable. But still i got same result. and i executed the command "route -n" to check default gateway. There i was getting only ip address for destination  and not for GateWay for ppp0. Will it be a cause for my problem? ??? Do i need to add default gateway for ppp0???