VPG Foil Resistors
  • Products
  • Manufacturers
  • VPG Foil Resistors
  • More
  • Cancel
VPG Foil Resistors
Documents VPG’s New Flip Chip Current Sense Foil Resistors Made in Japan Offer TCR to ±10 ppm/⁰C, Stability to ±0.05%, and Resistance Down To 0.001 Ω
  • Forum
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: DavidGazit
  • Date Created: 19 Sep 2013 10:23 AM Date Created
  • Last Updated Last Updated: 8 Oct 2021 5:48 AM
  • Views 716 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

VPG’s New Flip Chip Current Sense Foil Resistors Made in Japan Offer TCR to ±10 ppm/⁰C, Stability to ±0.05%, and Resistance Down To 0.001 Ω

VPG’s New Flip Chip Current Sense Foil Resistors Made in Japan Offer TCR to ±10 ppm/⁰C, Stability to ±0.05%, and Resistance Down To 0.001 Ω

MALVERN, Pa. — September 18, 2013 — Vishay Precision Group, Inc. (NYSE: VPG) today announced that its Vishay Foil Resistors brand (VFR) has released a new series of high-precision foil surface-mount current sensing flip chip resistors with low TCR down to ±10 ppm/°C from -55°C to +125°C, +25°C ref.; resistance down to 0.001 Ω; and tight tolerances to ±0.5%. Within this series, the RBH model is offered with a four-terminal Kelvin design. While typical current sensing resistors offer load-life stability of 0.5% through a 1000-hour workload, the RB Series provides stability of ±0.05% at 70°C for 2000 hours at rated power and screening options in accordance to MIL-PRF 55342 and MIL-PRF 49465 for enhanced reliability and performance in a range of applications, including precision current measurement.

The RB Series includes the RBD, RBF, and RBH resistors, which offer power ratings of 0.5 W, 1 W, and 1.5 W, respectively, in compact case sizes. The devices feature short time overload of ±0.03% (300 ppm); a voltage coefficient of < 0.1 ppm/V; a non-inductive (< 0.08 μH), non-capacitive design; and a resistance range from 0.001 Ω to 1 Ω.

The RB Series, built on VFR's Bulk MetalRegistered Foil technology and developed by  the company's R&D team in Japan, outperforms all other resistor technologies available today for applications that require high precision and high stability. It provides a low and predictable TCR, excellent load-life stability, and allows for the production of customer-oriented products designed to satisfy challenging and specific technical requirements. The devices' flip chip configuration saves 35% PCB space when compared to a surface-mount chip with wraparound terminations.

"Designers often unnecessarily pay for tighter tolerances than required simply to accommodate the resistance stability shifts they know to be imminent in an application due to the large application-related changes in the components they selected," said  Yuval Hernik, senior director of application engineering for VFR. "Selection of a high-stability component like the RBD, RBF, or RBH  in these applications eliminates the need for shift allowance due to 'planned instability,' and allows the use of looser initial tolerances than would be necessary with resistors based on other technologies. In addition, overall system costs are often reduced further by eliminating the necessity of additional compensating circuitry or temperature-controlling systems.

"We're proud of the unique history of VFR resistors in Japan, the quality resistive devises created in our domestic factory, and the people who work there to provide our customers with the best technical support and short lead times for our standard and customized precision resistor," continued Hernik.

Further information about the RBD, RBF, RBH, and other Vishay Foil Resistors products is available at www.vishayfoilresistors.com. Follow Vishay Foil Resistors at http://twitter.com/foilresistor.

About Vishay Precision Group

Vishay Precision Group (VPG) is an internationally recognized designer, manufacturer and marketer of: components based on its resistive foil technology; sensors; and sensor-based systems specializing in the growing markets of stress, force, weight, pressure, and current measurements. VPG is a market leader of Foil Technology Products, providing ongoing technology innovations in precision foil resistors and foil strain gages, which are the foundation of the Company’s Force Sensors Products and its Weighing and Control Systems. The product portfolio consists of a variety of well-established brand names recognized for precision and quality in the marketplace. To learn more, visit VPG at www.vishaypg.com.

About VPG Foil Resistors

VPG Foil Resistors, a part of Vishay Precision Group (VPG), produces the most precise and stable resistors available. Distinguished by the premier brands Vishay Foil Resistors, Powertron, and Alpha Electronics, the VPG Foil Resistors portfolio includes discrete resistors and resistor networks in surface mount and through-hole (fixed-lead) configurations; customized chip resistor networks; precision trimming potentiometers; and discrete chips for use in hybrid circuits. These devices are used in applications requiring a high degree of precision and stability, such as in medical testing equipment, semiconductor equipment, precision measuring instruments, aerospace, and military applications. To learn more, visit www.vishayfoilresistors.com.

Bulk Metal is a registered trademark of Vishay Precision Group, Inc.

  • Share
  • History