Wago
  • Products & Partners
  • Manufacturers
  • Wago
  • More
  • Cancel
Wago
Blog High-Current Terminal Blocks: Powering the Future of Industry
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wago to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: WAGO_ShannonC
  • Date Created: 12 Sep 2024 2:58 PM Date Created
  • Views 2176 views
  • Likes 5 likes
  • Comments 2 comments
  • electricalengineering
  • engineering
  • electrical engineering
  • wago
Related
Recommended

High-Current Terminal Blocks: Powering the Future of Industry

WAGO_ShannonC
WAGO_ShannonC
12 Sep 2024
In an era where industrial efficiency and sustainability are paramount, the 285 Series POWER CAGE CLAMP terminal blocks by WAGO stand out as a critical innovation. Designed for applications that demand robust power management, these high-current terminal blocks are becoming indispensable across a variety of sectors, including automotive, railway systems, power engineering, and more.
image

The 285 range is screwless, eliminating the need for special tools or extensive cable preparation. This user-friendly design ensures quick and secure connections, accommodating cable sizes up to 35, 50, 95, and 185 mm². These features make the 285 Series not only a reliable choice for current applications but also a future-proof solution as energy demands and technologies evolve.

Diverse Applications Across Industries

The versatility of the 285 Series POWER CAGE CLAMP terminal blocks is evident in their wide range of applications:

Automotive Industry: Ensuring reliable power supply in the assembly and operation of vehicles.

Railway Systems: Supporting the high-current demands of modern railway infrastructure.

Power Engineering: Essential in both renewable energy setups and traditional power plants.

Building Technology: Facilitating power distribution in, factory, and commercial buildings.

Marine and Offshore: Providing stable power solutions in challenging maritime environments.

Mechanical Engineering: Used in energy-intensive machinery like punching machines, presses, and printing machines.

High-current terminal blocks are crucial wherever robust and reliable power connections are needed, making them a staple in industries where WAGO is active.

Market Trends and Future Prospects

The importance of high-current terminal blocks is set to grow as industries evolve. Despite advancements in wireless technology, energy transmission for heavy-duty applications will always require reliable hardware. With the rise of renewable and decentralized energy sources, the demand for efficient power management solutions like the 285 Series POWER CAGE CLAMP is increasing.

Advantages of Aluminium Conductors

While copper has traditionally been the material of choice for electrical conductors, aluminium is gaining traction due to its cost-effectiveness and lighter weight. Aluminium conductors offer several advantages:

Cost Reduction: Aluminium is significantly cheaper than copper, providing substantial cost savings.

Weight: Aluminium wires are up to 60% lighter than their copper counterparts, which is beneficial for applications where weight is a critical factor.

Price Stability: Aluminium prices are more stable than copper, reducing the risk of cost fluctuations in long-term projects.

However, aluminium's lower conductivity and the need for larger wire sizes in confined spaces pose challenges. Special considerations, such as using Al/Cu compression joints, are necessary to mitigate issues like oxidation and material flow over time.

image

Product Features and Innovations

The 285 Series POWER CAGE CLAMP terminal blocks boast features designed for optimal performance in high-current applications:

Energy Management: Combining current transformers and voltage taps for precise energy monitoring and management.

Protection: Safeguarding downstream measuring instruments with secure voltage paths and integrated fuses.

Ease of Installation: Simplified installation process with plug-and-play components suitable for rail mounting.

These features make the 285 Series not only a reliable choice for current applications but also a future-proof solution as energy demands and technologies evolve.

Conclusion

As industries continue to push the boundaries of efficiency and sustainability, the need for reliable power management solutions like the 285 Series POWER CAGE CLAMP terminal blocks becomes ever more critical. With their versatile applications, market relevance, and advanced features, these terminal blocks are poised to play a pivotal role in powering the future of industry. Whether in automotive manufacturing, renewable energy, or building technology, the 285 Series stands as a testament to innovation and reliability in electrical engineering.

Find out more about the WAGO 285 Series: https://www.wago.com/gb/electrical-interconnections/discover-rail-mount-terminal-blocks/high-current-terminal-blocks 

As always, we love to hear your thoughts and opinions in the commentsBlushGreen heart

  • Sign in to reply
  • WAGO_ShannonC
    WAGO_ShannonC over 2 years ago in reply to Umuju

    Good Afternoon Umuju, 

    Thank you for your feedback and for sharing your experiences, I’m glad that many of them are positive. I’d like to help you understand our high current terminals. 

    The largest terminals in the WAGO range, the 285-1185 (DIN rail mount version), will clamp a solid, stranded or fine stranded wire up to 185mm² (350 kcmil). The force exerted on the wire within the cage by the clamping mechanism will not flatten or deform a solid wire of that size, however it will exert the force needed to clamp it securely, ensuring that there is no “hot spot”. The force is determined by the design of the mechanism and the size of the spring and cannot be influenced by the person making the connection. 

    The conductor is installed or removed easily using a hex wrench which slots into the top of the terminal. To release a conductor, insert the tool then twist it in the direction of the arrow on the top of terminal to release the spring pressure. When the spring is fully open, press in the orange button on the side of the terminal to lock it open. The conductor can then be removed. There is no additional pressure exerted onto the conductor to remove it, in fact from the moment the tool is first turned, the pressure is released. The connection is both easy to operate and reliable. 

    The lever on any WAGO terminal should not snap under normal use. Do you remember what type of terminal it was where you had this experience? 

    The housing will not break on any WAGO terminal during connection or disconnection either. When using the WAGO tool operated terminal (the slot type), if the housing is being damaged it is because either the wrong tool is being used or too much force is being exerted. 

    Yes, you are right, it is possible for connections to become loose over time, but not WAGO CAGE CLAMP, Push-In CAGE CLAMP or POWER CAGE CLAMP (as used in our 285 Series) type. The conductor is held in position with a spring rather than a screw so it cannot work loose, does not require maintenance and there is nothing to tighten. The clamp dynamically compensates for conductor deformation due to flow effects of the copper. The spring does not loose its ability to apply the required clamping force and does not require any adjustment at all. And the housing is designed to support the conductors and clamping mechanism for the full life of the terminal, in use and during connection and disconnection. As long as the terminal is stored, operated installed within the specified temperature ranges then it will not suffer any degradation. 

    I hope that my comments have been helpful and that they have given you a better understanding of our terminals. I have Laboratory Test Reports that I can share with you that give more detailed information, please get in contact with us if you wanted to learn more BlushThumbsupGreen heart

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Umuju
    Umuju over 2 years ago

    I’ve had pretty good experiences with your products in low voltage applications, but some of the issues I’ve run into would be compounded by higher current loads. I am curious of the ways this technology can simplify installation and troubleshooting, but I would like to know if/how some of these concerns have been addressed.

    The first concern would be if sufficient force can be applied to the wire when terminating  larger conductors such as a 350 kcmil. Typically, the amount of force necessary to ensure a solid connection will deform the wire and flatten it to the sidewall of the lug. In instances where sufficient force was not applied, the heat generated at the point of termination was enough to melt the insulation on the conductors back to the raceway and caused a short.

    My second concern would be the method for installing or removing the conductors. If sufficient force is being applied to ensure a good connection, greater force would need to be applied to release the tension allowing the conductor to move. My past experience with DIN rail mounted connections has given me doubts as to the ease or reliability of the options available. In using lever type WAGO connectors, I have had the lever used snap on the first attempt to open the block for termination. On screw type mounts, the plastic housing will often try to twist or even break. The slot type releases have similar issues as the housings are affected by the force necessary to release the pressure on the termination. 

    My final question would be of longevity. Over time, connections can become loose. Many companies have employed IR scanning of their equipment to map potential hot-spots and schedule maintenance. While this would require a shutdown, the only cost would be the manpower to tighten the lugs to spec and inspect the conductors for damage. In most cases, this can be accomplished at the time of the IR scan. If the pressure being applied is from a spring, I would be concerned how quickly the spring loses its ability to apply the required pressure and if this is adjustable, or would the full unit need to be replaced to be able to apply the appropriate amount of force. As most of the structure or the units are plastic, would they hold up to not only the force being applied to hold the conductors stable, but also to the force needed to install and remove the conductors? As plastics are exposed to different temperatures, they can become soft and/or brittle. When fluctuating between these states over time, the overall integrity degrades.

    I do like the convenience that WAGO offers with their connections and have been impressed with the improvements I’ve seen, but the issues I have encountered with spring pressure wire connections have limited my willingness to use them in my trade. My largest concern is with the reliability of the connection over time, and I haven’t seen a method of connection that I trust with the higher current demands that require larger wire.