XP Power
  • Products & Partners
  • Manufacturers
  • XP Power
  • More
  • Cancel
XP Power
Forum Ask an XPert -- Questions for the Power Supply Experts
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join XP Power to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 38 replies
  • Subscribers 6 subscribers
  • Views 5584 views
  • Users 0 members are here
  • expert
  • ac_dc
  • power
Related

Ask an XPert -- Questions for the Power Supply Experts

ksmith
ksmith over 17 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Embedded in the element14 Community Embedded group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community

 

Kent Smith

Applicaitons Engineer

XP Power

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 17 years ago

    What might you suggest for the following requirement:

     

    INPUT: 124-240AC

    OUTPUT: +12Vdc and -12Vdc at 3A per side

     

    for an audio amplifier application.  The supply could be external or internal, or a combination thereof.  DC/DC converter, switching supply, linear, etc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ksmith
    ksmith over 16 years ago in reply to e14 Contributor

    Steve,

     

    A dual output AC/DC supply with even split loads like this is not as common as a lot of people think in the OEM market.

     

    In the past we've handled these situations typically in one of three ways.

     

    Option #1 would be to use two single output supplies. For this I would recommend either our ECS45 or ECM40 for the application. The datasheets for each are attached below and more information is available on our website at the links.

     

    Option #2 is to use a triple (or quad) output supply that would have a +/-12V output as well. Typically the extra outputs (like 5V) are needed for some other aspect inside the system so it's actually beneficial to have it.

     

    Option #3 would be to use a higher power 12V unit and then a dc/dc converter to split off the -12V power from the additional +12V power. This may save a bit of space over Option #1, but it's typically more expensive as a 36W dc/dc would typically cost more than a 40W ac/dc supply. Our JCP40 dc/dc converter could be an option for this along with our ECS100 for the main ac/dc supply. Those attachments are below as well.

     

    As usual any of these options could be dependent on other details of your requirement such as thermals, quantities, performance, etc. I would be glad to speak to you in more detail on this if you would like. You can contact me via email at ksmith at xppower.com or you can find your local sales office and speak to a sales person there. The sales offices can be found on our website at: www.xppower.com

     

    Thank-you very much.

     

    Kent Smith

    Attachments:
    imageSF_JCP_060509.pdf
    imageSF_ECS100_040609.pdf
    imageSF_ECS45_060509.pdf
    imageSF_ECM_Series_110609.pdf
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ksmith
    ksmith over 16 years ago in reply to e14 Contributor

    Steve,

     

    A dual output AC/DC supply with even split loads like this is not as common as a lot of people think in the OEM market.

     

    In the past we've handled these situations typically in one of three ways.

     

    Option #1 would be to use two single output supplies. For this I would recommend either our ECS45 or ECM40 for the application. The datasheets for each are attached below and more information is available on our website at the links.

     

    Option #2 is to use a triple (or quad) output supply that would have a +/-12V output as well. Typically the extra outputs (like 5V) are needed for some other aspect inside the system so it's actually beneficial to have it.

     

    Option #3 would be to use a higher power 12V unit and then a dc/dc converter to split off the -12V power from the additional +12V power. This may save a bit of space over Option #1, but it's typically more expensive as a 36W dc/dc would typically cost more than a 40W ac/dc supply. Our JCP40 dc/dc converter could be an option for this along with our ECS100 for the main ac/dc supply. Those attachments are below as well.

     

    As usual any of these options could be dependent on other details of your requirement such as thermals, quantities, performance, etc. I would be glad to speak to you in more detail on this if you would like. You can contact me via email at ksmith at xppower.com or you can find your local sales office and speak to a sales person there. The sales offices can be found on our website at: www.xppower.com

     

    Thank-you very much.

     

    Kent Smith

    Attachments:
    imageSF_JCP_060509.pdf
    imageSF_ECS100_040609.pdf
    imageSF_ECS45_060509.pdf
    imageSF_ECM_Series_110609.pdf