PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Blogs Bad Soldering Practice: Why you need to remove solder flux from your PCB?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: akshayvn
  • Date Created: 16 Mar 2023 5:29 AM Date Created
  • Views 4798 views
  • Likes 9 likes
  • Comments 5 comments
  • electronic
  • electronic workbench
  • pcb
  • PCB Rework
  • solder flux
  • PCBA Repair
  • soldering
  • Printed Circuit Board
Related
Recommended

Bad Soldering Practice: Why you need to remove solder flux from your PCB?

akshayvn
akshayvn
16 Mar 2023
Bad Soldering Practice: Why you need to remove solder flux from your PCB?

INTRODUCTION

Solder flux is a very popular name in electronics industry and known to most of the electronic professionals. Flux is a chemical agent used extensively to ensure smooth flow of solder on the metal joints. The main purpose of using flux however is to remove oxidized metal from the surfaces to be soldered, seal out air thus preventing further oxidation, and by facilitating mixing it improves wetting characteristics of the solder. A chemical agent that aids so much in the process of soldering, what makes it so bad about flux then? Answer: The flux residue.

The flux residue is a flux leftover that is left on PCB after soldering. Apart from the board aesthetics one of the main reason why you should clean flux from your board is that it causes low voltage insulation short that can prevail (if not cleaned) between the pins of an IC where it was applied. Yes, flux left between the pins of an IC (especially the surface-mount devices with QFP, QFN and BGA package) allows leakage current to flow between them producing undesirable outcome. Let's look at this problem in detail.

ROOT CAUSE

Thing many of us don't know,

"Flux is a leaky insulator which can, under various environmental conditions, provide a current path between the conductors where it is present."

A flux on the contact itself doesn't cause the leakage problem. Under elevated ambient temperature, or moisten surrounding or any mechanical stress, they can short out closely spaced conductors. A close picture of an IC pins shown below illustrates how a thin layer of flux residue has settled between the pins which was left uncleaned. An undesired signal was observed on the pins when checked under oscilloscope. Cleaning the residue confirmed the root cause of the failure.

image

fig 1. flux residue providing a weak conductive path between the pins of an IC.

Another thing that occasionally happens with the flux residue is that a few tiny whiskers of solder get trapped in the flux while soldering. And if present in right proportion, it can well provide a conductive path through cooled flux residue.

UNDERSTANDING THE FAILURE MECHANISM

"Flux needs only to be present in trace amount to cause leakage problems."

Although there is a sufficient amount of flux present in the core of the solder wire to get your job done, the technicians (to make their job easy) tend to use additional flux in form of paste or liquid during the rework on the PCB. There is no problem with the use of flux during soldering. What creates problem is the uncleaned soldered area left with the traces of flux. In fact, you might have already invited a trouble in case where rework is done on surface-mount components with a lead pitch of 25 mils or less. Cleaning flux becomes almost impossible working with such fine pitch ICs. Moreover, using cleaning solvents may actually cause flux to migrate into these tricky areas where it cannot be seen.

In another case, where the flux is hygroscopic, becomes slightly conductive within hours after soldering. I don't know the numbers offhand, but in one case of replacing a part on a computer motherboard, a new coin-cell Lithium battery (CR2032) lasted about 3 weeks instead of the usual several years. After cleaning the flux residue, a new battery lasted at least a few years. The above conditions can only conduct a rather low current however, so they may or may not apply to your situation. But you got to take a special care while working with LVDS power supplies on your board, because even a leakage current in uA is sufficient to create nuisance and may damage your component.

GENERAL RECOMMENDATIONS

You should never ignore even the mere presence of the flux on your board. Few things to be taken care of while handling your board:

  1. Use flux in paste form or in the core of the solder where possible. If liquid flux is used, limit it to the smallest amount that will do the job.
  2. Never use 'no-clean' flux in liquid form for any purpose in a cable assembly. Never expect to remove 'no-clean' flux with solvents after soldering or heating (unless you have verified that you can). Remember, 'no-clean' means 'can't clean'!
  3. If you will be removing flux, be sure that solvents drain away from any contact insulator areas of the connector. Never allow solvents or water to drain into connector body. If there is any chance of flux-contaminated solvent wicking into these areas, flush them with fresh solvent.
  4. Trying to remove water-soluble flux with tap water may replace flux contaminants with ionic contaminants in the tap water. Use de-ionized water where possible or distilled water if nothing better is available.

P.S. I choose to write on this topic after retrospecting past course events that I came across while repairing electronic units. Few questions for which I found answer as YES:

1) Have I ever had a circuit where I was sure the flux residue was the cause of the problem?

2) Did cleaning it fixed the problem?

3) Did I ever find a way to prove that?

and that kept my interest on writing this article. Share your thoughts in the comments below to put more light on this topic, if you had faced similar issues with your board.

This article was first published on LinkedIn here -> https://www.linkedin.com/pulse/bad-soldering-practice-why-you-need-remove-solder-flux-nachankar

  • Sign in to reply

Top Comments

  • dougw
    dougw over 3 years ago +2
    Excellent article. We have experienced exactly all of those problems with flux residue, and it is hard to clean it well enough to have no problems. You can clean it to the point where you cannot see it…
  • michaelkellett
    michaelkellett over 3 years ago +1
    Some of this article isn't very well alligned with current practice. No clean fluxes are very widely used in commercial equipment (ie - pretty much everything). No clean fluxes can be removed by water…
  • embeddedguy
    embeddedguy over 3 years ago +1
    Very good write up. I am new to SMD soldering and did not even know how/where to start. Then, I asked some friend who is doing mobile repair work and he insisted me some solder liquid which unfortunately…
  • anniel747
    anniel747 over 3 years ago in reply to embeddedguy

    Steer clear of chinese junk. Is there a datasheet for the Max Gold?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • embeddedguy
    embeddedguy over 3 years ago in reply to embeddedguy

    Here are the things that my friend has suggested me to buy...Wouldn't be interesting if there is guide which explains which thing is best to use when?

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • embeddedguy
    embeddedguy over 3 years ago

    Very good write up. I am new to SMD soldering and did not even know how/where to start. Then, I asked some friend who is doing mobile repair work and he insisted me some solder liquid which unfortunately did not work for my use case. So now I have ordered solder paste online..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 3 years ago

    Some of this article isn't very well alligned with current practice.

    No clean fluxes are very widely used in commercial equipment (ie  - pretty much everything).

    No clean fluxes can be removed by water  + detergent + ultrasonic processes.

    The flux usually comes in solder paste - its part of what makes it paste rather than metal dust.

    There are several different kinds of liquid flux - for hand working you need to use a LOT - and then clean after.

    I agree about tap water.

    And except for special purposes you should always use water based cleaning (with compatible fluxes) (think of the ozone layer and your bank ballance)

    And dry the assembly as soon as its cleaned.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 3 years ago

    Excellent article. We have experienced exactly all of those problems with flux residue, and it is hard to clean it well enough to have no problems. You can clean it to the point where you cannot see it, and it still causes problems (that go away if you clean it even better). In our case it really shows up with low voltage signals in high impedance analog circuits where any leakage has a major influence on the signal voltage.