PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Blogs Creating a Flexible PCB!
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 17 May 2025 3:56 PM Date Created
  • Views 9303 views
  • Likes 13 likes
  • Comments 9 comments
  • kicad
  • pcb
  • flexible pcb
Related
Recommended

Creating a Flexible PCB!

shabaz
shabaz
17 May 2025

Recently, I've decided to give flexible PCBs a go, using the prototype service available from typical PCB manufacturers.

I had my reasons, in particular, it's a great time-saver, because I don't enjoy creating custom cables for off-board connections. Sure the flexible PCB has a price, but the time saving can make up for it, especially if you intend to make more than one prototype (in my case, five will be assembled).

Another good reason is that flexible PCBs take all the strain off main PCBs, if chassis connectors/controls are attached to the flexible PCB instead of a main rigid PCB. 

Thirdly, I found that it eliminated a lot of separate boards and cables; you can replace multiple boards and multiple cables with a single flexible PCB assembly.

The flexible PCBs in the photo below will ultimately form part of an antenna analyzer project; the flexible PCB will connect the rotary user controls to the main rigid PCB.

image

Here's how I went about it.

First off, configure the stackup in KiCad as shown in the screenshot below. It's not essential, but it will make your 3D renders look nice.

image

Next, create the flexible PCB design pretty much the same way as you would create any normal rigid PCB. In my case, I created a one-sided design, to save costs. You can see that I decided to create the copper tracks on the underside (blue). 

I decided to dedicate the top side silkscreen layer (yellow) for board notes. The key information you need to add is some text indicating how thick you want any flex PCB stiffeners to be, and draw outlines of the stiffeners, and draw arrows indicating them very clearly.

The thickness values in the screenshot below are supported by the PCB manufacturer.

image

That's all you need to do in terms of layout in KiCad. You can check the 3D render to see if all is as you expect:

image

image

Once you're happy, generate your Gerber files as usual, but deselect the top copper layer if you're creating just a single layer design as I did.. You could simply remove the top layer Gerber file (and the top mask layer and any other top layers, apart from the top silkscreen which you're using as a notes layer) from the zip file bundle of Gerber files which you submit to the PCB manufacturer. You could even rename the top silkscreen layer filename if desired, but I dont' think that's essential. 

Prior to completing the order, select that you want the manufacture to review the design before proceeding. This is just in case they have any questions.

Then, wait a week or two for the flexible PCBs to arrive!

The photo below shows the stiffener area at the end of the flexible PCB which will attach to the rigid PCB. You can get flat flex sockets from AliExpress, I used 2.54 mm pitch sockets that fit normal SIL header pin layouts.

image

The photo below shows how a rotary switch will fit onto the flexible PCB.

image

In terms of cost, it worked out to £3.60 per flex PCB, in a quantity of 10, including shipping. I think that's easily worth the time saving, if half a dozen or so are to be assembled.

Thanks for reading!

  • Sign in to reply
  • shabaz
    shabaz over 1 year ago in reply to embeddedguy

    Good question, high-speed digital signals over flat flex is normal, so I think it is feasible, something worth investigating for sure, but I don't know of any sources for specific information.

    Admittedly for this project, I kept the RF connectors directly attached to normal rigid PCB, but offloaded the rest of the external interfacing to the flexible PCB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • embeddedguy
    embeddedguy over 1 year ago

    Nice update. I don't think that the flex PCBs are good choice for tracks that require impedance control such as antenna or USB lines. Are they? If could be though, as the chargers of our mobile phones somehow have flexpcb or wires that can bend.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 1 year ago in reply to ralphjy

    Hi! I think a lot of it is down to using interesting techniques, of which I know almost zero, such as S-shaped curves, to allow things to flex even repeatedly. But for a one-time bend (and probably for a no-vibration environment), then I suspect you could even fully crease the material. I don't know enough to provide much insight on this topic unfortunately : (

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 1 year ago

    Looks great!  I'll have to give that a try.  Are there any guidelines on the bend radius of the flex PCB?  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<