PCB Design, Prototyping and Production
  • Products
  • More
PCB Design, Prototyping and Production
PCB Blogs Rosie Learns to Solder
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 17 Apr 2020 3:36 AM Date Created
  • Views 4701 views
  • Likes 20 likes
  • Comments 33 comments
  • blink_led
  • rosie
  • badass women makers and engineers
  • pcb
  • 555 timer
  • badge
  • learn to solder
  • pcb art
Related
Recommended

Rosie Learns to Solder

fmilburn
fmilburn
17 Apr 2020

Learning to solder with this kit is a fun way to obtain a new skill and a great introduction to electronics.  The art in this project is based on the logo used in the current Element14 Women Makers and Engineers Contest.  The Printed Circuit Board (PCB) accepts through hole components and a 555 Timer in astable mode blinks a LED while the iconic Rosie shows how it is done.

image

The following introductory video gives a quick overview.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Creating the Art

 

The original Element14 art is well suited to conversion for PCB art but some modifications were made:

  • Colors were modified to fit the palette available as described below
  • Circuit art was removed
  • Hand and soldering iron were repositioned

 

The method for transferring art to a PCB is described in greater detail in an earlier post located here.  My method uses Photoshop to reduce the colors to the color palette available and KiCad to create a footprint that can be inserted into a PCB design.  The colors available depend on the silk screen color, copper layer, and solder mask.  For example, when OSHPark Purple PCBs are used with ENIG on the copper the color palette is shown below:

image

The colors are broken into layers in Photoshop and then combined and converted into black and white images corresponding to the copper, mask, and silk layers shown at the bottom of the palette.  Next the black and white images are converted into component footprints in KiCad.  An additional manual step to combine the images is required as described in the link.

 

When finished, we have a footprint that can be placed on the PCB.

image

 

The Circuit

 

The circuit consists of a 3V coin cell powering a 555 timer in astable operation blinking a LED.

image

In this mode of operation the values of R1, R2, and C1 determine the frequency with which the LED blinks as well as the time it stays on (duty cycle).  The datasheet shows how to select components for different frequency and duty cycle and there are also calculators available online.  For more information on how the 555 timer works and the many uses there are a number of educational videos in Element14's The Learning Circuit series including this one.

 

To conserve the battery a switch was added so the circuit can be turned off.  The current limiting resistor R3 probably isn't necessary due the internal resistance of the coin cell battery but is good practice.

 

PCB

 

While larger surface mount components are not appreciably harder to hand solder we will start out with through hole.  Besides being a bit easier to solder they also look cool with the art image.  The image below from KiCad shows the layout and circuit tracks. 

image

Red tracks are on the front of the PCB and green tracks on the back.  With the exception of the switch, battery holder, and name space all components and footprints are on the front of the PCB.  The fabricated PCB (unpopulated) is shown below.

image

NOTE:  The PCB has been modified slightly from the photographs above to make soldering easier but doesn't change the circuit or materially change assembly of parts.  The modifications are:

  • Distance between resistor pads was increased slightly
  • New switch DPDT with 2.5 mm pitch used for easier soldering

 

 

Component Bill of Materials

 

SymbolProduct NameManufacturerQuantityBuy KitBuy Kit
BatteryBattery, Coin Cell, Single Cell, 3 V, 2032Varta1Buy NowBuy Now
BT1Battery Retainer Clip, 2032, 20mm, SMTmulticomp1Buy NowBuy Now
C1Multilayer Ceramic Capacitor, 0.1 µF, 50 VVishay1Buy NowBuy Now
C2CERAMIC CAPACITOR 0.01UF, 100V, X7R, 10%, RADIALmulticomp1Buy NowBuy Now
D1LED, Red, Through Hole, 3mm, 20 mA, 1.8 V, 643 nmmulticomp1Buy NowBuy Now
R1METAL FILM RESISTOR, 820KOHM, 250mW, 1%multicomp1Buy NowBuy Now
R2CARBON FILM RESISTOR, 6.8MOHM, 250mW 5%multicomp1Buy NowBuy Now
R3METAL FILM RESISTOR, 180 OHM, 250mW, 1%multicomp1Buy NowBuy Now
SW1Slide Switch, DPDT, On-On, Through Hole, JS Series, 300 mAC&K Components1Buy NowBuy Now
U1IC, TIMER CMOS, DIP8, 555Texas Insturments1Buy NowBuy Now

 

Additional Parts

 

SymbolProduct NameManufacturerQuantity
PCBOSHPark PCB with ArtOSHPark1

 

The components were selected to be commonly available. Substitutions for those shown in the table will generally work subject to the following:

  • 555 Timer DIL 0.1" pitch and works down to 2V
  • Switch DPDT 2.5 mm pitch through hole (see datasheet for C&K JS202011AQNJS202011AQN or Multicomp Pro MCLSS22PMCLSS22P)
  • LEDs 3 mm through hole
  • Resistors L6.3 x D2.5 mm through hole
  • Capacitors 2.5 mm pitch

 

The PCBs in sets of 3 can be ordered from OSHPark at this link and the gerber files can also be downloaded.

 

The following items are required or in some cases are helpful:

  • Temperature controlled soldering iron and stand
  • Lead free solder, e.g. Product LinkProduct Link
  • Safety glasses / eye protection
  • Well ventilated space / fume extraction
  • Well lit, non flammable work surface
  • Side cutters / wire cutters
  • Solder flux (optional)
  • Braided solder wick (optional)
  • Needle nose pliers (optional)
  • Vise or helping hand (optional)
  • Tweezers (optional)
  • Painter's tape (optional)
  • Isopropyl alcohol (optional)
  • Antistatic brush (optional)
  • Multimeter (nice to have when things go wrong)

 

The items labelled optional are optional for the most part until they aren't  image.  If you are teaching beginners bring them if you have them.

 

Soldering the Kit

 

SAFETY FIRST!  There is a safety list here.   Especially observe the following which I commonly see ignored:

  • Always wear eye protection
  • Use lead free solder - It is easier to get a good solder joint with lead based solder but this is project is for a wearable and will be handled.  Lead is especially dangerous for children.
  • Solder in an area with good ventilation and use a fume extractor
  • Do not multitask while holding a soldering iron - put it back in the stand
  • Always wash hands afterwards

 

When teaching children make sure there is adequate oversight for each child.

 

Sandpaper or a file can be used to smooth the edges of the PCB.  Take care to not inhale the dust.  Clean the PCB with alcohol if available.  If solder is not sticking, flux can help.  There is an introduction to soldering on PCBs with through hole components here.

 

The order of assembly is not terribly important for this project as the parts are large and spaced well apart.  However, I soldered the low profile discrete components on the front first. These were followed by the 8 pin DIP IC (555 Timer) and finally the battery holder on the back and the switch.

 

Use the schematic and the color codes on the resistors to place them properly.  Pay close attention to polarity of the LED and the pin placement on the 555 Timer.

image

The anode (positive) is the longer leg on the LED.  The cathode (negative) usually has a flat spot on the side of the case as shown in the photograph.  On the PCB there is a plus sign beside the pad where the LED anode is inserted.  The cathode is inserted into the square pad.

 

The 555 Timer has a circular indentation beside pin 1 (top left in the photo).  On some DIL (dual in-line) packages there may be a scallop shaped indentation at the top of the component next to pin 1.  Make sure to orient the 555 Timer correctly with pin 1 into square pad on this PCB.  A scallop shape next to pin 1 is also shown on the silk screen to illustrate correct orientation.  The photograph at the top of this post shows correct orientation.

 

The pins on the LED will need to be bent 90 degrees to place it horizontal with the PCB before soldering.  C1 has a tiny 104 written on it and C2 has a 103.  Reading the value of the capacitors is sometimes be difficult.  Accordingly it may be helpful to have a multimeter on hand that can read capacitance in case they get mixed up.  The pins on all components can be bent once placed in the PCB to hold them in place while soldering as shown in the photo below.

image

After soldering snip the pins off at an angle just above the solder joint.

 

Before soldering the battery holder put down a small blob of solder on the central negative pad as shown in the photo below.  This will insure good contact with the negative terminal of the battery.

image

Painter's Tape or some other easily removed tape is useful for holding the battery holder down while soldering as shown below.  Failure to do this or to use something like tweezers to hold it in place will result in burned fingers.  I sometimes put solder paste under the tabs but in this case just laid down a good amount of solder in the holes on tabs and it seemed fine.

image

The PCB in these photos is an earlier version and I subsequently selected another switch.  The new switch is a DPDT through hole version that is easier to solder.  It can be placed on the front or back of the PCB - your choice. After soldering and completing all components clean the flux off with alcohol and a brush.  Place the battery in the holder (positive side up) turn on the switch and watch it blink!

image

 

Summary

 

I really like the way this turned out and plan to use it to teach soldering to my two oldest grandchildren this summer.  Note again that the PCB has been revised somewhat from what is shown and new PCBs are on order.  It should be a bit easier to insert resistors into the revised PCB and the 2.5 mm pitch used for the new switch will be easier to solder.  A photo will be posted in the comments upon receipt.

 

Comments and suggestions are always welcome for a project like this which is intended to be educational in nature.  Your experiences that would help newcomers in soldering and assembly would be especially appreciated.

 

Edits

30 Apr 2020:  Added side cutters / wire cutters to the list of needed equipment

 

Useful Links

 

Transferring Art to PCB:  Screaming LM386:  An Audio Amplifier with PCB Art

LM555 Timer Datasheet: http://www.ti.com/lit/ds/symlink/lm555.pdf

The Learning Circuit: The Learning Circuit 67: 555 Timer Project | Flashing LED Headband

Soldering Safety:  University of Cambridge Department of Engineering Health & Safety

Makerspace Article on Soldering:  How to Solder

Order Revised PCB from OSHPark:  Rosie Learns to Solder

  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 6 years ago +6
    Very nicely done, although from the title I was expecting Rosie to be the name your granddaughter who was learning to solder. Just a couple of things I can't let pass without comment though: The American…
  • dougw
    dougw over 6 years ago +5
    Outstanding. Each attempt gets better.
  • fmilburn
    fmilburn over 6 years ago in reply to Fred27 +5
    I knew I shouldn’t have shown the soldering (correctly pronounced, poorly done). For sure some are snipped too close. It would have been even worse if you saw me trying to demonstrate it.
  • Fred27
    Fred27 over 6 years ago

    Very nicely done, although from the title I was expecting Rosie to be the name your granddaughter who was learning to solder.

     

    Just a couple of things I can't let pass without comment though:

    1. The American pronunciation of solder. It's just wrong!
    2. You realise we're now looking very closely at your soldering technique. Those resistors look a little suspect. (No you can't see some of my work.image)
    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 6 years ago in reply to dougw

    Thanks Doug.  I am having fun with these.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 6 years ago

    Outstanding. Each attempt gets better.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
<