PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum KiCad 7 is coming! (and fast!!)
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 163 subscribers
  • Views 5937 views
  • Users 0 members are here
  • kicad
  • schematic capture
  • pcb design
Related

KiCad 7 is coming! (and fast!!)

baldengineer
baldengineer over 3 years ago

kicad 6.99 with version crossed-out and 7.0 added lol

Post from the KiCad Blog: Features Coming to KiCad 7

One of the reasons I recommend KiCad to anyone who wants to make more than one PCB (in their life) is because of how fast it is developing. Compared to any other options, each major release has brought significant functionality AND usability to the tool. Starting with version 5, the minor updates became extremely frequent. With version 6, there was a promise to shorten the major release cycle. And based on the minor release in the 6.0 branch, the team struck a strong balance between fixing bugs and adding quality-of-life improvements. They call it “cherry picking” when adding a feature from the 6.99 (or pre-7.0) branch.

That promise of more frequent major releases appears to be coming true.

  • KiCad 4: November 2015
  • KiCad 5: August 2018
  • KiCad 6: December 2021
  • KiCad 7: January 2023 (est)

This announcement lists some new features and their contributors in KiCad 7.0’s upcoming release. Plus, the announcement hints that the release could be as early as January 2023. Regardless, my bet would be a Q1 release. And oh boy. There are so many things in this update I cannot wait to start using.

I am looking forward to the plugin manager having a (more?) robust update capability, the command line interface (kicad-cli), auto-complete routes (in PCB), and the properties panel (in PCB). Plus, many other minor features.

I’m curious about the database integration that is mentioned in this article. It sounds like the hooks to access an inventory management system. But I’m not sure how adaptable it will be.

Check the announcement post for a complete list and some demos!

Is anyone else watching the KiCad 7 development? What are you excited to see? Or even what do you wish they would work on next?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +2
    I'm mainly looking forward to this (Properties Panel). It's been a limitation that I couldn't simultaneously edit certain things. Now, this will speed it up! The Background Bitmaps will likely delight…
  • baldengineer
    baldengineer over 3 years ago in reply to shabaz +2
    OH! I forgot about the background bitmaps. I'm hoping that will help in reverse engineering existing PCBs. (Well, at least double-layer boards.)
  • baldengineer
    baldengineer over 3 years ago in reply to Andrew J +2
    Yes, copy/paste into sub-sheets works well. There is now a "paste special" to tell KiCad what you want to do with the annotations. That said, each subsheets still has to have unique annotations. If you…
Parents
  • genebren
    genebren over 3 years ago

    I have been following along with the development pf the KiCad for quite some time, as I have for a long time wanted a free and 'living' PCB development environment to replace my licensed copy of Eagle.  It is good to see a promised commitment  to more frequent releases of KiCad.  I will keep sitting on the fence for a while as no matter how much I complain about some of the clunky features of Eagle it is still the fastest way for me to design PCBs (I designed more that 15 PCB this year).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 3 years ago in reply to genebren

    Yeah, I dragged my feet for a very long time to make the switch. Back in 2016, I committed to doing at least three designs in KiCad. Until then, I had probably started 5 or 6 PCBs, got frustrated, and then went back to EAGLE. However, I had been creating schematics using KiCad Schematic for documentation. So, when I made that commitment, I was at least familiar with eeschema and its hotkeys. (Thankfully with v6 those hotkeys are shared better between the two.)

    As I recall, all three were relatively simple designs. Since then, I haven't looked back.

    I looked at EAGLE 9 when it came out and just shrugged. It couldn't really find anything significantly different than EAGLE 6 other than the re-drawn icons.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 3 years ago in reply to baldengineer

    I froze my Eagle License at 7.6.0 which was prior to their move to yearly subscription licensing.  I have been a licensed user since 4.09, having somewhat regularly updating the license as I needed new features or support.  Now I am feeling the need to move on to something else.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 3 years ago in reply to genebren

    Do IT!

    2023 Goal: Make 3 PCBs in KiCad. Slight smile

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • baldengineer
    baldengineer over 3 years ago in reply to genebren

    Do IT!

    2023 Goal: Make 3 PCBs in KiCad. Slight smile