PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum Driving relays..is this acceptable?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 162 subscribers
  • Views 1269 views
  • Users 0 members are here
  • relay circuits
  • pcb design
Related

Driving relays..is this acceptable?

colporteur
colporteur over 3 years ago

image

Is this acceptable? Are there any downsides?

I am looking to drive three 12V relays. My plan is to replace the single relay in the MOSET circuit with the three relays.

  • Sign in to reply
  • Cancel

Top Replies

  • kmikemoo
    kmikemoo over 3 years ago +2
    colporteur I've always been of the belief that placing the anti-spike diodes as close to the inductive spiking coils as possible is desired to minimize what is "felt" by the rest of the circuit. Redundant…
  • dougw
    dougw over 3 years ago +2
    The circuit looks good. As the others mentioned, put a snubber diode on each relay. Ensure the gate voltage provided by the resistor divider is sufficient to saturate the FET at the current it needs to…
  • shabaz
    shabaz over 3 years ago +1
    Hi Sean, You can add as many relays (or any other load) as required, with the circuit as you've shown (or add extra diodes close to the relays as Mike mentions), if the total current consumption is supported…
  • kmikemoo
    kmikemoo over 3 years ago

    colporteur  I've always been of the belief that placing the anti-spike diodes as close to the inductive spiking coils as possible is desired to minimize what is "felt" by the rest of the circuit.  Redundant diodes would only add to the protections.  I have nothing to back this up but the thought that three diodes will dissipate the energy faster than a single diode.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago

    Hi Sean,

    You can add as many relays (or any other load) as required, with the circuit as you've shown (or add extra diodes close to the relays as Mike mentions), if the total current consumption is supported by the MOSFET.

    Flexibility is lost for independent control, which depends on your need. However if (say) there is later found to be too high a surge current for whatever is being powered by the relays, then it's harder to do anything about it.

    Whereas if the relays were separately controlled, then they could be switched on in rapid sequence. It may not apply to your use-case, I'm just mentioning it as something to consider based on whatever you intend to do ultimately with it.

    In summary, it is fine to switch multiple relays with a MOSFET.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago

    The circuit looks good. As the others mentioned, put a snubber diode on each relay. Ensure the gate voltage provided by the resistor divider is sufficient to saturate the FET at the current it needs to drive the relays. (The gate threshold voltage is not enough) R1 shouldn't be too high a resistance because the gate capacitance will slow down turn-on and cause more power to be dissipated in the FET. R1 shouldn't be too low either to protect the VDRIVE from high current while charging the gate capacitance. If there is a lot of drain current, calculate if a heatsink is needed.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago

    Much appreciate the response folks. My electronics knowledge is dusty. Thanks for looking over my shoulder. There are snubber diodes across each relay. I got lazy at midnight to add them to the sketch.