PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum KiCad 7.0.0 Is Here!
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 161 subscribers
  • Views 33507 views
  • Users 0 members are here
  • eda
  • kicad
  • schematic capture
  • kicad 7.0
  • ecad
  • pcb
  • pcb design
Related

KiCad 7.0.0 Is Here!

baldengineer
baldengineer over 3 years ago

game gear schematic drawn in KiCad 7

Just slightly over a year since releasing version 6, the development team has released KiCad 7.0!

Something like 1200 (reported) issues were addressed in this update. And an ASIC-load (get it? instead of boat-load...) of new features. You can start the KiCad 7.0 download here. While that chonker downloads, you can read the full announcement or check out my longer KiCad 7 write-up on the release.

My Favorite Two New Features (so far)

Colorizing nets in the Schematic editor was the last thing I played with before the official release. The above image is my version of the Game Gear schematic. (It's in the Bit Preserve GitHub repo.) To help keep the various buses straight, I assigned the bus and its nets to a custom color. I love using this colorization for address, data, and power rails. It really helps things to pop when looking at the schematic.

My other favorite feature is the properties panel in PCB. As the name implies, it brings the properties of an element to the top of the UI. First, it saves you from having to "edit" a footprint to adjust its settings. And second, it lets you group multiple similar elements together and change common properties. So, for example, you can grab multiple graphic elements and move them to a different layer without opening any other dialogs!

So, those were the two stand-out features that I really liked. But there are so many more.

Have you used it yet? If so, what do you like (or not like!) about KiCad 7.0?

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 3 years ago in reply to baldengineer +4
    who will make the first Comic Sans board?
  • shabaz
    shabaz over 3 years ago +3
    I decided to edit a KiCad 6.0 version board with version 7.0, and happened to use the font capability. The font here looked too informal, so I reverted back to the KiCad standard font after this screenshot…
  • shabaz
    shabaz over 3 years ago +3
    I tried the Pack-and-Move ('P' key) on an older Kicad 6 schematic. It's going to save a HUGE amount of time!
Parents
  • shabaz
    shabaz over 3 years ago

    I decided to edit a KiCad 6.0 version board with version 7.0, and happened to use the font capability. The font here looked too informal, so I reverted back to the KiCad standard font after this screenshot was taken! 

    However the inverse print (knockout) feature was super-useful! 

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 3 years ago in reply to shabaz

    The knockouts look great and draw your eye to them.

    I will respectfully disagree on the fonts looking informal.

    It gives the board a bit of visual hierarchy. The subtle difference means it is more obvious you should read that text. Versus, say, the reference designators which you can visually filter out because of their font. At least, until you need them.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • baldengineer
    baldengineer over 3 years ago in reply to shabaz

    The knockouts look great and draw your eye to them.

    I will respectfully disagree on the fonts looking informal.

    It gives the board a bit of visual hierarchy. The subtle difference means it is more obvious you should read that text. Versus, say, the reference designators which you can visually filter out because of their font. At least, until you need them.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to baldengineer

    who will make the first Comic Sans board?

    • Cancel
    • Vote Up +4 Vote Down