PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum Breaking out pins on a 2.54 header
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 159 subscribers
  • Views 1466 views
  • Users 0 members are here
  • pcb trace
  • PCB routing
  • pcb design
Related

Breaking out pins on a 2.54 header

colporteur
colporteur over 3 years ago

image

I'm tight for space on a PCB I am designing and was going to use the space between the pin pads to route traces. Can this be done using KiCad? If yes, could you provide some insight into the setup?

I have seen PCB that route traces between pins on headers. I have no experience doing this mainly because I'm old. When this was done many years ago the traces were never reliable when they etched. That has all changed since the 80's. I now see traces routed between pins. I would like to use this technique in a board I am designing. I'm hoping someone who has hoed the row, would share the setup for KiCad that makes it successful.

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 3 years ago +5
    I'm worming through 2.54 header pins in this KiCad design ( Programmable Electronic Load ): I didn't have issues to do that. I can share the project if that helps.
  • shabaz
    shabaz over 3 years ago +5
    Hi Sean, Jan's screenshot shows you can easily route a trace reliably between pads. There are some settings of trace widths (and other settings) screenshots here: (+) KiCad 6 Unofficial Quick Start…
  • ggabe
    ggabe over 3 years ago +1
    You can go right in the middle as well - just adjust the grid (or the secondary grid) so that it will have one in the midpoint. It's perfectly OK not to cross in the middle, for me it's a visual standard…
Parents
  • ggabe
    ggabe over 3 years ago

    You can go right in the middle as well - just adjust the grid (or the secondary grid) so that it will have one in the midpoint. It's perfectly OK not to cross in the middle, for me it's a visual standard I used to apply on my work. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ggabe
    ggabe over 3 years ago

    You can go right in the middle as well - just adjust the grid (or the secondary grid) so that it will have one in the midpoint. It's perfectly OK not to cross in the middle, for me it's a visual standard I used to apply on my work.