PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum How to merge two KiCad 7.x PCB circuits into one
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 160 subscribers
  • Views 5256 views
  • Users 0 members are here
  • kicad 7
  • pcb design
Related

How to merge two KiCad 7.x PCB circuits into one

colporteur
colporteur over 2 years ago

What is your technique for combining two KiCad  projects into one?

I'm trying to develop some skill in KiCad  7, for combining the schematic and PCB of two completed projects into one. I've a small power supply circuit I would like to reuse in other projects. I was hoping to copy and paste the details into an existing project thereby avoiding some overhead. I wouldn't have to draw the schematic and I wouldn't have to layout the components on the PCB.

I've become frustrated and am thinking the best approach is to start from scratch each time. That seem so inefficient. Maybe you have project starting points as a template to begin with no a project.  I've little over a year in KiCad so an expert I am not. I was hoping to draw on some experience of the members who have a strong grasp of KiCad. I just like to become more efficient. Starting from scratch is so boring.

Any suggestions KiCad aficionados? 

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago +2
    Hi Sean, I've not tried to reuse portions of a PCB layout, but, there's a good feature in KiCad 7 to at least speed up the PCB portion, especially for modular bits of functionality. It is called 'Pack…
  • baldengineer
    baldengineer over 2 years ago +1
    Schematics are easily copied/pasted between KiCad instances. I've done it multiple times. Just be aware that Edit -> Paste Special gives you some control over how to handle the reference designators. …
  • mayermakes
    mayermakes over 2 years ago

    I make templates for some project that might come in handy later (actual kicad templates) for example for the Sudosom (ESp32 Linux module in the style of a Cm4) I made a template for the connectors and board shape as well as Sub sheets for all the sections.
    In case its about a specific design  for example a power supply that gets reused over and over I copy paste them in to new projects.on schematic and board level.
    whenever I need them I just copy paste them from the projects into my new current work.
    BUT BE AWARE: always copy the reused parts in first on both levels and make sure to not reenumerate the components in your design! this would mess up the matching between schematic and board level and you would have to rearange/route on the pcb level again.

    there is at this point no dedicate "module" approach for kicad but i think this is a frequent request to the devs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 2 years ago

    Schematics are easily copied/pasted between KiCad instances. I've done it multiple times. Just be aware that Edit -> Paste Special gives you some control over how to handle the reference designators.

    image

    So, if you give your "modules" very unique reference designators, then you could copy/paste the schematic with "Keep existing" followed by a copy/paste of the PCB section.

    You would need to then re-link the two together. That is done with the Tools -> Update PCB from Schematic (also the F8 hotkey).

    image

    This would be one of the very few cases where you'd want to use the "Re-link footprints..." option. (otherwise, that should not be checked!) As the name implies, it'll re-link elements in the schematic and PCB using the reference designator instead of an internal id that KiCad assigns.

    To be upfront, this is all theory on my side. While I regularly copy/paste Schematic blocks (letting KiCad auto-assign new designators), I haven't tried to do the same with re-usable blocks or PCB elements.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mayermakes
    mayermakes over 2 years ago in reply to baldengineer

    while I do copy regularly on the schematic side, apart form a few cases I usually do the pcb level layout routing fresh each time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 2 years ago in reply to mayermakes

    Same. It always seems like there is some constraint that makes me need to re-do it anyway.

    I guess it would be different if I didn't care about the size of the PCBs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mayermakes
    mayermakes over 2 years ago in reply to baldengineer

    my main constraint is that with every time I do I get better at routing/placing that design. so each time I reuse a circuit it also gets a bit better layed out.
    the gains might diminish over time....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago

    Hi Sean,

    I've not tried to reuse portions of a PCB layout, but, there's a good feature in KiCad 7 to at least speed up the PCB portion, especially for modular bits of functionality.

    It is called 'Pack and Move'. The way it works, is in the schematic, drag to highlight in a box selection around all the parts that make up the portion that (say) you've copy-pasted from a different project.

    Then, in the PCB editor, you'll see that all those parts are highlighted. Now press 'P' and it will group all those parts together, so you can quickly drop them on a PCB somewhere and then tweak their positions and lay out the traces as usual, etc.

    It's a time-saver for having bits of circuitry easily positioned together on a PCB. Not quite what you asked for, but speeds up the task that perhaps raised the question.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 2 years ago

    I use Ctrl + C and Ctrl + V when making stencils for multiple PCBs. It most probably is not the right way, but it works.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 2 years ago in reply to mayermakes

    I confess I have discovered myself the design improvements that come from a wash-rinse-repeat cycle.

    I get some satisfaction from working the schematic but find the PCB layout arduous.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 2 years ago in reply to colporteur

    I am the opposite!

    I detest the schematic side but enjoy the puzzle and challenge of making a good layout.