PCB Design, Prototyping and Production
  • Products
  • More
PCB Design, Prototyping and Production
PCB Forum KiCad 8 is here!
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 32 replies
  • Subscribers 135 subscribers
  • Views 6960 views
  • Users 0 members are here
  • kicad 8
  • kicad
Related

KiCad 8 is here!

shabaz
shabaz over 1 year ago

Installing KiCad 8 went smoothly.

First off, I went to my KiCad project folder (e.g. C:\KICAD_PROJECTS), and made a backup copy of it. Then, I installed KiCad 8. At the prompt,I chose to import settings from KiCad 7:

image

It started up just fine, with my previously opened project all ready for me in the new KiCad 8.

image

After that, I went to my old KiCad folder in C:\users (C:\users\shabaz\Documents\KiCad\7.0) and copied everything there to C:\users\shabaz\Documents\KiCad\8.0.

Clicking on Symbol Editor or Footprint Editor will bring up a prompt. I selected the default:

image

When in the Symbol or Footprint editors, the default KiCad libraries will be there, but any user-created ones won't be. I clicked on File->Add Library and navigated to C:\users\shabaz\Documents\KiCad\8.0\symbols or \footprints respectively, and selected my user library and it got added.

I've not tried much so far, but very happy that this feature is available:

image

The above will speed up footprint creation/editing a lot. It is a feature that was sorely missing, it should have been added years ago.

I don't know if the 'teardrops' feature is new, but I've only noticed it now in KiCad 8:

image

I'm looking forward to exploring more in the next few weeks (I will use KiCad 8 unless I hit any showstopper; I still have KiCad 7 and KiCad 6 installed, I think it's time to remove v6!).

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 1 year ago +6
    baldengineer posted a top-8 of new features on his youtube channel . I endorse that message .
  • baldengineer
    baldengineer over 1 year ago in reply to genebren +4
    For what it is worth, the last time I used Eagle was in 2015. I've done about 50 PCBs since then. Granted, most of them were small breakout boards. However, since then, I have not found a single case where…
  • shabaz
    shabaz over 1 year ago in reply to BigG +3
    A bit clunky using it, but eventually got a simple circuit working. This was with a op-amp SPICE file pulled from the web. In short, it all majorly revolves around two main points: (1). In the symbol…
Parents
  • Jan Cumps
    Jan Cumps over 1 year ago

    I'm installing it today. Also a good excuse to start designing some circuits.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 1 year ago in reply to Jan Cumps

    I've used it a bit so far, raised a couple of bugs (one crash) but generally it seems fine. I found I couldn't align parts on the PCB as easy as before, it sometimes wouldn't select the pad center (and instead would snap to the grid) when grabbing and moving components, but that may be a config setting, either new or something that didn't migrate properly from existing config. I didn't look in detail. I'll investigate a bit more to get to the bottom of that next time I try it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 1 year ago in reply to Jan Cumps

    I've used it a bit so far, raised a couple of bugs (one crash) but generally it seems fine. I found I couldn't align parts on the PCB as easy as before, it sometimes wouldn't select the pad center (and instead would snap to the grid) when grabbing and moving components, but that may be a config setting, either new or something that didn't migrate properly from existing config. I didn't look in detail. I'll investigate a bit more to get to the bottom of that next time I try it.