PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum KiCad 8 is here!
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 32 replies
  • Subscribers 160 subscribers
  • Views 8415 views
  • Users 0 members are here
  • kicad 8
  • kicad
Related

KiCad 8 is here!

shabaz
shabaz over 2 years ago

Installing KiCad 8 went smoothly.

First off, I went to my KiCad project folder (e.g. C:\KICAD_PROJECTS), and made a backup copy of it. Then, I installed KiCad 8. At the prompt,I chose to import settings from KiCad 7:

image

It started up just fine, with my previously opened project all ready for me in the new KiCad 8.

image

After that, I went to my old KiCad folder in C:\users (C:\users\shabaz\Documents\KiCad\7.0) and copied everything there to C:\users\shabaz\Documents\KiCad\8.0.

Clicking on Symbol Editor or Footprint Editor will bring up a prompt. I selected the default:

image

When in the Symbol or Footprint editors, the default KiCad libraries will be there, but any user-created ones won't be. I clicked on File->Add Library and navigated to C:\users\shabaz\Documents\KiCad\8.0\symbols or \footprints respectively, and selected my user library and it got added.

I've not tried much so far, but very happy that this feature is available:

image

The above will speed up footprint creation/editing a lot. It is a feature that was sorely missing, it should have been added years ago.

I don't know if the 'teardrops' feature is new, but I've only noticed it now in KiCad 8:

image

I'm looking forward to exploring more in the next few weeks (I will use KiCad 8 unless I hit any showstopper; I still have KiCad 7 and KiCad 6 installed, I think it's time to remove v6!).

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 2 years ago +6
    baldengineer posted a top-8 of new features on his youtube channel . I endorse that message .
  • baldengineer
    baldengineer over 2 years ago in reply to genebren +4
    For what it is worth, the last time I used Eagle was in 2015. I've done about 50 PCBs since then. Granted, most of them were small breakout boards. However, since then, I have not found a single case where…
  • shabaz
    shabaz over 2 years ago in reply to BigG +3
    A bit clunky using it, but eventually got a simple circuit working. This was with a op-amp SPICE file pulled from the web. In short, it all majorly revolves around two main points: (1). In the symbol…
Parents
  • Jan Cumps
    Jan Cumps over 2 years ago

    I've been playing with the symbol editor a little.

    I needed a symbol for the ROHM US6MS. It's a complementary MOSFET pair. Rohm's datasheet symbol:

    image
    source: datasheet

    I could have used one of the existing complementary FET symbols and start from there (I may do that later).

    What I did this time, is find the closest resemblance for symbol and package in Snapmagic: a US64K4. That MOSFET pair, also from ROHM, shares the same package, but it's 2 N-CHANNELs.

    I imported the symbol, then saved it as US6MS. I flipped and moved some triangles to make one of the FETS (and its body diode) become P-CHANNEL:

    image

    Good for now. Although I prefer the approach of some other symbols that use Unit A and Unit B. Gives more flex to place them at will on the schematic.

    To make my current footprint fit on my schematic, I first placed it, then edited the "schematic local" symbol:

    image

    I rotated one of the FETs and placed it under the other one. And put a rectangle around the whole to indicate it's one component.

    Probably too much hassle. I may go for the Unit A + Unit B type. In that case, the labels would be Q1A Q1B, Q2A, Q2B. And I wouldn't need to customise the symbol ...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Jan Cumps

    I redid it, with Unit A and B.

    Symbols:

    image image

    Schematic:

    image

    Definitely easier to handle. And the Q*A + Q*B make it clear enough that it's one package. 

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Jan Cumps

    I redid it, with Unit A and B.

    Symbols:

    image image

    Schematic:

    image

    Definitely easier to handle. And the Q*A + Q*B make it clear enough that it's one package. 

    • Cancel
    • Vote Up +3 Vote Down