PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum KiCAD 8: alternative pin functions
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 158 subscribers
  • Views 5313 views
  • Users 0 members are here
  • kicad 8
  • kicad
Related

KiCAD 8: alternative pin functions

Jan Cumps
Jan Cumps over 2 years ago

I tried KiCAD's (not so) new alternative pin functions option in  the library editor.

I'm designing a project with a Renesas controller. There wasn't a symbol yet, so I started to create one. The majority of the mcu's pins have more than 5 functions. I figured this would be a good candidate to test the new option.

image

Here's the definition in the editor:

image

And a schematic with 3 symbols placed, with a few pins showing different functions.

image

I've attached the symbols: MCU_RENESAS_R_20240323_3.zip

It's a bit of work to get this set up, but it works well. Thoughts?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago +4
    Very interesting! For sure it will simplify many circuit layouts. I'm looking forward to using it. I have not used that so far, but I think I would be super-tempted during symbol creation, to add one…
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to shabaz +2
    I was tempted to do that for a few pins. The same that have multiple functions in the datasheet (43, 44, 47, 48) But what choice do you make as a symbol designer. It 'll always be the wrong one.…
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to shabaz +2
    ... and I've also been playing with alternatives. Below a functionally-split-up one, and two with all in one symbol the U1 has a separate block for analogue, digital and power.
  • HKPhysicist
    HKPhysicist over 2 years ago

    Is this a circuit simulation or just a schematic?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago

    Very interesting! For sure it will simplify many circuit layouts. I'm looking forward to using it.

    I have not used that so far, but I think I would be super-tempted during symbol creation, to add one more alternative pin function, which would be the names of a few of the alternate pin functions (not all)  combined with '/' separators, simply because initially one might not have decided during the first part of schematic entry, which of the alternatives they would be using.

    In other words, the user might want a pin displayed as "PD5/TIMR1/SCL" until they have later refined the selection.

    In the past, what I've done during symbol creation for microcontrollers, is to create function names of a few of the most interesting alternative pin functions, but not all of them. 

    Example:

    image

    image

    Having said that, for each project sometimes the symbols need tweaking too, e.g. to move some of the pins around, or to reduce the size of the symbol etc, since some alternative function names are long, or to change from "bidirectional" to "input", etc. (EDIT: just saw that the alternative pin functions do have that direction property alongside them - perfect).

    But this new feature is really excellent, it will make life a lot simpler.

    Also, a bit unrelated, but touching on the direction thing..

    Maybe this is unorthodox, but I took to creating an arrow symbol, and sometimes add it to schematics to remind myself of the direction of a few interesting signals. I know it shouldn't really be necessary, but might be a handy thing for occasional use, to go along with general annotation, etc.

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to HKPhysicist

    KiCAD 8 Symbol editor and Schematic editor. No simulation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to shabaz

    I was tempted to do that for a few pins. The same that have multiple functions in the datasheet (43, 44, 47, 48)

    image

    But what choice do you make as a symbol designer. It 'll always be the wrong one.

    Suggestion (mine), is to use the default value if it's uncommitted yet. Or create a custom symbol?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to shabaz

    ... and I've also been playing with alternatives. Below a functionally-split-up one, and two with all in one symbol

    image

    the U1 has a separate block for analogue, digital and power.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago
    shabaz said:
    Maybe this is unorthodox, but I took to creating an arrow symbol, and sometimes add it to schematics to remind myself of the direction of a few interesting signals.

    The library allows for different pin styles. For the default function, and a different one for each of the alternatives. Not a simple I, O or IO option though.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Jan Cumps

    Renesas' own house style:

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to Jan Cumps

    Hehe yeah their's is for sure ugly. Rarely the pin-number-sequence layout can be fine. Might be ok for serving double-duty, (1) showing the chip overview and (2) showing a basic example circuit, which I suppose is what they are doing, so it's kind-of acceptable for their documentation use-case.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 2 years ago

    Looks useful.  I recently created a schematic with a PIC MCU and ended up creating a new symbol with the pin names I wanted where they were multi-functional.  I sometimes create a symbol where the pins are positioned based on keeping the schematic clean and easy to follow.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to shabaz
    shabaz said:
    (2) showing a basic example circuit,

    It's for a full design:

    image

    I like what they do for their basic examples and "principles" schematics:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>