PCB Design, Prototyping and Production
  • Products
  • More
PCB Design, Prototyping and Production
PCB Forum Let's talk about Crosstalk !
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 133 subscribers
  • Views 3852 views
  • Users 0 members are here
  • cross-talk
  • frequency_generator
  • pcb
  • oscilloscope
  • spectrum_analyzer
  • debugging
Related

Let's talk about Crosstalk !

battlecoder
battlecoder over 1 year ago

I've been a member for a long time, but this is my first time posting.

I guess it's a bit too late for a presentation, but I'm a software engineer with a fascination for electronics; It's been my hobby for more than 20 years, and I keep learning new things almost every day.

I recently became interested in frequency domain analysis. I know it has countless applications in the Ham/radio world, but I was thinking about more general-purpose use cases; like identifying cross-talk or interference on a PCB design.

I know that's a huge topic and there's some well known general advice and practices to reduce this, like ground planes and decoupling capacitors, and filters... but I wanted to check how bad it could be, if absolutely no sane advice or practice was followed.

So I came up with this ugly PCB as my ultimate test-bed:

image

This is honestly not far from a PCB I would have designed when I was starting in electronics. I liked having nothing but the tracks on the board.

For a first test, I injected two signals from a signal generator on the left side of the PCB, both very stable and clean. One of them a 7 Mhz sine wave, and the other one a 10 Mhz square wave. I picked two relatively close frequencies to see how easy (or hard) was going to be telling them apart later.

Both traces start very far from each other on the left side of the PCB on big pads, and then they get closer together near the center, just to take on their own separate paths again as their approach the right side.

I'm monitoring the "output pad" on the right side for both waveforms on an oscilloscope, and while I was initially watching both on the screen of the scope, the one that I think looked more interesting was the output of the "sine wave" trace:

image

That's one messed up sine wave. For the record; without the square wave signal connected (or with the signal turned off), that wobbly sine-wave becomes a very clean, proper sinusoidal wave, so this was clearly the influence of the other signal.

I'm sure it's possible to use the FFT on the scope to dissect the frequency content of that signal,but I wanted to explore none-invasive methods. Something that I could use for a quick inspection and that didn't require probing around test points or component pins. Something that could potentially identify higher-frequency content outside of the range of my scope. And for that  I went for a cheap "near field" probe, connected to a TinySA Ultra Spectrum Analyzer. You can actually see the near field "probe" hovering over the tracks in the first picture.

This is a capture from the TinySA:

image

I was honestly amazed at how well this worked. The probe captured perfectly the two main components of the coupled signal (both a 7 and a 10 Mhz component) even without touching the PCB. Because I zoomed tightly on the frequency range of both signals there's no harmonics from the square wave in sight.

The results were pretty exciting to me, but this left me curious about a couple of things. And I thought this forum was the perfect place to ask::

How often is this kind of debugging needed in real life? How frequently is this kind of analysis required? (other than when performing EMI emissions testing). Is there an area in electronics where cross-talk issues are more of a problem than in others? (for example is this problem worse in high-frequency applications?)

If any of you have an anecdote or story where cross-talk has been an issue, a mystery, or a lesson well learned, I'd love to hear it!

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 1 year ago in reply to battlecoder +4
    I found the book that I was referring to, "Mixed-Signal Hardware and Housekeeping Techniques" by Walt Kester of Analog Devices. This was a part of the handout for a seminar session that I attended on dealing…
  • cstanton
    cstanton over 1 year ago +3
    battlecoder said: How frequently is this kind of analysis required? When you start discussing crosstalk, you perhaps also start delving into the concepts and implications of information leakage, what…
  • battlecoder
    battlecoder over 1 year ago in reply to e14phil +3
    Thanks! I've been meaning to write here for a while, but I couldn't find something interesting to write about. When I decided to experiment with this I figured it would be great to have input from actual…
Parents
  • robogary
    robogary over 1 year ago

    This type of debugging is also done with testing new designs, at the electrical panel level too. 

    Various HF signals are broadcast with a directional antenna at panels and cables to test susceptibility. Panel doors are then opened to see how it behaves with doors open. 

    There is the old walkie talkie test to see if there is misbehavior while techs worked on electrical equipment with the doors open, and they talked with walkie talkies.

    Really old electrical panels for big control systems wired in audio headsets into panels so folks didnt use walkie talkies.   

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • battlecoder
    battlecoder over 1 year ago in reply to robogary

    That's very interesting. This actually makes me wonder about sort of the opposite experiment: Instead of having a trace "induce" a signal into a neighboring trace, what about testing interference from an external "radio" source into existing signals on the board. The setup would be pretty much the same, except that maybe the frequency analysis would be done with physical contact (instead of using an H-Field probe) and the source of interference would be a nearby transmitter instead of one of the traces in the circuit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 1 year ago in reply to battlecoder

    Quite a sticky wicket - Physical contact for debugging can provide interaction with the signals as well, either by injecting noise from other sources like ground, or providing some filtering of the noise and cross talk. These troubleshooting guys make the big bucks :-) 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • battlecoder
    battlecoder over 1 year ago in reply to robogary

    That's true. There's also the issue of probe loading at high frequencies. I haven't gone too deep into the subject, but I did have a close encounter with that, recently. Turns out that the 10M impedance of the scope probe is just at DC, and at higher frequencies that goes ridiculously low to the point of severely loading your signals and introducing artifacts that aren't really there. So I'm definitely not a fan of physically probing high-speed signals anymore.

    But high frequency, EMI and interference is still a domain of black magic and mysteries to me. I got the tinySA to learn more about the topic, and I'm very tempted to acquire an actual, proper SA in a future. But it's hard to justify the price just for the sake of learning, when something like the tinySA seems to do just fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • battlecoder
    battlecoder over 1 year ago in reply to robogary

    That's true. There's also the issue of probe loading at high frequencies. I haven't gone too deep into the subject, but I did have a close encounter with that, recently. Turns out that the 10M impedance of the scope probe is just at DC, and at higher frequencies that goes ridiculously low to the point of severely loading your signals and introducing artifacts that aren't really there. So I'm definitely not a fan of physically probing high-speed signals anymore.

    But high frequency, EMI and interference is still a domain of black magic and mysteries to me. I got the tinySA to learn more about the topic, and I'm very tempted to acquire an actual, proper SA in a future. But it's hard to justify the price just for the sake of learning, when something like the tinySA seems to do just fine.