PCB Design, Prototyping and Production
  • Products & Partners
  • More
PCB Design, Prototyping and Production
PCB Forum PCB design - Question from schematic to PCB | Kicad
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join PCB Design, Prototyping and Production to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 158 subscribers
  • Views 3048 views
  • Users 0 members are here
  • kicad
Related

PCB design - Question from schematic to PCB | Kicad

feiticeir0
feiticeir0 over 2 years ago

Hi all !

I'm coming to you with, probably, a newby question from PCB design.

I'm trying to design my second PCB (the first one had a flaw that I didn't foresaw and was a bust) and I'm coming to you for a small verification.

I'm trying to design a PCB for the following circuit (from https://randomnerdtutorials.com/power-esp32-esp8266-solar-panels-battery-level-monitoring/:

image

I'm going to use a ESP32-CAM .

I already have the kicad project done - the schematics:

image

and the PCB layout:

image

Now, my question is regarding the wiring from the battery to the two capacitors and then to the ESP32-CAM. Will the wiring, like it is, be the same like in Fritzing design ?

I have this working on a breadboard - but there I wire all the wires on the same rail -

image

Thank you

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 2 years ago in reply to Jan Cumps +3
    Zones are a bit odd, until you managed to use them once. Maybe create a project with just Vss, Vdd and two resistors in parallel. Then try to play with zones on the PCB design of that simple example. …
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to feiticeir0 +2
    When you add the zone, give it the same net name as the pads that you try to connect.
  • feiticeir0
    feiticeir0 over 2 years ago in reply to shabaz +1
    Thank you ! I'm not even considering the TP4056 for the PCB - that will be connected to the solar panels. This PCB will only be from output of the TP4056 - it will be connected to the battery holes.…
Parents
  • strb
    0 strb over 2 years ago

    I'm not 100% sure about you doubt, I hope I'm understanding your question correctly. From what I see, capacitors on your scheme are connected as pictured in the tutorial diagram and also as you have connected on the breadboard (between gnd and regulator output). I can't say much more on all the other wiring from the breadboard photo.

    I would also like to give you a couple more suggestions:
    - on the scheme, try using "global symbols" like gnd and/or 3.3V supply rail, it will make for a more readable scheme
    - on the pcb, I would suggest to increase the trace width. You don't need such thin connections and you risk to make you pcb more costly without any real benefit. Thin traces are more fragile and difficult to patch in case you need to correct a mistake manually

    Hope it will help Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • strb
    0 strb over 2 years ago

    I'm not 100% sure about you doubt, I hope I'm understanding your question correctly. From what I see, capacitors on your scheme are connected as pictured in the tutorial diagram and also as you have connected on the breadboard (between gnd and regulator output). I can't say much more on all the other wiring from the breadboard photo.

    I would also like to give you a couple more suggestions:
    - on the scheme, try using "global symbols" like gnd and/or 3.3V supply rail, it will make for a more readable scheme
    - on the pcb, I would suggest to increase the trace width. You don't need such thin connections and you risk to make you pcb more costly without any real benefit. Thin traces are more fragile and difficult to patch in case you need to correct a mistake manually

    Hope it will help Slight smile