Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Performance problem as 1920 pixels squashed into 1824
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 707 subscribers
  • Views 2488 views
  • Users 0 members are here
  • raspberry_pi
Related

Performance problem as 1920 pixels squashed into 1824

morgaine
morgaine over 14 years ago

My Pi is currently suffering the same "picture frame" problem that many others have described, losing 96 pixels vertically and horizontally (48 from each edge) from the native resolution of a  good quality 27" Dell 2408 1920x1200 LCD monitor, feeding into its HDMI port.  The monitor data is being read fine, and includes:

 

Group CEA has 8 modes:

  (native) mode 16: 1920x1080 @ 60Hz, progressive

Group DMT has 11 modes:

               mode 68: 1920x1200 @ 60Hz, progressive

HDMI status:

               state 0x120016, 1920x1200 @ 60Hz, progressive

 

To match the monitor's expectations, I set up /boot/config.txt with:

 

hdmi_group=2

hdmi_mode=68

 

 

So far so good, but when I bring up X11, /var/log/Xorg.0.log shows:

 

(--) FBDEV(0): Virtual size is 1824x1104 (pitch 1824)

 

which is confirmed by /proc/cmdline:

 

dma.dmachans=0x3c bcm2708_fb.fbwidth=1824 bcm2708_fb.fbheight=1104

bcm2708.boardrev=0x2 bcm2708.serial=0x25f2f590 smsc95xx.macaddr=B8:27:EB:F2:F5:90

dwc_otg.lpm_enable=0 console=ttyAMA0,115200 kgdboc=ttyAMA0,115200

console=tty1 root=/dev/mmcblk0p2 rootfstype=ext4 rootwait

 

This looks like a simple problem of overscan, but setting the four overscan_* parameters to 0 in /boot/config.txt does not change the situation.

 

So, although the display and HDMI are running at 1920x1200, only 1824x1104 is being used for visible data.  Now this is the same problem that others have reported and so it may get sorted out, but there is a 2nd problem that I haven't seen reported and which is causing me trouble which this post is about.

 

If I add "bcm2708_fb.fbwidth=1920 bcm2708_fb.fbheight=1200" to /boot/cmdline.txt (as people have suggested), then sure enough the system makes the change and /var/log/Xorg.0.log shows that it's heading in the right direction:

 

(--) FBDEV(0): Virtual size is 1920x1200 (pitch 1920)

 

The trouble is, X11's 1920x1200 area is now mapped into the old 1824x1104 letterbox section of the screen, so instead of better it's actually worse.  Unsurprisingly the fonts look horrible and there is moire patterning as 1920 virtual screen pixels are squashed into 1824 real ones, and correspondingly 1200->1104 on the y axis.  And what's even worse is that in this configuration there is also a lot of USB data loss from both keyboard and mouse, possibly because the drivers are spending so much time converting the virtual screen resolution to the real one.  It's really quite bad.

 

This may be related to the rather ambivalent state of /proc/cmdline under these conditions, which shows both resolutions!

 

dma.dmachans=0x3c bcm2708_fb.fbwidth=1824 bcm2708_fb.fbheight=1104

bcm2708 boardrev=0x2 bcm2708.serial=0x25f2f590 smsc95xx.macaddr=B8:27:EB:F2:F5:90

dwc_otg.lpm_enable=0 console=ttyAMA0,115200 kgdboc=ttyAMA0,115200

console=tty1 root=/dev/mmcblk0p2 rootfstype=ext4 rootwait

bcm2708_fb.fbwidth=1920 bcm2708_fb.fbheight=1200

 

I don't really know what it means when it displays both resolutions like that, but the end result is wrong.  A lot of threads have already been written in the RPF forums on this general topic, but I don't think I see a clear way forward.  Any suggestions?

 

Morgaine.

  • Sign in to reply
  • Cancel
  • johnbeetem
    johnbeetem over 14 years ago in reply to e14 Contributor

    "dom" has a new firmware patch that reduces interrupts to 300 per second: http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=7866&p=117575#p117575.  The good news: better CPU performance.  The bad news: much worse NFS performance.  He doesn't say if this is caused by dropped Ethernet frames, which is by far the easiest way to destroy network performance since most protocols assume Ethernet is usually reliable and that lost frames only rarely need to be retransmitted.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to johnbeetem

    hmm.. that doesn't look like an improvement to me. I mostly ssh in to my pi, so I think I'll stick with older firmware for now and see if it improves later.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to johnbeetem

    John Beetem wrote:

     

    The good news: better CPU performance. The bad news: much worse NFS performance.

     

    Eeeek.  Well I'll have to try it.

     

    Regarding CPU, I thought initially that the ~30% CPU that MOC uses when playing an ogg from an NFS server might be mostly the USB interrupts cost, but that can't be since the CPU load is the same when playing the same track from SD card.

     

    Hmmm, just had the nasty thought that maybe the SoC can't decode oggs or that ALSA hasn't yet been made aware that it can, so the poor little ARM is doing the whole job of decoding.  Yet another thing to figure out.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to e14 Contributor

    BTW, my Pi crashed today while playing music over NFS.  I wasn't touching the mouse or keyboard at the time.

     

    The screen went totally black (unfortunately I can't remember the state of the LEDs), and the Pi was making no network response to pings from other machines on the LAN.

     

    I removed the "arm_freq=800" from config.txt just in case it was caused by the slight overclocking.  My LAN9512 is so blisteringly hot that it's possible that the increased frequency made a bad situation worse.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    I've not had issues with the arm_freq=800, it's on every card I have. While the lan9512 gets warm I'd not say it's a problem on mine. It certainly doesn't fail the fingertip test for me.

     

    I suspect the arm is decoding the ogg, not that I'm an expert on this sort of stuff, but a quick squint at the driver gives no indication that it's anything special or indeed anything more than a simple pcm output.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<