Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspi-updater, how do I install it?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 708 subscribers
  • Views 2456 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspi-updater, how do I install it?

wallarug
wallarug over 14 years ago

Question says it all.

 

I am running Raspbian.

  • Sign in to reply
  • Cancel
  • morgaine
    morgaine over 14 years ago in reply to wallarug

    I rummaged around a bit but couldn't find any kind of automatic update system installed in the usual places, not even after an apt-get update and upgrade.  And although the Raspbian site claims that the distro comes with the rpi-update script now, that seems to be incorrect as well.

     

    I grabbed rpi-update from Hexxeh's repo and ran it manually, which was successful.  It doesn't seem to have improved anything though, as all the USB and networking problems remain, and there doesn't appear to be any improvement in codecs either.

     

    Whatever the update updated isn't something that I'm using, apparently.  And the kernel remains at 3.1.9+, bleh.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to morgaine

    And the kernel remains at 3.1.9+, bleh.

    It's quite disappointing that they seem to be stuck at 3.1.9 no matter what. Especially as there are better alternatives available.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    And the kernel remains at 3.1.9+, bleh.

    It's quite disappointing that they seem to be stuck at 3.1.9 no matter what. Especially as there are better alternatives available.

    So, it is not required.  Thank you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rhughes-uk
    rhughes-uk over 14 years ago in reply to morgaine

    Perhaps I was being a little misleading when I said updated automagically. What I should have said was:

     

    I beleive that that firmware updates are in the distro repository now so that a $ Sudo apt-get update && sudo apt-get upgrade will do all that is expected including the fimware if there is a newer version.

     

    Of course no one on Linux HAS to do any upgrades or updates. So its totally free choice. But I have to admit that I was happy to do the upgrade and then not need to do that Hexxeh bit after as well.(one thing less to forget)

     

    All your needs may differ. Indeed this process may differ in time. Probably already has knowing my luck. image

     

    Have fun all

     

    Ray

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 14 years ago in reply to rhughes-uk

    One big disappointment after all the upgrades though was the fact that media still barely works.

     

    Wasn't media supposed to be the best part of Raspberry Pi, because the BCM2835 is basically just one huge media and DSP processor with a tiny old ARM core tucked in one corner?  Well that would be great if the media stuff worked well, but even after these latest upgrades omxplayer is still the only player that will play videos with hardware acceleration.  Unfortunately it can play only a single type of video format, and even that jitters at 1080p.

     

    And we can't even fix this poor state of affairs, because the media side of Pi is closed source.

     

    This is a really disappointing situation.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to wallarug

    So, it is not required.  Thank you.

    Well not quite sure I'd go that far.  There will be different revisions of 3.1.9 - maybe one will solve your wifi problems, who knows.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wallarug
    wallarug over 14 years ago in reply to e14 Contributor

    selsinork wrote:

     

    So, it is not required.  Thank you.

    Well not quite sure I'd go that far.  There will be different revisions of 3.1.9 - maybe one will solve your wifi problems, who knows.image

    I have been working in two threads on E14 and RPi forums, I found a thing that installs the rpi-updater and fixes my wireless (sort of).

     

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=26&t=6256&p=148282&hilit=wallarug#p148282

     

    Other forums I have been working on:

    http://www.element14.com/community/thread/18605?start=60&tstart=0

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=45&t=13482&p=141143&hilit=fergus#p141143

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=45&t=13482&p=141143&hilit=fergus#p141143
    It fixed my wireless but failed to install rpi-update.  I don't mind if I don't have the latest firmware on my RPi becasue I don't know how to build anything in linux and mess-up linux in a way that requires this feature.  I would just download a fresh image off the raspberrypi.org page.

     

    Thanks for all your help anyway.


    PS: I just read the first link above and it seems that he has suggested some help that I will try later.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<