http://www.raspberrypi.org/phpBB3/viewtopic.php?f=63&t=16418
Liz writes:
"It's really good fun for us watching them arrive and confuse you guys. \smile "
http://www.raspberrypi.org/phpBB3/viewtopic.php?f=63&t=16418
Liz writes:
"It's really good fun for us watching them arrive and confuse you guys. \smile "
try twitter!
http://twitter.com/mcmarto/status/227388029638152193
http://twitter.com/_mebito_/status/220208700659478528
http://twitter.com/Dinsmoor/statuses/233616956090089473
http://twitter.com/codebutler/status/215337825791524864
http://twitter.com/cymplecy/status/240146369535410176
http://twitter.com/bldngnerd/statuses/219573098045915138
http://199.59.148.102/rcklmk/status/229869185755410433
coder27: There's a serious message there, and I hope that the other ARM Linux board manufacturers are listening carefully. The message says:
"Make it so cheap that it falls under the budget radar, and you'll sell it not only to tech-aware people but also to their dogs, and to their dogs' fleas as well."
Morgaine.
It's all about education.
So, why not use the Pi for the marketing, accounting and management classes..
How to create a need on the market and produce a best seller using a non profit buisiness model.
You only need one Pi to show to the class what you are talking about. (Very cheap)
It even doesn't need to work.
Those who graduate can instantly sollicitate at apple....
"What I find distasteful though is the way it is being handled by the Foundation, responding with unprofessional quips when people discover changes, instead of making official announcements on the day that each revision is released for sale."
I do agree the Foundation have made their fair share of mistakes but as the Foundation is not responsible for Manufacturing or Distribution then you are shooting at the wrong body on this one, yes?
Chris Evans wrote:
"What I find distasteful though is the way it is being handled by the Foundation, responding with unprofessional quips when people discover changes, instead of making official announcements on the day that each revision is released for sale."
I do agree the Foundation have made their fair share of mistakes but as the Foundation is not responsible for Manufacturing or Distribution then you are shooting at the wrong body on this one, yes?
I think Morgaine was commenting on some of liz's comments like "It's really good fun for us [to watch] them arrive and confuse you guys." Yes, I realize that liz was being gamesome, and I haven't heard of anyone being grossly inconvenienced by the 2.0 changes. So as they say, "no harm, no foul".
OTOH, how would you feel if you had designed a board that used the old GPIO pinout, manufactured a few thousand of them, and then discovered that there was a new revision being delivered before RasPi announced the change? Wouldn't you have liked to have known that the change was being considered so you could plan ahead? RasPi may not have precise control over distribution, but they do have control over what information is released, and when.