Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Timeout Waiting for Hardware Interrupt on mmc0
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 708 subscribers
  • Views 5445 views
  • Users 0 members are here
  • single_board_computer
  • single_board_computers
Related

Timeout Waiting for Hardware Interrupt on mmc0

GeorgeIoak
GeorgeIoak over 13 years ago

I'm not even going to bother posting this over in the "other" forum. I've got a project with 27 RPi and I purchased 27 Patriot 8GB Class 10 cards. 25/27 of the cards work fine but 2 of them keep throwing these errors on boot up. I have used GParted, Windows, the kitchen sink, to reformat, delete, check and every other system has no problems with these 2 cards.

 

Anyone got any ideas what else I can try to salvage these 2 cards? It's gotten under my skin now and I want to figure this out as it doesn't make any sense.

Attachments:
image
  • Sign in to reply
  • Cancel
  • morgaine
    morgaine over 13 years ago in reply to GeorgeIoak

    George Ioakimedes wrote:

     

    We're all somewhat assumming that some of these problems we've encountered can be attributed to the BCM2835 but if so what's the big deal for the Foundation to fess up and say hey the chip works great but these are the known problems and we're stuck with them.

     

    Problems with the BCM2835 progressed beyond the stage of assumption with this post by gsh on the RPi forum --- http://www.raspberrypi.org/phpBB3/viewtopic.php?f=28&t=12097&hilit=elephant&start=75 .  Quoting from it:

     

    I've had a little while to understand what is going wrong with the USB and traced it back to a problem with poor interrupt latency in the kernel.  This is causing the split transactions to be delayed beyond a 1ms frame which in turn means that the hub is dropping the packets it stores.

     

    This would have come as no surprise to anyone even moderately acquainted with Linux kernels (nor indeed with any Unix-type system), because none of the *nix family of operating systems have realtime-capable kernels as standard functionality, and that is inherent in their design.

     

    Linux acquired some basic realtime capability with special patches for that purpose, but although these allow certain realtime constraints to be met, their best possible realtime response latency is still very poor compared to operating systems expressly designed for realtime use.  (I've used these patched kernels personally for MIDI applications, and they are not very effective, loss of USB events still being common.)

     

    It's because of this that we know that the ARM11 inside the BCM2835 was never intended to be used to power a general purpose computer, because its CPU power is required to be permanently available for servicing the SoC's USB controller in order to keep response latency below 1 ms so that USB's split transactions are not dropped.  As a matter of principle, this is impossible to guarantee under normal operation in a Linux kernel that is also scheduling significant user-space applications.

     

    So, it's a lot more than a mere assumption that the BCM2835 was the wrong device to choose for the job.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GeorgeIoak
    GeorgeIoak over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    Do take a look at this RasPi forum thread started by dom: Request for Failing sdcards.  He may be interested in testing your failing cards.  Good engineers love reproducible bugs because they're already half solved.

     

    I had seen that thread and it looked somewhat dead so I didn't bother posting to it. Unfortunately in this tight economy I can't afford to sit on unused stock so I already returned those cards. I kind of kick myself for not keeping one just for reference but in the heat of the moment I said screw it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GeorgeIoak
    GeorgeIoak over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    It's because of this that we know that the ARM11 inside the BCM2835 was never intended to be used to power a general purpose computer, because its CPU power is required to be permanently available for servicing the SoC's USB controller in order to keep response latency below 1 ms so that USB's split transactions are not dropped.  As a matter of principle, this is impossible to guarantee under normal operation in a Linux kernel that is also scheduling significant user-space applications.

     

    So, it's a lot more than a mere assumption that the BCM2835 was the wrong device to choose for the job.

     

    Morgaine.

    I'd love to sit down with you guys one time over some beers but I have a feeling that we're spread across the world so I'll just drink one in your honor tonight!

     

    Are you thinking that the ARM11 in general isn't enough or just one in the BCM2835? I ask because I don't see these issues being brought up on the Pandaboard or Beagleboard forums. I know that's not comparing Apples to Apples but at least I haven't heard of these latency issues and they're running Ubuntu as one of the standard platforms.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to GeorgeIoak

    Are there any scope plots anywhere that show what speeds the RPi uses during the different phases of boot up, I didn't see any. That really seems odd to me especially since there are so many people working with these boards with all different levels of experience.

    Well I have actually watched what goes on during boot with a scope. It turns out not to be particularly relevant as different cards cause different speeds to be used. As you've already surmised, you can't always tell from the label on the outside of the card who made the innards and what it's capable of. So any scope trace is only useful for the exact card it was taken with, even an identically branded one can be different, so there's no real help there.

    The SD card fails at such an early stage in the boot process

    actually, as I tried to explain, when you see that timeout message from linux you're a long way into the boot. It's nothing like as early as you seem to assume.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • GeorgeIoak
    GeorgeIoak over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    The SD card fails at such an early stage in the boot process

     

    actually, as I tried to explain, when you see that timeout message from linux you're a long way into the boot. It's nothing like as early as you seem to assume.

    Going back and looking at the picture I snapped it's a bit misleading as I let that board run awhile before the picture was taken. From memory I would say that it thows the interrupt or other error message at about the 4th line displayed on the screen.

     

    Do you really think that all cards operate at slightly different clock rates? I haven't read the spec in quite a while but I would think you have the initial 400kHz for reading the CSD and once that's read it sets a clock rate depending on what is reported. If I was writing the driver I would then perform some type of operation to see if communication is good (perhaps a register read and checking the CRC?). Since every command has an expected response you'll know right away if there's any problem with the communication. Even with bulk transfers there's CRC and error status responses.

     

    You're right, I'm by no means a Linux guru so I couldn't tell you where in the boot process the RPi was complaining but in a very general sense the system didn't boot but yet that card worked fine in other systems and both chkdsk and fsck both reported not bad blocks.

     

    When you were probing the cards did you verify that they actually use 4-bit mode out of curiosity? Just because the schematic shows all lines connected still doesn't mean that they're used.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to GeorgeIoak

    George Ioakimedes wrote:

     

    Are you thinking that the ARM11 in general isn't enough or just one in the BCM2835? I ask because I don't see these issues being brought up on the Pandaboard or Beagleboard forums. I know that's not comparing Apples to Apples but at least I haven't heard of these latency issues and they're running Ubuntu as one of the standard platforms.

     

    The ARM11 is perfectly general.  It's the BCM2835's design that requires a CPU core to be dedicated to it if it is to maintain sub-1-ms latency in response to USB controller requests.  The ARM can't guarantee that response latency and be servicing the Linux process queue at the same time.  When it tries, a proportion of the time it can't meet the 1 ms maximum response time for split transactions, and so those get dropped.  The user sees this as lost USB events, which have totally plagued the Pi community as numerous RPF forum threads testify.

     

    This shouldn't really have come as any surprise to Pi designers, because they're clearly very knowledgeable about both the Linux kernel and the BCM2835, and hence should have known that a normal Linux kernel is not designed for low-latency realtime response whereas the BCM2835 is designed to require it.

     

     

    I'd love to sit down with you guys one time over some beers but I have a feeling that we're spread across the world so I'll just drink one in your honor tonight!

     

    A glass of nice Shiraz for me please. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to GeorgeIoak

    Going back and looking at the picture I snapped it's a bit misleading as I let that board run awhile before the picture was taken. From memory I would say that it thows the interrupt or other error message at about the 4th line displayed on the screen.

    Ok,  let me try again. When you see any message from Linux, you're a long way into the boot process.  Where do you think the linux kernel was loaded from ?

    It's also unfortunate that most current linux distros go out of their way to hide what's going on at boot, so your fourth line is even further in than you think.

     

    So, there's an example from my Pi at http://pastebin.com/uVAmd6ji since it's a bit big to post here. Go down to line 133, that's where the sdcard driver finally gets loaded by linux. Your message can't appear before then and likely won't appear before line 144 as that's where the card is starting to be used.

     

    Remember also that at least three other bits of code have booted off the card before linux runs and (in my case) something like 10-15Mb of data has been sucessfully read off the card before you see a single line on the screen.  An 'early' boot failure gives you a blank screen.

     

    Do you really think that all cards operate at slightly different clock rates? I haven't read the spec in quite a while but I would think you have the initial 400kHz for reading the CSD and once that's read it sets a clock rate depending on what is reported.

    Yes of course. You have two cards, the CSD in one says it can run at 10Mhz, the other says 20Mhz. You expect they'll run at the same speed ?  It is always possible that the early boot code (i.e. everything before linux) runs in some dumb, safe, mode (maybe only 400kHZ SPI mode), so it works, albeit slowly, until something increases the clock, enables 4 bit mode or whatever. 

    The early bits are very difficult to capture reliably on a scope, the clock changes a lot as different things happen during boot. It's much easier to see what's happening once the boot is complete, but thats after the interesting stuff has finished.

    Remind me another day and I'll see if I can get an OLS trace of the early boot to post here. Not sure that the OLS has enough memory to capture much, but it might at least give us a better idea.

    When you were probing the cards did you verify that they actually use 4-bit mode out of curiosity? Just because the schematic shows all lines connected still doesn't mean that they're used.

    What more can I say than the other bits are active - I don't have an SD-Card bus analyzer, so can't verify it for sure.

     

    However, here's a little snippet from the linux debugfs showing how the driver thinks it's talking to the card in my Pi:

     

    root@raspberry-pi:/sys/kernel/debug/mmc0# cat ios

    clock:          50000000 Hz

    vdd:            17 (2.9 ~ 3.0 V)

    bus mode:       2 (push-pull)

    chip select:    0 (don't care)

    power mode:     2 (on)

    bus width:      2 (4 bits)

    timing spec:    2 (sd high-speed)

     

    I currently have no reason to believe it's lying to me, especially when I can scope the lines and verify the clock and that all the bits are active.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
<